This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

gpio GPIO conectoin in DM6437

hi,

 

in DM6437 i need to build an output interface for that i want to conect it for the project with an wireup conection.

i thught that there should be an GPIO conectors that i can use but i didnt found them.

the things that most sutibale for the project is the DC_P1 and the DC_P2 but as i see in the datasheets i saw that they have another purpose.

my question is the following, is there any GPIO that i can actually use?

another is if there is not can i use the DC_P1 or the DC_P2 for a general purpose and use it as interupts in my project?

and finally is the last option is to use it with an test points.

 

thanks,

vadim