Part Number: TDA2EVM5777
Dear TI
I would like to include in new sensor to the TDA2. How or where can i create it to do that?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDA2EVM5777
Dear TI
I would like to include in new sensor to the TDA2. How or where can i create it to do that?
Hi Yordan
I wouls like to ask what is the follow abbreviation
DCC
H3A
GLBCE
AEWB
Also is it a must for me to code them?
On top of this ISS is it suitable to run in TAD2EVM5777 if i am going to add this new sensor? From the VisionSDK it seem like its for the TDA3xxEVm and TDA2PxEVM instead.
Hi Wilson,
These components are used in the ISS usecase, ISS is present in TDA3x and TDA2Px It is not supported in TDA2Ex.
DCC = Dynamic Camera Configuration
H3A = Statistics generation module for AE and AWB.
GLBCE = Global and Local Contrast and brightness Enhancement
AEWB = Auto Exposure and White Balance
Rgds,
Brijesh
Dear Brijesh
I notice there are 2 type of yuv which format i should be convering the bayer to?
Wilson,
DSS supports both YUV420 (Semi-planar) and YUV422 (Interleaved) data format. So if you could convert RAW to one of these data format, dss will be able to display it.
Rgds,
Brijesh