To keep costs down and simplify layout it would be great if standard 64-bit DDR2/DDR3 SO-DIMMs or DIMMs were usable with the C6A816x/AM389x.
The DDR interfaces are 32-bit wide. Is there a way to link them or have them both clock their data at the same time.
I have not been able to deduce from the latest datasheet (19 Oct 2010) or Technical Reference Manual (29 Oct 2010) whether all the memory on a standard 64-bit DDR2/DDR3 SO-DIMM would be usable.