Part Number: 66AK2H14
Tool/software: TI-RTOS
Hi,
66AK2H14 is interfaced to Altera MAX10 series CPLD through EMIF16 interface.
EMIF16 is configured to Select Strobe Mode.We have to perform CPLD read/write through EMIF16.
I have posted one query about how to configure control lines of EMIF. here is the link of my previous post 
I have to write 4096 bytes of data from the position 0000 to 4095.
I am writing to EMIF as ,
#define CPLD_DATA_ADDR 0x0034000000
data_addr = ( uint16_t *)CPLD_DATA_ADDR;
/* 8-bit flash */
while(i++ < SIZE)
{
if(j==256)
j=0;
*data_addr = cmp_val[j++];
data_addr++;
}
as per the previous post , The address lines are carried though from the lower address bits of the memory map with the shift.
When I signal tap the address line which goes to CPLD I am getting address like 000000 , 800000 , 000001 etc which I have to right rotate to get the correct address.
I have attached the screenshot for your reference.
My doubt is Whether this rotation has to be done by the master(66ak2h14) while writing to 0x34000000 or by the slave(CPLD)?