Other Parts Discussed in Thread: BEAGLEBOARD-X15,
Tool/software: Linux
Hi - when I try loading a pdk_am57xx_1_0_10 example project (built into packages/MyExampleProjects using the pdkProjectCreate.sh script), I'm getting the error below posted on the Linux A15 side:
[ 4765.421123] ------------[ cut here ]------------
[ 4765.425778] WARNING: CPU: 0 PID: 0 at drivers/bus/omap_l3_noc.c:147 l3_interrupt_handler+0x25c/0x36c
[ 4765.434951] 44000000.ocp:L3 Custom Error: MASTER IPU2 TARGET L4_PER1_P3 (Idle): Data Access in User mode during Functional access
[ 4765.446650] Modules linked in: sha512_generic sha512_arm sha256_generic sha1_generic sha1_arm_neon sha1_arm md5 cbc xfrm_user xfrm4_tunnel ipcomp xfrm_ipcomp esp4 ah4 af_key xfrm_algo bluetooth bc_example(O) xhci_plat_hcd xhci_hcd dwc3 udc_core pru_rproc pruss_intc rpmsg_proto rpmsg_rpc pruss ahci_platform libahci_platform libahci libata scsi_mod snd_soc_simple_card snd_soc_simple_card_utils snd_soc_omap_hdmi_audio omap_sham snd_soc_tlv320aic3x pvrsrvkm(O) omap_aes_driver omap_wdt pruss_soc_bus rtc_ds1307 dwc3_omap rtc_palmas ti_vpe rtc_omap ti_sc ti_csc ti_vpdma extcon_palmas extcon_core omap_des des_generic crypto_engine omap_remoteproc virtio_rpmsg_bus rpmsg_core remoteproc sch_fq_codel uio_module_drv(O) uio ftdi_sio usbserial usbcore usb_common gdbserverproxy(O) cryptodev(O) cmemk(O)
[ 4765.517291] CPU: 0 PID: 0 Comm: swapper/0 Tainted: G W O 4.9.69-g9ce43c71ae #1
[ 4765.525503] Hardware name: Generic DRA74X (Flattened Device Tree)
[ 4765.531620] Backtrace:
[ 4765.534093] [<c020b2bc>] (dump_backtrace) from [<c020b578>] (show_stack+0x18/0x1c)
[ 4765.541697] r7:00000009 r6:600b0193 r5:00000000 r4:c1022668
[ 4765.547384] [<c020b560>] (show_stack) from [<c04ce720>] (dump_stack+0x8c/0xa0)
[ 4765.554641] [<c04ce694>] (dump_stack) from [<c022e3ec>] (__warn+0xec/0x104)
[ 4765.561633] r7:00000009 r6:c0bc2f08 r5:00000000 r4:c1001d10
[ 4765.567318] [<c022e300>] (__warn) from [<c022e444>] (warn_slowpath_fmt+0x40/0x48)
[ 4765.574836] r9:00000006 r8:eea1c6d0 r7:c0bc32a0 r6:00000000 r5:c0bc2e34 r4:c0bc2ed8
[ 4765.582616] [<c022e408>] (warn_slowpath_fmt) from [<c04fe560>] (l3_interrupt_handler+0x25c/0x36c)
[ 4765.591524] r3:eea1c540 r2:c0bc2ed8
[ 4765.595112] r4:80080003
[ 4765.597659] [<c04fe304>] (l3_interrupt_handler) from [<c027fd6c>] (__handle_irq_event_percpu+0xb4/0x138)
[ 4765.607181] r10:c104dfaf r9:eea1a300 r8:00000017 r7:c1001e34 r6:00000000 r5:eea1a300
[ 4765.615041] r4:eea1ca40
[ 4765.617587] [<c027fcb8>] (__handle_irq_event_percpu) from [<c027fe14>] (handle_irq_event_percpu+0x24/0x60)
[ 4765.627283] r10:c10030ac r9:c1000000 r8:ee808000 r7:00000000 r6:c1008bf4 r5:eea1a300
[ 4765.635145] r4:eea1a300
[ 4765.637690] [<c027fdf0>] (handle_irq_event_percpu) from [<c027fe90>] (handle_irq_event+0x40/0x64)
[ 4765.646600] r5:eea1a360 r4:eea1a300
[ 4765.650194] [<c027fe50>] (handle_irq_event) from [<c0283540>] (handle_fasteoi_irq+0xc0/0x190)
[ 4765.658755] r7:00000000 r6:c1008bf4 r5:eea1a360 r4:eea1a300
[ 4765.664443] [<c0283480>] (handle_fasteoi_irq) from [<c027efa8>] (generic_handle_irq+0x2c/0x3c)
[ 4765.673091] r7:00000000 r6:00000000 r5:00000017 r4:c0e5cde0
[ 4765.678776] [<c027ef7c>] (generic_handle_irq) from [<c027f51c>] (__handle_domain_irq+0x64/0xbc)
[ 4765.687515] [<c027f4b8>] (__handle_domain_irq) from [<c02014a0>] (gic_handle_irq+0x40/0x7c)
[ 4765.695903] r9:c1000000 r8:fa213000 r7:fa212000 r6:c1001ef0 r5:fa21200c r4:c1003424
[ 4765.703681] [<c0201460>] (gic_handle_irq) from [<c020c038>] (__irq_svc+0x58/0x8c)
[ 4765.711193] Exception stack(0xc1001ef0 to 0xc1001f38)
[ 4765.716265] 1ee0: 00000001 00000000 fe600000 00000000
[ 4765.724479] 1f00: c1000000 c100303c 00000001 c10030a4 00000000 00000000 c10030ac c1001f4c
[ 4765.732691] 1f20: c1001f2c c1001f40 c0220e74 c0208714 600b0013 ffffffff
[ 4765.739335] r9:c1000000 r8:00000000 r7:c1001f24 r6:ffffffff r5:600b0013 r4:c0208714
[ 4765.747116] [<c02086ec>] (arch_cpu_idle) from [<c08d6934>] (default_idle_call+0x28/0x34)
[ 4765.755245] [<c08d690c>] (default_idle_call) from [<c026eb9c>] (cpu_startup_entry+0x1b4/0x230)
[ 4765.763899] [<c026e9e8>] (cpu_startup_entry) from [<c08d1c60>] (rest_init+0x8c/0x90)
[ 4765.771672] r7:ffffffff
[ 4765.774222] [<c08d1bd4>] (rest_init) from [<c0e00d80>] (start_kernel+0x3e0/0x3ec)
[ 4765.781734] r5:00000000 r4:c105104c
[ 4765.785329] [<c0e009a0>] (start_kernel) from [<80008090>] (0x80008090)
[ 4765.791881] ---[ end trace adeeca7fb9773f53 ]---
Specifically, the I2C basic example and the UART basic example from the pdk_am57xx_1_0_10 packages are the ones giving this error.
I read from another E2E thread that it may be related to the resources requested already being enabled through the device tree source on the linux side. I'm trying to figure out which I2C bus is being used and which UART is being used but I can't determine which I2C bus or which UART is being used in order to ensure it's being disabled in the board device tree.
Any ideas on this and if there are any other possible causes that I should be checking would be a great help!
Thanks,
Dermot