Other Parts Discussed in Thread: CCSTUDIO, OMAP-L137, OMAPL138
I have a spectrum ' s OMAPL137 evm board.
I want to connect the evm to my 560PCI emulator via JTAG.
But I can not find proper ccs setup files.
Could anyone give me some advice ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I had intended to test out this .ccs file but apparently my other machine with the XDS560PCI does not want to cooperate this morning. I created this configuration from scratch, but it should work. Note that I left out the GEL files from the DSP and ARM, but you can add those in manually.
After downloading this file you will need to open CCS Setup and select File->Import, then navigate to this .ccs file. I suggest placing it in C:\CCStudio_v3.3\drivers\import as this is the default location for these configurations.
Let me know if this works, and if not I will try to get my other PC working and fix any issues.
Yangsb is my colleague, Thanks for your reply.
After downloading this file , I open CCS Setup and select File->Import, then navigate to this .ccs file and plac3 it in C:\CCStudio_v3.3\drivers\import.
Now I can connect TMS320C674X_0. After connecting it, I view the address 0x11700000 of the memory according the document SPRAB04A. It's totally right.
But after connecting the TMS320C674X_0, I want to connect arm9_0. It's wrong with the following massage
"Warning
Error 0x40000260/-02062
Warning during: Execution, Initialization, OCS,
Cannot halt the processor
"
I also try to connect ARM9_0 without connecting TMS320C674X_0 first. It's also wrong. (According the document SPRUGI8, it should connect DSP first, then ARM later)
So I can't connect arm9_0 now.
The DSP needs to wake up the ARM before you can connect to it. Once you connect to the DSP, open up CCS and select Gel->OMAPL137Functions->Enable_ARM. This wakes up the ARM and should allow you to connect to it.
After I connect the DSP, the output shows "omap-l137 DSP Startup Sequence
Setup PINMUX Registers... [Done]
PLL Setup Complete
Setup Power Modules (All on)... [Done]
ARM Enabled
Startup Complete.
"
I then select Gel->OMAPL137Functions->Enable_ARM. (I also try not to do this step.)
the output shows "ARM Enabled"
But when I connect arm9_0. It's also wrong with the following massage
"Warning:
Error 0x40000260/-02062
Warning during: Execution, Initialization, OCS,
Cannot halt the processor"
When I connect DSP, the pointer stops at "
117F74E0 0000D303 .fphead n, l, W, BU, nobr, nosat, 1101011
117F74F0 00034000 SPKERNEL 0,0
"
The DSP GEL's content is as follow:
/* ------------------------------------------------------------------------ *
* *
* evmomapl137_dsp.gel *
* Version 1.02 *
* *
* This GEL file is designed to be used in conjunction with *
* CCStudio 3.3+ and the omap-l137 based EVM. *
* *
* Version History: *
* 1.00 Initial Release *
* 1.01 Added USB1 clock enable in CFGCGHIP2 *
* 1.02 Force CFGCGHIP2 == 0x0000EB42 *
* ------------------------------------------------------------------------ */
/* ------------------------------------------------------------------------ *
* *
* StartUp( ) *
* Setup Memory Map *
* *
* ------------------------------------------------------------------------ */
StartUp( )
{
Setup_Memory_Map( );
}
/* ------------------------------------------------------------------------ *
* *
* OnTargetConnect( ) *
* Setup PinMux, Power, PLLs, SDRAM & EMIFs *
* *
* ------------------------------------------------------------------------ */
OnTargetConnect( )
{
GEL_TextOut( "\nomap-l137 DSP Startup Sequence\n\n" );
Setup_System_Config( ); // Setup Pin Mux and other system module registers
Setup_PLL(); // Setup PLL0 (300MHZ ARM, 300MHz DSP, 133MHz EMIFs
Setup_Psc_All_On( ); // Setup All Power Domains
Setup_EMIFA(); // Async EMIF
Setup_EMIFB(); // Setup SDRAM
Enable_ARM();
GEL_TextOut( "\nStartup Complete.\n\n" );
}
/* ------------------------------------------------------------------------ *
* *
* OnPreFileLoaded( ) *
* This function is called automatically when the 'Load Program' *
* Menu item is selected. *
* *
* ------------------------------------------------------------------------ */
OnPreFileLoaded( )
{
/*
* GEL_Reset() is used to deal with the worst case senario of
* unknown target state. If for some reason a reset is not desired
* upon target connection, GEL_Reset() may be removed and replaced
* with something "less brutal" like a cache initialization
* function.
*/
GEL_Reset( );
// Disable_EDMA( ); // Disable EDMA
GEL_TextOut( "\n" );
}
/* ------------------------------------------------------------------------ *
* *
* OnRestart( ) *
* This function is called by CCS when you do Debug->Restart. *
* The goal is to put the CPU into a known good state with respect to *
* edma. *
* Failure to do this can cause problems when you restart and *
* run your application code multiple times. This is different *
* then OnPreFileLoaded() which will do a GEL_Reset() to get the *
* ARM9 into a known good state. *
* *
* ------------------------------------------------------------------------ */
OnRestart( int nErrorCode )
{
Disable_EDMA( ); // Disable EDMA
GEL_TextOut( "\n" );
}
menuitem "omap-l137 Memory Map";
/* ------------------------------------------------------------------------ *
* *
* Setup_Memory_Map( ) *
* Setup the Memory Map for DSP. *
* *
* ------------------------------------------------------------------------ */
hotmenu
Setup_Memory_Map( )
{
GEL_MapOn( );
GEL_MapReset( );
/* ARM */
GEL_MapAddStr( 0xFFFD0000, 0, 0x00010000, "R|W|AS4", 0 ); // ARM Local ROM
GEL_MapAddStr( 0xFFFE0000, 0, 0x00002000, "R|W|AS4", 0 ); // ARM INTC
GEL_MapAddStr( 0xFFFF0000, 0, 0x00002000, "R|W|AS4", 0 ); // ARM Local RAM
GEL_MapAddStr( 0x01BC0000, 0, 0x00001000, "R|W|AS4", 0 ); // ARM ETB Memory
GEL_MapAddStr( 0x01BC1000, 0, 0x00000800, "R|W|AS4", 0 ); // ARM ETB Regs
GEL_MapAddStr( 0x01BC1800, 0, 0x00000100, "R|W|AS4", 0 ); // ARM Ice Crusher
/* DSP */
GEL_MapAddStr( 0x00700000, 0, 0x00100000, "R|W|AS4", 0 ); // DSP L2 ROM
GEL_MapAddStr( 0x00800000, 0, 0x00040000, "R|W|AS4", 0 ); // DSP l2 RAM
GEL_MapAddStr( 0x00E00000, 0, 0x00008000, "R|W|AS4", 0 ); // DSP L1P RAM
GEL_MapAddStr( 0x00F00000, 0, 0x00008000, "R|W|AS4", 0 ); // DSP L1D RAM
GEL_MapAddStr( 0x01800000, 0, 0x00010000, "R|W|AS4", 0 ); // DSP Interrupt Controller
GEL_MapAddStr( 0x01810000, 0, 0x00001000, "R|W|AS4", 0 ); // DSP Powerdown Controller
GEL_MapAddStr( 0x01811000, 0, 0x00001000, "R|W|AS4", 0 ); // DSP Security ID
GEL_MapAddStr( 0x01812000, 0, 0x00008000, "R|W|AS4", 0 ); // DSP Revision ID
GEL_MapAddStr( 0x01820000, 0, 0x00010000, "R|W|AS4", 0 ); // DSP EMC
GEL_MapAddStr( 0x01830000, 0, 0x00010000, "R|W|AS4", 0 ); // DSP Internal Reserved
GEL_MapAddStr( 0x01840000, 0, 0x00010000, "R|W|AS4", 0 ); // DSP Memory System
GEL_MapAddStr( 0x11700000, 0, 0x00100000, "R|W|AS4", 0 ); // DSP L2 ROM (mirror)
GEL_MapAddStr( 0x11800000, 0, 0x00040000, "R|W|AS4", 0 ); // DSP l2 RAM (mirror)
GEL_MapAddStr( 0x11E00000, 0, 0x00008000, "R|W|AS4", 0 ); // DSP L1P RAM (mirror)
GEL_MapAddStr( 0x11F00000, 0, 0x00008000, "R|W|AS4", 0 ); // DSP L1D RAM (mirror)
/* Shared RAM */
GEL_MapAddStr( 0x80000000, 0, 0x00020000, "R|W|AS4", 0 ); // Shared RAM
/* EMIFA */
GEL_MapAddStr( 0x68000000, 0, 0x00008000, "R|W|AS4", 0 ); // EMIFA Control
GEL_MapAddStr( 0x40000000, 0, 0x20000000, "R|W|AS4", 0 ); // EMIFA SDRAM Data
GEL_MapAddStr( 0x60000000, 0, 0x02000000, "R|W|AS4", 0 ); // AEMIF CS2
GEL_MapAddStr( 0x62000000, 0, 0x02000000, "R|W|AS4", 0 ); // AEMIF CS3
GEL_MapAddStr( 0x64000000, 0, 0x02000000, "R|W|AS4", 0 ); // AEMIF CS4
GEL_MapAddStr( 0x66000000, 0, 0x02000000, "R|W|AS4", 0 ); // AEMIF CS5
/* DDR */
GEL_MapAddStr( 0xB0000000, 0, 0x00008000, "R|W|AS4", 0 ); // EMIFB Control
GEL_MapAddStr( 0xC0000000, 0, 0x20000000, "R|W|AS4", 0 ); // EMIFB SDRAM Data
/* Peripherals */
GEL_MapAddStr( 0x01C00000, 0, 0x00008000, "R|W|AS4", 0 ); // TPCC
GEL_MapAddStr( 0x01C08000, 0, 0x00000400, "R|W|AS4", 0 ); // TPTC0
GEL_MapAddStr( 0x01C08400, 0, 0x00000400, "R|W|AS4", 0 ); // TPTC1
GEL_MapAddStr( 0x01C10000, 0, 0x00001000, "R|W|AS4", 0 ); // PSC 0
GEL_MapAddStr( 0x01C11000, 0, 0x00001000, "R|W|AS4", 0 ); // PLL Controller 0
GEL_MapAddStr( 0x01C12000, 0, 0x00001000, "R|W|AS4", 0 ); // Key Manager
GEL_MapAddStr( 0x01C13000, 0, 0x00001000, "R|W|AS4", 0 ); // Security Controller
GEL_MapAddStr( 0x01C14000, 0, 0x00001000, "R|W|AS4", 0 ); // BootConfig
GEL_MapAddStr( 0x01C16000, 0, 0x00001000, "R|W|AS4", 0 ); // IOPU 0
GEL_MapAddStr( 0x01C17000, 0, 0x00001000, "R|W|AS4", 0 ); // IOPU 2
GEL_MapAddStr( 0x01C20000, 0, 0x00001000, "R|W|AS4", 0 ); // Timer64P 0
GEL_MapAddStr( 0x01C21000, 0, 0x00001000, "R|W|AS4", 0 ); // Timer64P 1
GEL_MapAddStr( 0x01C22000, 0, 0x00001000, "R|W|AS4", 0 ); // I2C 0
GEL_MapAddStr( 0x01C23000, 0, 0x00001000, "R|W|AS4", 0 ); // RTC
GEL_MapAddStr( 0x01C24000, 0, 0x00001000, "R|W|AS4", 0 ); // IOPU 1
GEL_MapAddStr( 0x01C30000, 0, 0x00000200, "R|W|AS4", 0 ); // dMax Data RAM 0
GEL_MapAddStr( 0x01C32000, 0, 0x00000200, "R|W|AS4", 0 ); // dMax Data RAM 1
GEL_MapAddStr( 0x01C34000, 0, 0x00004000, "R|W|AS4", 0 ); // dMax Control Registers
GEL_MapAddStr( 0x01C38000, 0, 0x00001000, "R|W|AS4", 0 ); // dMAX MAX0 Config Memory
GEL_MapAddStr( 0x01C3C000, 0, 0x00001000, "R|W|AS4", 0 ); // dMAX MAX1 Config Memory
GEL_MapAddStr( 0x01C40000, 0, 0x00001000, "R|W|AS4", 0 ); // MMC/SD 0
GEL_MapAddStr( 0x01C41000, 0, 0x00001000, "R|W|AS4", 0 ); // SPI 0
GEL_MapAddStr( 0x01C42000, 0, 0x00001000, "R|W|AS4", 0 ); // UART 0
GEL_MapAddStr( 0x01C43000, 0, 0x00001000, "R|W|AS4", 0 ); // MPU 0
GEL_MapAddStr( 0x01D00000, 0, 0x00001000, "R|W|AS4", 0 ); // McASP 0 Control
GEL_MapAddStr( 0x01D01000, 0, 0x00001000, "R|W|AS4", 0 ); // McASP 0 FIFO Ctrl
GEL_MapAddStr( 0x01D02000, 0, 0x00001000, "R|W|AS4", 0 ); // McASP 0 Data
GEL_MapAddStr( 0x01D04000, 0, 0x00001000, "R|W|AS4", 0 ); // McASP 1 Control
GEL_MapAddStr( 0x01D05000, 0, 0x00001000, "R|W|AS4", 0 ); // McASP 1 FIFO Ctrl
GEL_MapAddStr( 0x01D06000, 0, 0x00001000, "R|W|AS4", 0 ); // McASP 1 Data
GEL_MapAddStr( 0x01D08000, 0, 0x00001000, "R|W|AS4", 0 ); // McASP 2 Control
GEL_MapAddStr( 0x01D09000, 0, 0x00001000, "R|W|AS4", 0 ); // McASP 2 FIFO Ctrl
GEL_MapAddStr( 0x01D0A000, 0, 0x00001000, "R|W|AS4", 0 ); // McASP 2 Data
GEL_MapAddStr( 0x01D0C000, 0, 0x00001000, "R|W|AS4", 0 ); // UART 1
GEL_MapAddStr( 0x01D0D000, 0, 0x00001000, "R|W|AS4", 0 ); // UART 2
GEL_MapAddStr( 0x01D0E000, 0, 0x00001000, "R|W|AS4", 0 ); // IOPU 4
GEL_MapAddStr( 0x01E00000, 0, 0x00010000, "R|W|AS4", 0 ); // USB0 (USB HS) Cfg
GEL_MapAddStr( 0x01E10000, 0, 0x00001000, "R|W|AS4", 0 ); // UHPI Cfg
GEL_MapAddStr( 0x01E11000, 0, 0x00001000, "R|W|AS4", 0 ); // UHPI (IODFT)
GEL_MapAddStr( 0x01E12000, 0, 0x00001000, "R|W|AS4", 0 ); // SPI 1
GEL_MapAddStr( 0x01E13000, 0, 0x00001000, "R|W|AS4", 0 ); // LCD Controller
GEL_MapAddStr( 0x01E14000, 0, 0x00001000, "R|W|AS4", 0 ); // MPU 1
GEL_MapAddStr( 0x01E15000, 0, 0x00001000, "R|W|AS4", 0 ); // MPU 2
GEL_MapAddStr( 0x01E20000, 0, 0x00002000, "R|W|AS4", 0 ); // EMAC CPPI port
GEL_MapAddStr( 0x01E22000, 0, 0x00001000, "R|W|AS4", 0 ); // EMAC CPGMACSS registers
GEL_MapAddStr( 0x01E23000, 0, 0x00001000, "R|W|AS4", 0 ); // EMAC CPGMAC registers
GEL_MapAddStr( 0x01E24000, 0, 0x00001000, "R|W|AS4", 0 ); // EMAC MDIO port
GEL_MapAddStr( 0x01E25000, 0, 0x00001000, "R|W|AS4", 0 ); // USB1 (USB FS)
GEL_MapAddStr( 0x01E26000, 0, 0x00001000, "R|W|AS4", 0 ); // GPIO
GEL_MapAddStr( 0x01E27000, 0, 0x00001000, "R|W|AS4", 0 ); // PSC 1
GEL_MapAddStr( 0x01E28000, 0, 0x00001000, "R|W|AS4", 0 ); // I2C 1
GEL_MapAddStr( 0x01E29000, 0, 0x00001000, "R|W|AS4", 0 ); // IOPU 3
GEL_MapAddStr( 0x01E2A000, 0, 0x00001000, "R|W|AS4", 0 ); // PBIST Controller
GEL_MapAddStr( 0x01E2B000, 0, 0x00001000, "R|W|AS4", 0 ); // PBIST Combiner
GEL_MapAddStr( 0x01F00000, 0, 0x00001000, "R|W|AS4", 0 ); // EPWM 0
GEL_MapAddStr( 0x01F01000, 0, 0x00001000, "R|W|AS4", 0 ); // HRPWM 0
GEL_MapAddStr( 0x01F02000, 0, 0x00001000, "R|W|AS4", 0 ); // EPWM 1
GEL_MapAddStr( 0x01F03000, 0, 0x00001000, "R|W|AS4", 0 ); // HRPWM 1
GEL_MapAddStr( 0x01F04000, 0, 0x00001000, "R|W|AS4", 0 ); // EPWM 2
GEL_MapAddStr( 0x01F05000, 0, 0x00001000, "R|W|AS4", 0 ); // HRPWM 2
GEL_MapAddStr( 0x01F06000, 0, 0x00001000, "R|W|AS4", 0 ); // ECAP 0
GEL_MapAddStr( 0x01F07000, 0, 0x00001000, "R|W|AS4", 0 ); // ECAP 1
GEL_MapAddStr( 0x01F08000, 0, 0x00001000, "R|W|AS4", 0 ); // ECAP 2
GEL_MapAddStr( 0x01F09000, 0, 0x00001000, "R|W|AS4", 0 ); // EQEP 0
GEL_MapAddStr( 0x01F0A000, 0, 0x00001000, "R|W|AS4", 0 ); // EQEP 1
GEL_MapAddStr( 0x01F0B000, 0, 0x00001000, "R|W|AS4", 0 ); // IOPU 5
}
/* ------------------------------------------------------------------------ *
* *
* Clear_Memory_Map( ) *
* Clear the Memory Map *
* *
* ------------------------------------------------------------------------ */
hotmenu
Clear_Memory_Map( )
{
GEL_MapOff( );
GEL_MapReset( );
}
menuitem "EVMOMAPL137 Functions";
_wait( int delay )
{
int i;
for( i = 0 ; i < delay ; i++ ){}
}
#define SYS_BASE 0x01C14000
#define REVID *(unsigned int*)(SYS_BASE + 0x000)
#define DIEIDR0 *(unsigned int*)(SYS_BASE + 0x008)
#define DIEIDR1 *(unsigned int*)(SYS_BASE + 0x00C)
#define DIEIDR2 *(unsigned int*)(SYS_BASE + 0x010)
#define DIEIDR3 *(unsigned int*)(SYS_BASE + 0x014)
#define DEVIDR0 *(unsigned int*)(SYS_BASE + 0x018)
#define DEVIDR1 *(unsigned int*)(SYS_BASE + 0x01C)
#define BOOTCFG *(unsigned int*)(SYS_BASE + 0x020)
#define CHIPREVIDR *(unsigned int*)(SYS_BASE + 0x024)
#define KICK0R *(unsigned int*)(SYS_BASE + 0x038)
#define KICK1R *(unsigned int*)(SYS_BASE + 0x03c)
#define HOST0CFG *(unsigned int*)(SYS_BASE + 0x040) //ARM HOST0CFG
#define HOST1CFG *(unsigned int*)(SYS_BASE + 0x044)
#define IRAWSTAT *(unsigned int*)(SYS_BASE + 0x0E0)
#define IENSTAT *(unsigned int*)(SYS_BASE + 0x0E4)
#define IENSET *(unsigned int*)(SYS_BASE + 0x0E8)
#define IENCLR *(unsigned int*)(SYS_BASE + 0x0EC)
#define EOI *(unsigned int*)(SYS_BASE + 0x0F0)
#define FLTADDRR *(unsigned int*)(SYS_BASE + 0x0F4)
#define FLTSTAT *(unsigned int*)(SYS_BASE + 0x0F8)
#define MSTPRI0 *(unsigned int*)(SYS_BASE + 0x110)
#define MSTPRI1 *(unsigned int*)(SYS_BASE + 0x114)
#define MSTPRI2 *(unsigned int*)(SYS_BASE + 0x118)
#define PINMUX0 *(unsigned int*)(SYS_BASE + 0x120) //PINMUX0
#define PINMUX1 *(unsigned int*)(SYS_BASE + 0x124) //PINMUX1
#define PINMUX2 *(unsigned int*)(SYS_BASE + 0x128) //PINMUX2
#define PINMUX3 *(unsigned int*)(SYS_BASE + 0x12C) //PINMUX3
#define PINMUX4 *(unsigned int*)(SYS_BASE + 0x130) //PINMUX4
#define PINMUX5 *(unsigned int*)(SYS_BASE + 0x134) //PINMUX5
#define PINMUX6 *(unsigned int*)(SYS_BASE + 0x138) //PINMUX6
#define PINMUX7 *(unsigned int*)(SYS_BASE + 0x13C) //PINMUX7
#define PINMUX8 *(unsigned int*)(SYS_BASE + 0x140) //PINMUX8
#define PINMUX9 *(unsigned int*)(SYS_BASE + 0x144) //PINMUX9
#define PINMUX10 *(unsigned int*)(SYS_BASE + 0x148) //PINMUX10
#define PINMUX11 *(unsigned int*)(SYS_BASE + 0x14C) //PINMUX11
#define PINMUX12 *(unsigned int*)(SYS_BASE + 0x150) //PINMUX12
#define PINMUX13 *(unsigned int*)(SYS_BASE + 0x154) //PINMUX13
#define PINMUX14 *(unsigned int*)(SYS_BASE + 0x158) //PINMUX14
#define PINMUX15 *(unsigned int*)(SYS_BASE + 0x15C) //PINMUX15
#define PINMUX16 *(unsigned int*)(SYS_BASE + 0x160) //PINMUX16
#define PINMUX17 *(unsigned int*)(SYS_BASE + 0x164) //PINMUX17
#define PINMUX18 *(unsigned int*)(SYS_BASE + 0x168) //PINMUX18
#define PINMUX19 *(unsigned int*)(SYS_BASE + 0x16C) //PINMUX19
#define SUSPSRC *(unsigned int*)(SYS_BASE + 0x170)
#define CHIPSIG *(unsigned int*)(SYS_BASE + 0x174)
#define CHIPSIG_CLR *(unsigned int*)(SYS_BASE + 0x178)
#define CFGCHIP0 *(unsigned int*)(SYS_BASE + 0x17C)
#define CFGCHIP1 *(unsigned int*)(SYS_BASE + 0x180)
#define CFGCHIP2 *(unsigned int*)(SYS_BASE + 0x184)
#define CFGCHIP3 *(unsigned int*)(SYS_BASE + 0x188)
#define CFGCHIP4 *(unsigned int*)(SYS_BASE + 0x18C)
#define PLL0_BASE 0x01C11000 /*SYSTEM PLL BASE ADDRESS*/
#define PLL0_PID *(unsigned int*) (PLL0_BASE + 0x00) /*PID*/
#define PLL0_FUSERR *(unsigned int*) (PLL0_BASE + 0xE0) /*x*FuseFarm Error Reg*/
#define PLL0_RSTYPE *(unsigned int*) (PLL0_BASE + 0xE4) /*Reset Type status Reg*/
#define PLL0_PLLCTL *(unsigned int*) (PLL0_BASE + 0x100) /*PLL Control Register*/
#define PLL0_OCSEL *(unsigned int*) (PLL0_BASE + 0x104) /*OBSCLK Select Register*/
#define PLL0_SECCTL *(unsigned int*) (PLL0_BASE + 0x108) /*PLL Secondary Control Register*/
#define PLL0_PLLM *(unsigned int*) (PLL0_BASE + 0x110) /*PLL Multiplier*/
#define PLL0_PREDIV *(unsigned int*) (PLL0_BASE + 0x114) /*Pre divider*/
#define PLL0_PLLDIV1 *(unsigned int*) (PLL0_BASE + 0x118) /*Diveder-1*/
#define PLL0_PLLDIV2 *(unsigned int*) (PLL0_BASE + 0x11C) /*Diveder-2*/
#define PLL0_PLLDIV3 *(unsigned int*) (PLL0_BASE + 0x120) /*Diveder-3*/
#define PLL0_OSCDIV1 *(unsigned int*) (PLL0_BASE + 0x124) /*Oscilator Divider*/
#define PLL0_POSTDIV *(unsigned int*) (PLL0_BASE + 0x128) /*Post Divider*/
#define PLL0_BPDIV *(unsigned int*) (PLL0_BASE + 0x12C) /*Bypass Divider*/
#define PLL0_WAKEUP *(unsigned int*) (PLL0_BASE + 0x130) /*Wakeup Reg*/
#define PLL0_PLLCMD *(unsigned int*) (PLL0_BASE + 0x138) /*Command Reg*/
#define PLL0_PLLSTAT *(unsigned int*) (PLL0_BASE + 0x13C) /*Status Reg*/
#define PLL0_ALNCTL *(unsigned int*) (PLL0_BASE + 0x140) /*Clock Align Control Reg*/
#define PLL0_DCHANGE *(unsigned int*) (PLL0_BASE + 0x144) /*PLLDIV Ratio Chnage status*/
#define PLL0_CKEN *(unsigned int*) (PLL0_BASE + 0x148) /*Clock Enable Reg*/
#define PLL0_CKSTAT *(unsigned int*) (PLL0_BASE + 0x14C) /*Clock Status Reg*/
#define PLL0_SYSTAT *(unsigned int*) (PLL0_BASE + 0x150) /*Sysclk status reg*/
#define PLL0_PLLDIV4 *(unsigned int*) (PLL0_BASE + 0x160) /*Divider 4*/
#define PLL0_PLLDIV5 *(unsigned int*) (PLL0_BASE + 0x164) /*Divider 5*/
#define PLL0_PLLDIV6 *(unsigned int*) (PLL0_BASE + 0x168) /*Divider 6*/
#define PLL0_PLLDIV7 *(unsigned int*) (PLL0_BASE + 0x16C) /*Divider 7*/
#define PLL0_PLLDIV8 *(unsigned int*) (PLL0_BASE + 0x170) /*Divider 8*/
#define PLL0_PLLDIV9 *(unsigned int*) (PLL0_BASE + 0x174) /*Divider 9*/
#define PLL0_PLLDIV10 *(unsigned int*) (PLL0_BASE + 0x178) /*Divider 10*/
#define PLL0_PLLDIV11 *(unsigned int*) (PLL0_BASE + 0x17C) /*Divider 11*/
#define PLL0_PLLDIV12 *(unsigned int*) (PLL0_BASE + 0x180) /*Divider 12*/
#define PLL0_PLLDIV13 *(unsigned int*) (PLL0_BASE + 0x184) /*Divider 13*/
#define PLL0_PLLDIV14 *(unsigned int*) (PLL0_BASE + 0x188) /*Divider 14*/
#define PLL0_PLLDIV15 *(unsigned int*) (PLL0_BASE + 0x18C) /*Divider 15*/
#define PLL0_PLLDIV16 *(unsigned int*) (PLL0_BASE + 0x190) /*Divider 16*/
#define PLLEN_MUX_SWITCH 4
#define PLL_LOCK_TIME_CNT 2400
/*PSC Module Related Registers*/
#define PSC0_BASE 0x01C10000
#define PSC1_BASE 0x01E27000
#define PSC0_MDCTL (PSC0_BASE+0xA00)
#define PSC0_MDSTAT (PSC0_BASE+0x800)
#define PSC0_PTCMD *(unsigned int*) (PSC0_BASE + 0x120)
#define PSC0_PTSTAT *(unsigned int*) (PSC0_BASE + 0x128)
#define PSC1_MDCTL (PSC1_BASE+0xA00)
#define PSC1_MDSTAT (PSC1_BASE+0x800)
#define PSC1_PTCMD *(unsigned int*) (PSC1_BASE + 0x120)
#define PSC1_PTSTAT *(unsigned int*) (PSC1_BASE + 0x128)
/*Enable Function for PSC0*/
PSC0_lPSC_enable(unsigned int PD, unsigned int LPSC_num) {
*(unsigned int*) (PSC0_MDCTL+4*LPSC_num) = (*(unsigned int*) (PSC0_MDCTL+4*LPSC_num) & 0xFFFFFFE0) | 0x0003;
PSC0_PTCMD = 0x1<<PD;
while( (PSC0_PTSTAT & (0x1<<PD) ) !=0) ; /*Wait for power state transition to finish*/
while( (*(unsigned int*)(PSC0_MDSTAT+4 * LPSC_num) & 0x1F) !=0x3);
}
/*Enable Function for PSC1*/
PSC1_lPSC_enable(unsigned int PD, unsigned int LPSC_num) {
*(unsigned int*) (PSC1_MDCTL+4*LPSC_num) = (*(unsigned int*) (PSC1_MDCTL+4*LPSC_num) & 0xFFFFFFE0) | 0x0003;
PSC1_PTCMD = 0x1<<PD;
while( (PSC1_PTSTAT & (0x1<<PD) ) !=0) ; /*Wait for power state transition to finish*/
while( (*(unsigned int*)(PSC1_MDSTAT+4 * LPSC_num) & 0x1F) !=0x3);
}
hotmenu
Setup_PLL()
{
int i = 0;
/* Configure ARM, DSP at 300MHz, EMIFs at 133MHz */
unsigned int DIV45_EN = 1;
unsigned int CLKMODE = 0;
unsigned int PLLM = 24;
unsigned int POSTDIV = 1;
unsigned int PLLDIV3 = 2;
unsigned int PLLDIV5 = 5;
unsigned int PLLDIV7 = 7;
// Moved step 2c and 2d to step 0
/*Set PLLEN=0 and PLLRST=0, Reset the PLL*/
PLL0_PLLCTL &= 0xFFFFFFFE; /*PLL BYPASS MODE*/
/*wait for 4 cycles to allow PLLEN mux switches properly to bypass clock*/
for(i=0; i<PLLEN_MUX_SWITCH; i++) {;} /*Make PLLEN_MUX_SWITCH as bootpacket*/
/*Select the Clock Mode bit 8 as External Clock or On Chip Oscilator*/
PLL0_PLLCTL &= 0xFFFFFEFF;
PLL0_PLLCTL |= (CLKMODE<<8); /* Make CLKSRC as BootPacket to pass the value*/
/*Set PLLENSRC '0',bit 5, PLL Enable(PLLEN) selection is controlled through MMR*/
PLL0_PLLCTL &= 0xFFFFFFDF;
/*PLLCTL.EXTCLKSRC bit 9 should be left at 0 for Primus*/
PLL0_PLLCTL &= 0xFFFFFDFF;
/* Clear PLLRST bit to 0 -Reset the PLL */
PLL0_PLLCTL &= 0xFFFFFFF7;
/*Disable the PLL output*/
PLL0_PLLCTL |= 0x10;
/*PLL initialization sequence*/
/*Power up the PLL- PWRDN bit set to 0 to bring the PLL out of power down bit*/
PLL0_PLLCTL &= 0xFFFFFFFD;
/*Enable the PLL from Disable Mode PLLDIS bit to 0 - This is step is not required for Primus*/
PLL0_PLLCTL &= 0xFFFFFFEF;
/*PLL stabilisation time- take out this step , not required here when PLL in bypassmode*/
/* for(i=0; i<PLL_STABILIZATION_TIME; i++) {;} /* Make PLL_STABILIZATION_TIME as bootpacket*/
/*Program the required multiplier value in PLLM*/
PLL0_PLLM = PLLM; /* Make PLLMULTIPLEIR as bootpacket*/
/*If desired to scale all the SYSCLK frequencies of a given PLLC, program the POSTDIV ratio*/
PLL0_POSTDIV = 0x8000 | POSTDIV; /* Make POSTDIV as bootpacket*/
/*If Necessary program the PLLDIVx*/
/*Check for the GOSTAT bit in PLLSTAT to clear to 0 to indicate that no GO operation is currently in progress*/
while(PLL0_PLLSTAT & 0x1==1){}
/*Program the RATIO field in PLLDIVx with the desired divide factors. In addition, make sure in this step you leave the PLLDIVx.DxEN bits set so clocks are still enabled (default).*/
PLL0_PLLDIV3 = 0x8000 | PLLDIV3; /* Make PLLDIV3 as bootpacket, do it for other PLLDIVx to if required*/
PLL0_PLLDIV5 = 0x8000 | PLLDIV5; /* Make PLLDIV5 as bootpacket, do it for other PLLDIVx to if required*/
PLL0_PLLDIV7 = 0x8000 | PLLDIV7; /* Make PLLDIV7 as bootpacket, do it for other PLLDIVx to if required*/
/*Set the GOSET bit in PLLCMD to 1 to initiate a new divider transition.*/
PLL0_PLLCMD |= 0x1;
/*Wait for the GOSTAT bit in PLLSTAT to clear to 0 (completion of phase alignment).*/
while(PLL0_PLLSTAT & 0x1==1) { }
/*Wait for PLL to reset properly. See PLL spec for PLL reset time - This step is not required here -step11*/
/* for(i=0; i<PLL_RESET_TIME_CNT; i++) {;} /*128 MXI Cycles*/ /*Make PLL_RESET_TIME_CNT as boot packet*/
/*Set the PLLRST bit in PLLCTL to 1 to bring the PLL out of reset*/
PLL0_PLLCTL |= 0x8;
/*Wait for PLL to lock. See PLL spec for PLL lock time*/
for(i=0; i<PLL_LOCK_TIME_CNT; i++) {;} /*Make PLL_LOCK_TIME_CNT as boot Packet*/
/*Set the PLLEN bit in PLLCTL to 1 to remove the PLL from bypass mode*/
PLL0_PLLCTL |= 0x1;
KICK0R = 0x83e70b13; // Kick0 register + data (unlock)
KICK1R = 0x95a4f1e0; // Kick1 register + data (unlock)
CFGCHIP3 |= 0x4; // Enable 4.5 divider PLL
CFGCHIP3 |= 0x1; // Select 4.5 divider for EMIFB clock source only (not EMIFA)
GEL_TextOut( "PLL Setup Complete\n" );
}
/* ------------------------------------------------------------------------ *
* *
* setup_pll_0( ) *
* *
* clock_source <- 0: Onchip Oscillator *
* 1: External Clock *
* *
* pll_mult <- 21: 22x Multiplier * 27MHz Clk = 594 MHz *
* *
* ------------------------------------------------------------------------ */
setup_pll_0( int clock_source, int pll_mult )
{
unsigned int* pll_ctl = ( unsigned int* )( 0x01c11100 );
unsigned int* pll_pllm = ( unsigned int* )( 0x01c11110 );
unsigned int* pll_cmd = ( unsigned int* )( 0x01c11138 );
unsigned int* pll_postdiv = ( unsigned int* )( 0x01c11128 );
unsigned int* pll_bpdiv = ( unsigned int* )( 0x01c1112c );
unsigned int* pll_div1 = ( unsigned int* )( 0x01c11118 );
unsigned int* pll_div2 = ( unsigned int* )( 0x01c1111c );
unsigned int* pll_div3 = ( unsigned int* )( 0x01c11120 );
unsigned int* pll_div4 = ( unsigned int* )( 0x01c11160 );
unsigned int* pll_div5 = ( unsigned int* )( 0x01c11164 );
unsigned int* pll_div6 = ( unsigned int* )( 0x01c11168 );
unsigned int* pll_div7 = ( unsigned int* )( 0x01c1116c );
unsigned int* pll_div8 = ( unsigned int* )( 0x01c11170 );
unsigned int* pll_div9 = ( unsigned int* )( 0x01c11174 );
int pll0_freq = 24 * ( pll_mult + 1 );
GEL_TextOut( "Setup PLL0 " );
/*
* Step 1 - Set clock mode
*/
if ( clock_source == 0 )
*pll_ctl &= ~0x0100; // Onchip Oscillator
else
*pll_ctl |= 0x0100; // External Clock
/*
* Step 2 - Set PLL to bypass
* - Wait for PLL to stabilize
*/
*pll_ctl &= ~0x0020;
*pll_ctl &= ~0x0001;
_wait( 150 );
/*
* Step 3 - Reset PLL
*/
*pll_ctl |= 0x0008;
/*
* Step 4 - Disable PLL
* Step 5 - Powerup PLL
* Step 6 - Enable PLL
* Step 7 - Wait for PLL to stabilize
*/
*pll_ctl |= 0x0010; // Disable PLL
*pll_ctl &= ~0x0002; // Power up PLL
*pll_ctl &= ~0x0010; // Enable PLL
_wait( 150 ); // Wait for PLL to stabilize
/*
* Step 8 - Load PLL multiplier
*/
*pll_pllm = pll_mult & 0x3f;
/*
* Step 9 - Set PLL post dividers
*/
*pll_postdiv= 0x8000 | 1; // Post divider
*pll_div5 = 0x8001;
*pll_cmd |= 0x0001; // GO
_wait( 2000 );
/*
* Step 10 - Wait for PLL to reset ( 2000 cycles )
* Step 11 - Release from reset
*/
_wait( 2000 );
*pll_ctl &= ~0x0008;
/*
* Step 12 - Wait for PLL to re-lock ( 2000 cycles )
* Step 13 - Switch out of BYPASS mode
*/
_wait( 2000 );
*pll_ctl |= 0x0001;
// Enable 4.5X divider
KICK0R = 0x83e70b13; // Kick0 register + data (unlock)
KICK1R = 0x95a4f1e0; // Kick1 register + data (unlock)
CFGCHIP3 |= 0x4; // Enable 4.5 divider PLL
// CFGCHIP3 |= 0x3; // Select 4.5 divider for EMIFA / EMIFB clock source
pll0_freq = 24 * ( ( *pll_pllm & 0x3f ) + 1 ) / 2;
GEL_TextOut( "(DSP = %d MHz + ",,,,, pll0_freq );
GEL_TextOut( "ARM = %d MHz + ",,,,, pll0_freq );
if ( clock_source == 0 )
GEL_TextOut( "Onchip Oscillator)... " );
else
GEL_TextOut( "External Clock)... " );
GEL_TextOut( "[Done]\n" );
}
/* ------------------------------------------------------------------------ *
* *
* Disable_IRQ_Flush_Cache( ) *
* Flush Cache & Disable Interrupts *
* *
* ------------------------------------------------------------------------ */
Disable_IRQ_Flush_Cache( )
{
}
/* ------------------------------------------------------------------------ *
* *
* Disable_EDMA( ) *
* Disabe EDMA events and interrupts, clear any pending events *
* *
* ------------------------------------------------------------------------ */
Disable_EDMA( )
{
#define EDMA_3CC_IECRH *( unsigned int* )( 0x01c0105c )
#define EDMA_3CC_EECRH *( unsigned int* )( 0x01c0102c )
#define EDMA_3CC_ICRH *( unsigned int* )( 0x01c01074 )
#define EDMA_3CC_ECRH *( unsigned int* )( 0x01c0100c )
#define EDMA_3CC_IECR *( unsigned int* )( 0x01c01058 )
#define EDMA_3CC_EECR *( unsigned int* )( 0x01c01028 )
#define EDMA_3CC_ICR *( unsigned int* )( 0x01c01070 )
#define EDMA_3CC_ECR *( unsigned int* )( 0x01c01008 )
GEL_TextOut( "Disable EDMA events\n" );
EDMA_3CC_IECRH = 0xffffffff; // IERH - Disable high interrupts
EDMA_3CC_EECRH = 0xffffffff; // EERH - Disable high events
EDMA_3CC_ICRH = 0xffffffff; // ICRH - Clear high interrupts
EDMA_3CC_ECRH = 0xffffffff; // ICRH - Clear high events
EDMA_3CC_IECR = 0xffffffff; // IER - Disable low interrupts
EDMA_3CC_EECR = 0xffffffff; // EER - Disable low events
EDMA_3CC_ICR = 0xffffffff; // ICR - Clear low interrupts
EDMA_3CC_ECR = 0xffffffff; // ICRH - Clear low events
}
/* ------------------------------------------------------------------------ *
* *
* Enable_Instruction_Cache( ) *
* Enable I-Cache *
* *
* ------------------------------------------------------------------------ */
hotmenu Enable_Instruction_Cache( )
{
GEL_TextOut( "\Enable Instruction Cache.\n\n" );
CPSR = 0x400000d3; // Set to supervisor mode, disable IRQ/FIQ
REG_CP15_I_CACHE = 1; // Enable Instruction Cache
}
/* ------------------------------------------------------------------------ *
* *
* Setup_System_Config( ) *
* Configure PINMUX and other system module registers *
* *
* ------------------------------------------------------------------------ */
hotmenu
Setup_System_Config( )
{
GEL_TextOut( "Setup PINMUX Registers... " );
KICK0R = 0x83e70b13; // Kick0 register + data (unlock)
KICK1R = 0x95a4f1e0; // Kick1 register + data (unlock)
PINMUX0 = 0x11111188; // EMIFB, Check EMU0/RTCK
PINMUX1 = 0x11111111; // EMIFB
PINMUX2 = 0x11111111; // EMIFB
PINMUX3 = 0x11111111; // EMIFB
PINMUX4 = 0x11111111; // EMIFB
PINMUX5 = 0x11111111; // EMIFB
PINMUX6 = 0x11111111; // EMIFB
PINMUX7 = 0x11111111; // EMIFB, SPI0
PINMUX8 = 0x21122111; // UART2, McASP1, I2C0, I2C1
PINMUX9 = 0x11011112; // RMII CLK, McASP0, USB_DRVVBUS, UART2
PINMUX10 = 0x22222221; // RMII/ McASP0
PINMUX11 = 0x11112222; // McASP1, UART1, McASP0, MDIO (last 2 digits 0x22 for MDIO instead of GPIO)
PINMUX12 = 0x11111111; // McASP0 / McASP1
PINMUX13 = 0x22111111; // SD / McASP1
PINMUX14 = 0x88222222; // SD / EMIFA
PINMUX15 = 0x21888888; // SD / EMIFA
PINMUX16 = 0x11111112; // SD / EMIFA
PINMUX17 = 0x00100111; // EMIFA
PINMUX18 = 0x11111111; // EMIFA
PINMUX19 = 0x00000001; // EMIFA
// CHIP CONFIG 2 Register: Enable USB1 clock
CFGCHIP2 = 0x0000EB42; //USB0REF_FREQ=2 24 MHz, USB0PHY_PLLON=1 ,USB0PHYPWDN= 0
GEL_TextOut( "[Done]\n" );
}
/*Enable Function for PSC0*/
PSC0_lPSC_enableARM(unsigned int PD, unsigned int LPSC_num) {
*(unsigned int*) (PSC0_MDCTL+4*LPSC_num) = (*(unsigned int*) (PSC0_MDCTL+4*LPSC_num) & 0xFFFFFEE0) | 0x0103;
PSC0_PTCMD = 0x1<<PD;
while( (PSC0_PTSTAT & (0x1<<PD) ) !=0) ; /*Wait for power state transition to finish*/
while( (*(unsigned int*)(PSC0_MDSTAT+4 * LPSC_num) & 0x1F) !=0x3);
}
hotmenu Enable_ARM()
{
/* Turn on ARM RAM */
PSC0_lPSC_enable(0, 7);
/* Put branch to self at ARM vector table before releasing PSC */
*( unsigned int* )( 0xFFFF0000 ) = 0xEAFFFFFE;
*( unsigned int* )( 0xFFFF0004 ) = 0xEAFFFFFE;
*( unsigned int* )( 0xFFFF0008 ) = 0xEAFFFFFE;
*( unsigned int* )( 0xFFFF000C ) = 0xEAFFFFFE;
HOST0CFG = 0x00000001;
/* Turn on ARM */
PSC0_lPSC_enableARM(0, 14);
GEL_TextOut(" ARM Enabled\n");
}
/* ------------------------------------------------------------------------ *
* *
* Setup_Psc_All_On( ) *
* Enable all PSC modules on ALWAYSON and DSP power dominas. *
* *
* ------------------------------------------------------------------------ */
hotmenu
Setup_Psc_All_On( )
{
int i;
GEL_TextOut( "Setup Power Modules (All on)... " );
// PSC0
PSC0_lPSC_enable(0, 0);
PSC0_lPSC_enable(0, 1);
PSC0_lPSC_enable(0, 2);
PSC0_lPSC_enable(0, 3); // EMIFA
PSC0_lPSC_enable(0, 4);
PSC0_lPSC_enable(0, 5);
PSC0_lPSC_enable(0, 6);
PSC0_lPSC_enable(0, 8);
PSC0_lPSC_enable(0, 9);
PSC0_lPSC_enable(0, 10);
PSC0_lPSC_enable(0, 11);
PSC0_lPSC_enable(0, 12);
PSC0_lPSC_enable(0, 13);
// PSC1
PSC1_lPSC_enable(0, 1);
PSC1_lPSC_enable(0, 2);
PSC1_lPSC_enable(0, 3);
PSC1_lPSC_enable(0, 4);
PSC1_lPSC_enable(0, 5);
PSC1_lPSC_enable(0, 6); // EMIFB
PSC1_lPSC_enable(0, 7);
PSC1_lPSC_enable(0, 8);
PSC1_lPSC_enable(0, 9);
PSC1_lPSC_enable(0, 10);
PSC1_lPSC_enable(0, 11);
PSC1_lPSC_enable(0, 12);
PSC1_lPSC_enable(0, 13);
PSC1_lPSC_enable(0, 16);
PSC1_lPSC_enable(0, 17);
PSC1_lPSC_enable(0, 20);
PSC1_lPSC_enable(0, 21);
PSC1_lPSC_enable(0, 24);
PSC1_lPSC_enable(0, 25);
PSC1_lPSC_enable(0, 26);
PSC1_lPSC_enable(0, 31);
GEL_TextOut( "[Done]\n" );
}
/* ------------------------------------------------------------------------ *
* *
* Setup_EMIFA( ) *
* Setup Async-EMIF to the specified timings using either NAND Hw *
* controller or normal EMIF controller *
* *
* ------------------------------------------------------------------------ */
#define AEMIF_AWCCR *( unsigned int* )( 0x68000004 )
#define AEMIF_A1CR *( unsigned int* )( 0x68000010 )
#define AEMIF_A2CR *( unsigned int* )( 0x68000014 )
#define AEMIF_A3CR *( unsigned int* )( 0x68000018 )
#define AEMIF_A4CR *( unsigned int* )( 0x6800001C )
#define AEMIF_NANDFCR *( unsigned int* )( 0x68000060 )
Setup_EMIFA( )
{
/* Use extended wait cycles to keep CE low during NAND access */
AEMIF_AWCCR = 0xff;
/* Setup CS2 - 8-bit normal async */
AEMIF_A1CR = 0x00300608;
AEMIF_NANDFCR &= ~1;
/* Setup CS3 - 8-bit NAND */
AEMIF_A2CR = 0x00300388;
AEMIF_NANDFCR |= 2;
/* Setup CS4 - 8-bit normal async */
AEMIF_A3CR = 0x00a00504; // Setup=0, Strobe=A, Hold=0, TA=1, 8-bit
AEMIF_NANDFCR &= ~4;
/* Setup CS5 - 8-bit normal async */
AEMIF_A4CR = 0x00a00504; // Setup=0, Strobe=A, Hold=0, TA=1, 8-bit
AEMIF_NANDFCR &= ~8;
}
/* ------------------------------------------------------------------------ *
* *
* Setup_EMIFB( ) *
* Configure SDRAM. *
* *
* ------------------------------------------------------------------------ */
#define EMIFB_BASE 0xB0000000
#define EMIFB_SDSTAT *(unsigned int*)(EMIFB_BASE + 0x04) //SDRAM Status Register
#define EMIFB_SDCFG *(unsigned int*)(EMIFB_BASE + 0x08) //SDRAM Bank Config Register
#define EMIFB_SDREF *(unsigned int*)(EMIFB_BASE + 0x0C) //SDRAM Refresh Control Register
#define EMIFB_SDTIM1 *(unsigned int*)(EMIFB_BASE + 0x10) //SDRAM Timing Register
#define EMIFB_SDTIM2 *(unsigned int*)(EMIFB_BASE + 0x14) //SDRAM Timing Register
Setup_EMIFB()
{
// ISSI IS42S16160B-6BL SDRAM, 2 x 16M x 16 (32-bit data path), 133MHz
EMIFB_SDCFG = 0 // SDRAM Bank Config Register
|( 1 << 15) // Unlock timing registers
|( 2 << 9 ) // CAS latency is 2
|( 2 << 4 ) // 4 bank SDRAM devices
|( 1 << 0 ); // 512-word pages requiring 9 column address bits
EMIFB_SDREF = 0 // SDRAM Refresh Control Register
|( 0 << 31) // Low power mode disabled
|( 0 << 30) // MCLK stoping disabled
|( 0 << 23) // Selects self refresh instead of power down
|( 1040 <<0); // Refresh rate = 7812.5ns / 7.5ns
EMIFB_SDTIM1 = 0 // SDRAM Timing Register 1
|( 25 << 25) // (67.5ns / 7.55ns) - 1 = TRFC @ 133MHz
|( 2 << 22 ) // (20ns / 7.5ns) - 1 =TRP
|( 2 << 19 ) // (20ns / 7.5ns) - 1 = TRCD
|( 1 << 16 ) // (14ns / 7.5ns) - 1 = TWR
|( 5 << 11 ) // (45ns / 7.5ns) - 1 = TRAS
|( 8 << 6 ) // (67.5ns / 7.5ns) - 1 = TRC
|( 2 << 3 ); // *(((4 * 14ns) + (2 * 7.5ns)) / (4 * 7.5ns)) -1. = TRRD
// but it says to use this formula if 8 banks but only 4 are used here.
// and SDCFG1 register only suports upto 4 banks.
EMIFB_SDTIM2 = 0 // SDRAM Timing Register 2
|( 14<< 27) // not sure how they got this number. the datasheet says value should be
// "Maximum number of refresh_rate intervals from Activate to Precharge command"
// but has no equation. TRASMAX is 120k.
|( 9 << 16) // ( 70 / 7.5) - 1
|( 5 << 0 ); // ( 45 / 7.5 ) - 1
EMIFB_SDCFG = 0 // SDRAM Bank Config Register
|( 1 << 16)
|( 0 << 15) // Unlock timing registers
|( 2 << 9 ) // CAS latency is 2
|( 2 << 4 ) // 4 bank SDRAM devices
|( 1 << 0 ); // 512-word pages requiring 9 column address bits
/*Program the EMIF3C_SDRAM Controller*/
// EMIF3C_SDCFG = 0x00008421;
// EMIF3C_SDTIM1 = 0x10912A10;
// EMIF3C_SDTIM2 = 0x70090005;
// EMIF3C_SDREF = 0x410;
}