Part Number: AM5728
Tool/software: Linux
Hi,
I'm developing on am5728 a realtime linux OS.
I tried connecting a realtek network adapter to the PCIe slot and quickly discovered that there are known issues:
I'm using kernel 4.9.65 with rt-preempt patch. lspci shows nothing and dmesg shows errors:
root@am57xx-evm:~# dmesg | grep -i pci
[ 0.690382] PCI: CLS 0 bytes, default 64
[ 0.712427] dra7-pcie 51000000.pcie: Linked as a consumer to phy-4a094000.pciephy.3
[ 0.712591] dra7-pcie 51000000.pcie: GPIO lookup for consumer (null)
[ 0.712598] dra7-pcie 51000000.pcie: using device tree for GPIO lookup
[ 0.712627] dra7-pcie 51000000.pcie: lookup for GPIO (null) failed
[ 0.712635] dra7-pcie 51000000.pcie: gpio request failed, ret -517
[ 0.712770] dra7-pcie 51000000.pcie: Dropping the link to phy-4a094000.pciephy.3
[ 0.712802] dra7-pcie 51000000.pcie: probe deferral not supported
root@am57xx-evm:~#
Is there a remedy?
thanks a lot.