This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/PROCESSOR-SDK-DRA7X: DRA75X J6 EVM Rev H Wakeup 0 implementation.

Part Number: PROCESSOR-SDK-DRA7X


Tool/software: Linux

How to implement Wakeup on CAN message on TI J6 EVM.

Guidelines to implement RTC mode on TI J6.

How DCAN1_RX (AD17) configure to CAN rx and Wakeup 0 source.

  • Hi

    Assume that your questions are more at system level (and not necessarily Linux related)

    Would you expect the system to come out of Low Power state(and also elaborate on this) - are both RTC, CAN your intended wakeup sources

  • We dont support RTC mode on J6. So the way we see CAN wakeup is as below - 

    1. Device is OFF, PMIC has gated the power

     WUP on bus -> CAN TRCV detects it and uses inhibit/wakup pins to signal to PMIC which boot the device. In this mode, J6 does cold boot and responds to CAN message. We can discuss on CAN response time based on your system needs.

    2. Device is in standby, which means that the cores are in WFE/OFF. 

    We may not necessarily put the CAN TRCV in sleep mode. In case there is any activity on bus, the message comes to message RAM and an interrupt from CAN controller wakes up the core. This mode may not be as power friendly as previous.

    regards

    yashwant 

  • Hi
    let us know if you have any further clarifications. Marking the thread closed for now