Other Parts Discussed in Thread: TMS320DM6446
We are designing a board with a high memory bandwidth requirement and we have the following quesitons regarding the DM6446 for our board design.
Device: TMS320DM6446 594MHz, 297MHz
1) Is there another DaVinci device with 32-bit EMIF port (External Memory I/F)?
2) If not, what will be the best Bus Bandwidth for the EMIF port?
3) What is the maximum Bus Bandwidth for DDR2 port?
4) Can we utilize the EDMA to read data from an external memory device through EMIF port and write it into DDR2? How?
5) If code were to be executed from DDR2, will DDR2 port have enough Bus Bandwidth to handle both code execution and writing data into DDR2 memory?
6) I think code access to DDR2 should be cache refill, is that true?
Thanks,
Brian