Hi,
I'm using a DM365 EVM board which is hooked to a PC by it's ethernet port and a small switch.
What I'm trying to do is the same but by using the onboard mini-usb port, to be hooked (by USB cable) to one of the PC's USB ports.
My goal is to run the WEB SERVER supplied with the TI DVSDK software, so that the EVM may be accessed by an ordinary browser on the PC.
My questions are the following:
1. assuming the web-server is functional when using the RJ45 ethernet port (I haven't tested it yet), can it be altered to use the mini-usb port instead?
2. What do I need to do on the PC side so that an ordinary browser (e.g. MS-Internet Explorer or FireFox) can have access/connect to the EVM board using an USB port?
I'd appriciate any comments,
Thank you,
Danny