Other Parts Discussed in Thread: THS8200, THS8135, TVP5147M1, TVP7002
(((EDIT: NEVERMIND ALL THIS. The Spectrum Digital ADV7343 daughter card for the HD 1080P EVM includes SD (NTSC) Composite Out using the Analog Devices ADV7343 chip. This auxiliary reference design includes the circuit diagram and technical reference. See http://support.spectrumdigital.com/boards/evmdm6467t/revb/)))
I'm designing a new board, using as reference design the DM6467T EVM (Spectrum Digital calls it HD 1080P EVM). I'm designing multiple daughter card options for various video I/O formats. (This post is about SD-in/SD-out at this time, not format conversion.)
The HD 1080P EVM has an SD (Standard-Definition) Composite Input, but does *NOT* include an SD Composite Output. I'm trying to figure out the hardware to produce this from the DM6467T, which does not have built-in DACs like the DM6446 has.
I found a post at http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/99/p/6920/26839.aspx#26839 entitled "DM6467 VGA output" that implies I might be able to output SD Composite (one cable) with the same THS8200 that the HD 1080P EVM uses to output HD Component (three cable) (parens added to prevent readers from mis-reading Composite v. Component). Is this true? If so, is it the case that I can just design the board per my reference design's use of the THS8200 for HD Component, then later make software changes to get SD Composite out of it (and still make efficient use of the DM6467T's built-in abilities, rather than totally hard coding and custom handling the data to force out SD composite).
[I added this paragraph to my post before seeing Steve's response below.] While reading the THS8200 datasheet, I find it commenting "Its ITU-R.BT656 output port could be used to connect to an NTSC/PAL video encoder, such as the Texas Instruments TVP6000, for regular composite/S-video output". Two things. First, this implies the THS8200 can't produce SD Composite Output by itself using the same circuit as I find in the reference design. Second, I can't find the TVP6000 anywhere on focus.ti.com, although I do find an Analog Devices ADV7170/ADV7171 and could probably find others; yet I'm looking for a easy and fast development solution and all-TI might make it easier.
Please note that right now I'm in the schematic and board design phase. While I can save for later any suggestions about software, I don't have the mental bandwidth right now to focus on that. At this time, I just need to make sure I'm putting enough of the right hardware on the board.
Thanks very much for your help.
P.S. My boss demands I design the board before trying to do proof-of-concept on the EVM, so I don't have the liberty of simply trying it out on the EVM first.