Part Number: TDA2
Other Parts Discussed in Thread: INA226
Tool/software: TI-RTOS
Dear TI,
Understand a TI customized Caffe-Jacinto model is supported by TI, and "Only certain models" of Caffe and TensorFlow are supported. My questions are:
1) I can use official Caffe and TensorFlow model but only certain models can be used, correct? If this is true, what are these "certain models"?
2) For TensorFlow, Can you provide a example of the .txt file to use for the converting tool? e.g. in the current user guild, the below example is given for caffe:
tidl_model_import.out.exe ..\..\test\testvecs\config\import\tidl_import_jseg21.txt
inputNetFile = ..\..\test\testvecs\config\caffe_models\tiscapes_jseg21\jacintonet11.prototxt
inputParamsFile = ..\..\test\testvecs\config\caffe_models\tiscapes_jseg21\jacintonet11.caffemodel
What could be input files if using TensorFlow?
Thanks and best regards
He Wei