Other Parts Discussed in Thread: AM3715
Hi,
The following pins are separately listed as "VDDS" in AM3715's datasheet: AG20, AG21 and H28. However there is another group of pins also listed as "VDDS" that is explained as "1.8V power for standard IOs". Those pins include AD3/AD4/W4/AF8/AE8/AF16/AE16/AF23/AE23/F25/F26/AG27. What is the difference between the two groups of "VDDS"? Can they be tide together? Or must be separately treated? Any voltage difference on them?
Please advise.