Hi All,
I have a question on SDOFST register of 643x VPFE, on page 50 of document SPRU977a.

There are several fields in SDOFST and let’s take a look at LOFTS0:
“offset, in lines, between even lines on even fields (field 0)"
According to this and the bottom of the page, offset between even lines should be two lines.
By examining Fig. 20, one actually finds (only four lines are shown but we can infer from them arrangement of the following lines) that the offset between even lines are four lines.
Is this a mistake in expression? Because if we refer to page 132 where SDOFST fields are explained, LOFTS0 is “line offset values of even lines and even field ID=0”, rather than “between”.

By “between”, we mean between line (2k-2, 2k).
By “of”, we can either mean between (2k-2, 2k), or (2k-1, 2k).
Therefore although the use “of” still has ambiguity, its second interpretation makes sense.
Is this a mistake in the document's expression (especially with “between”)?
Sincerely,
Zheng