Other Parts Discussed in Thread: XIO2001
Hi,
Based on the c6454 datasheet:
"Once all the power supplies are within valid operating conditions, the POR pin must remain asserted (low) for a minimum of 256 CLKIN2 cycles. The PLL1 controller input clock, CLKIN1, and the PCI input clock, PCLK, must also be valid during this time. PCLK is only needed if the PCI module is being used."
In my case the PCI clock is provided by the XIO2001 bridge which holds the PCI clock as long as the PCI-e reset line is asserted (100msec'), long after the POR is de-asserted. Based on the requirement above, I need to hold the POR asserted after the PCI-e reset is de-asserted, however this will cause miss - enumeration of the DSP by the BIOS. Pls. explain.
Thanks,
Meir