Part Number: XEVMK2LX
Other Parts Discussed in Thread: RFSDK, DAC38J84, ADC14X250
Hi Joe
Thanks for the fast response. I notice that using the DFE will limit the throughput. In our application we do not necessarily need the DFE functionality. We would like to get raw data into the DSP (in a ping-pong buffer in memory) as fast as possible. We need a time synchronized dual ADC configuration (similar to IQ receiver).
What is the maximum dual ADC sample rate (12-14bit resolution) that can be used with the 66AK2L06 EVM. From the information provided it appears that we should be able to use all 4 Rx JESD lanes on the first FMC connector and get 737.28Msps per ADC channel in dual channel configuration. Is this correct? Is there a subsequent speed limitation at the IQN2 that will prevent this?
We also need a DAC in our system to be driven from the 66AK2L06 EVM. The DAC identified is DAC37J82. Can the DAC EVM be driven from the other FMC connector or do we need the deterministic latency card to get the DAC and ADC better synchronized?
Thank you