Part Number: DRA72
Tool/software: Linux
Team
We are trying to read MMCHS_xx registers using omapconf, but we are getting
omapconf read 0x480B4114
[ 58.369819] Unhandled fault: asynchronous external abort (0x1211) at 0x00000000
[ 58.377163] pgd = c9625cc0
[ 58.379878] [00000000] *pgd=89788003, *pmd=89763003, *pte=00000000
!!! OUPS... MEMORY ERROR @ 0x00000000 !!!
Are you sure that:
MEMORY ADDRESS IS VALID?
TARGETED MODULE IS CLOCKED?
or using
omapconf dump 0x480B4224 0x480B4228
[ 930.918438] Unhandled fault: asynchronous external abort (0x1211) at 0x00000000
[ 930.925783] pgd = cac49900
[ 930.928498] [00000000] *pgd=8c981003, *pmd=896ae003, *pte=00000000
!!! OUPS... MEMORY ERROR @ 0x00000000 !!!
Are you sure that:
MEMORY ADDRESS IS VALID?
TARGETED MODULE IS CLOCKED?
Version information
OMAPCONF (rev v1.73-19-gbe8626b built Thu Sep 21 14:28:34 CDT 2017)
....
Kernel:
Version: 4.4.91-00045-g9b0e56f-dirty
Author: christian@famar
Toolchain: gcc version 4.9.x 20150123 (prerelease) (GCC)
Type: #3 SMP PREEMPT
Date: Fri Aug 17 10:56:07 -03 2018
....
We try several MMC1 and MMC2 registers with the same results. (MMC2 is working, our system is there)
We can get MCASP, DSS or any other registers values
Is there any constraint for using omapconf with MMCx?
Regards