Part Number: TDA2PXEVM
Hi,
The sample file for the radar FFT heat map generates a target at about 20m. I have implemented a custom usecase which also does peak detection, beam forming, and object drawing for display on the radar object detection plot. However, when I feed the sample file to this usecase, the target doesn't show up since the plot is limited to 4m. How can I increase the range of the plot in order to display the target at 20m?
Thanks,
Richard