Dear Sir,
I already implemented the Ethernet function on 6437 EVM board with NDK, and would like to port it to 6431.
But the setting in ".gel" file and "DSP/BIOS Config" file really differ a lot. (Cache, RAM, SRAM, DDR2 ...)
In NDK's example, there is even SRAM in the memory setting within "DSP/BIOS Config" file.
I try to modify the .gel file & "DSP/BIOS Config" file and delete the SRAM in memory setting, but my project just doesn't work.
When I load the code & run, I can not see the code. I can only see lots of NOP assembly code.
Is there a guide to port Ethernet from 6437 to 6431?
Or is there a Ethernet sample code for 6431 DSP?
Or you have any sugesstion for my situation?
Really appreciate your help!!
Best Regards,
Eric Fang