Other Parts Discussed in Thread: AM3352, TPS65217
Tool/software: Linux
Goodmorning to all,
This is my first post, as explained by the title I'm trying to develop Qt application with Beaglebone. I've a little experience with Qt with EGFLS platform and yocto.
I've followed the steps described here:

I could have many questions, but I prefer to focus on the point that I reached. I have the ARAGO screen shown in the HDMI screen of Beaglebone black. I've cross compiled a simple Qt application and generated the .exe.
I followed the settings explained here (AM3 Beagle Bone Black Board Configuration):

When I run the helloWorld project, it doesn't show anything over the console, I get the following answer:
Using Wayland-EGL
wlpvr: PVR Services Initialised
Using the 'xdg-shell-v5' shell integration
I'd expect that the application screen would have appear over the console screen. Below some files that could help..
qt_env.sh
- ### QT Environment Variables ###
- export QT_QPA_EVDEV_TOUCHSCREEN_PARAMETERS="rotate=180"
- export SSL_CERT_FILE=/etc/ssl/certs/ca-certificates.crt
- export QT_QPA_EGLFS_KMS_CONFIG=/etc/qt5/eglfs_kms_cfg.json
- export QT_QPA_EGLFS_INTEGRATION=none
- export QT_WAYLAND_SHELL_INTEGRATION=xdg-shell-v5
wenston.ini
- [shell]
- locking=false
- animation=zoom
- panel-location=top
- startup-animation=fade
- [screensaver]
- # Uncomment path to disable screensaver
- #path=@libexecdir@/weston-screensaver
- gbm-format=rgb565 at section [core]
- [output]
- name=HDMI-A-1
- mode=1024x768
powervr.ini:
- [default]
- #WindowSystem=libpvrws_WAYLAND.so
- DefaultPixelFormat=RGB565
The modetest message is:
trying to open device 'i915'...failed
trying to open device 'amdgpu'...failed
trying to open device 'radeon'...failed
trying to open device 'nouveau'...failed
trying to open device 'vmwgfx'...failed
trying to open device 'omapdrm'...failed
trying to open device 'exynos'...failed
trying to open device 'tilcdc'...done
Encoders:
id crtc type possible crtcs possible clones
29 28 TMDS 0x00000001 0x00000000
Connectors:
id encoder status name size (mm) modes encoders
30 29 connected HDMI-A-1 510x290 25 29
modes:
name refresh (Hz) hdisp hss hse htot vdisp vss vse vtot)
1280x1024 60 1280 1328 1440 1688 1024 1025 1028 1066 108000 flags: phsync, pvs
ync; type: driver
1440x900 60 1440 1488 1520 1600 900 903 909 926 88750 flags: phsync, nvsync; t
ype: driver
1280x960 60 1280 1376 1488 1800 960 961 964 1000 108000 flags: phsync, pvsync;
type: driver
1280x800 60 1280 1328 1360 1440 800 803 809 823 71000 flags: phsync, nvsync; t
ype: driver
1152x864 75 1152 1216 1344 1600 864 865 868 900 108000 flags: phsync, pvsync;
type: driver
1280x720 60 1280 1390 1430 1650 720 725 730 750 74250 flags: phsync, pvsync; t
ype: driver
1280x720 60 1280 1390 1430 1650 720 725 730 750 74176 flags: phsync, pvsync; t
ype: driver
1280x720 50 1280 1720 1760 1980 720 725 730 750 74250 flags: phsync, pvsync; t
ype: driver
1024x768 75 1024 1040 1136 1312 768 769 772 800 78750 flags: phsync, pvsync; t
ype: driver
1024x768 70 1024 1048 1184 1328 768 771 777 806 75000 flags: nhsync, nvsync; t
ype: driver
1024x768 60 1024 1048 1184 1344 768 771 777 806 65000 flags: nhsync, nvsync; t
ype: driver
832x624 75 832 864 928 1152 624 625 628 667 57284 flags: nhsync, nvsync; type:
driver
800x600 75 800 816 896 1056 600 601 604 625 49500 flags: phsync, pvsync; type:
driver
800x600 72 800 856 976 1040 600 637 643 666 50000 flags: phsync, pvsync; type:
driver
800x600 60 800 840 968 1056 600 601 605 628 40000 flags: phsync, pvsync; type:
driver
800x600 56 800 824 896 1024 600 601 603 625 36000 flags: phsync, pvsync; type:
driver
720x576 50 720 732 796 864 576 581 586 625 27000 flags: nhsync, nvsync; type:
driver
720x480 60 720 736 798 858 480 489 495 525 27027 flags: nhsync, nvsync; type:
driver
720x480 60 720 736 798 858 480 489 495 525 27000 flags: nhsync, nvsync; type:
driver
640x480 75 640 656 720 840 480 481 484 500 31500 flags: nhsync, nvsync; type:
driver
640x480 73 640 664 704 832 480 489 492 520 31500 flags: nhsync, nvsync; type:
driver
640x480 67 640 704 768 864 480 483 486 525 30240 flags: nhsync, nvsync; type:
driver
640x480 60 640 656 752 800 480 490 492 525 25200 flags: nhsync, nvsync; type:
driver
640x480 60 640 656 752 800 480 490 492 525 25175 flags: nhsync, nvsync; type:
driver
720x400 70 720 738 846 900 400 412 414 449 28320 flags: nhsync, pvsync; type:
driver
props:
1 EDID:
flags: immutable blob
blobs:
value:
00ffffffffffff004c2dd40737343030
3015010380331d782a01f1a257529f27
0a5054bfef80714f8100814081809500
950fa940b300023a801871382d40582c
4500fd1e1100001e011d007251d01e20
6e285500fd1e1100001e000000fd0032
4b1f5111000a202020202020000000fc
00534d53323341333530480a202001cf
020313b14890041f051413120365030c
001000011d80d0721c1620102c2580fd
1e1100009e011d8018711c1620582c25
00fd1e1100009e011d00bc52d01e20b8
285540fd1e1100001e8c0ad090204031
200c405500fd1e110000188c0ad08a20
e02d10103e9600fd1e11000018000000
000000000000000000000000000000d4
2 DPMS:
flags: enum
enums: On=0 Standby=1 Suspend=2 Off=3
value: 0
5 link-status:
flags: enum
enums: Good=0 Bad=1
value: 0
CRTCs:
id fb pos size
28 34 (0,0) (1024x768)
1024x768 75 1024 1040 1136 1312 768 769 772 800 78750 flags: phsync, pvsync; t
ype: driver
props:
Planes:
id crtc fb CRTC x,y x,y gamma size possible crtcs
27 28 34 0,0 0,0 0 0x00000001
formats: RG16 BG24 XB24
props:
6 type:
flags: immutable enum
enums: Overlay=0 Primary=1 Cursor=2
value: 1
Frame buffers:
id size pitch
The dmesg of boot is:
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 4.14.40-g4796173fc5 (oe-user@oe-host) (gcc version
7.2.1 20171011 (Linaro GCC 7.2-2017.11)) #1 PREEMPT Wed Jul 25 15:43:15 UTC 2018
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instructio
n cache
[ 0.000000] OF: fdt: Machine model: TI AM335x BeagleBone Black
[ 0.000000] Memory policy: Data cache writeback
[ 0.000000] efi: Getting EFI parameters from FDT:
[ 0.000000] efi: UEFI not found.
[ 0.000000] cma: Reserved 48 MiB at 0x9d000000
[ 0.000000] On node 0 totalpages: 131072
[ 0.000000] free_area_init_node: node 0, pgdat c0d4d25c, node_mem_map dcb6100
0
[ 0.000000] Normal zone: 1152 pages used for memmap
[ 0.000000] Normal zone: 0 pages reserved
[ 0.000000] Normal zone: 131072 pages, LIFO batch:31
[ 0.000000] CPU: All CPU(s) started in SVC mode.
[ 0.000000] AM335X ES2.1 (sgx neon)
[ 0.000000] pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768
[ 0.000000] pcpu-alloc: [0] 0
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 129920
[ 0.000000] Kernel command line: console=ttyO0,115200n8 video=HDMI-A-1:1024x7
68 root=PARTUUID=a63a8d29-02 rw rootfstype=ext4 rootwait
[ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Memory: 456920K/524288K available (8192K kernel code, 318K rwdata
, 2488K rodata, 1024K init, 275K bss, 18216K reserved, 49152K cma-reserved, 0K h
ighmem)
[ 0.000000] Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
vmalloc : 0xe0800000 - 0xff800000 ( 496 MB)
lowmem : 0xc0000000 - 0xe0000000 ( 512 MB)
pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
.text : 0xc0008000 - 0xc0900000 (9184 kB)
.init : 0xc0c00000 - 0xc0d00000 (1024 kB)
.data : 0xc0d00000 - 0xc0d4fb08 ( 319 kB)
.bss : 0xc0d4fb08 - 0xc0d948bc ( 276 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] Tasks RCU enabled.
[ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrup
ts
[ 0.000000] OMAP clockevent source: timer2 at 24000000 Hz
[ 0.000015] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478
484971ns
[ 0.000033] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max
_idle_ns: 79635851949 ns
[ 0.000042] OMAP clocksource: timer1 at 24000000 Hz
[ 0.000198] timer_probe: no matching timers found
[ 0.000384] Console: colour dummy device 80x30
[ 0.000410] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
[ 0.000417] This ensures that you still see kernel messages. Please
[ 0.000422] update your kernel commandline.
[ 0.000448] Calibrating delay loop... 996.14 BogoMIPS (lpj=4980736)
[ 0.089202] pid_max: default: 32768 minimum: 301
[ 0.089366] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.089379] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.090074] CPU: Testing write buffer coherency: ok
[ 0.090702] Setting up static identity map for 0x80100000 - 0x80100060
[ 0.090836] Hierarchical SRCU implementation.
[ 0.091117] EFI services will not be available.
[ 0.092269] devtmpfs: initialized
[ 0.099343] random: get_random_u32 called from bucket_table_alloc+0x8c/0x1ac
with crng_init=0
[ 0.099763] VFP support v0.3: implementor 41 architecture 3 part 30 variant c
rev 3
[ 0.100042] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, ma
x_idle_ns: 19112604462750000 ns
[ 0.100062] futex hash table entries: 256 (order: -1, 3072 bytes)
[ 0.103339] pinctrl core: initialized pinctrl subsystem
[ 0.104000] DMI not present or invalid.
[ 0.104380] NET: Registered protocol family 16
[ 0.106346] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.118670] omap_hwmod: debugss: _wait_target_disable failed
[ 0.170800] cpuidle: using governor ladder
[ 0.170831] cpuidle: using governor menu
[ 0.174444] gpio gpiochip0: (gpio): added GPIO chardev (254:0)
[ 0.174524] gpiochip_setup_dev: registered GPIOs 0 to 31 on device: gpiochip0
(gpio)
[ 0.174583] OMAP GPIO hardware version 0.1
[ 0.175279] gpio gpiochip1: (gpio): added GPIO chardev (254:1)
[ 0.175350] gpiochip_setup_dev: registered GPIOs 32 to 63 on device: gpiochip
1 (gpio)
[ 0.175994] gpio gpiochip2: (gpio): added GPIO chardev (254:2)
[ 0.176064] gpiochip_setup_dev: registered GPIOs 64 to 95 on device: gpiochip
2 (gpio)
[ 0.176695] gpio gpiochip3: (gpio): added GPIO chardev (254:3)
[ 0.176781] gpiochip_setup_dev: registered GPIOs 96 to 127 on device: gpiochi
p3 (gpio)
[ 0.183357] No ATAGs?
[ 0.183375] hw-breakpoint: debug architecture 0x4 unsupported.
[ 0.194637] edma 49000000.edma: TI EDMA DMA engine driver
[ 0.194998] of_get_named_gpiod_flags: can't parse 'gpio' property of node '/f
ixedregulator0[0]'
[ 0.197255] omap_i2c 44e0b000.i2c: could not find pctldev for node /ocp/l4_wk
up@44c00000/scm@210000/pinmux@800/pinmux_i2c0_pins, deferring probe
[ 0.197319] omap_i2c 4819c000.i2c: could not find pctldev for node /ocp/l4_wk
up@44c00000/scm@210000/pinmux@800/pinmux_i2c2_pins, deferring probe
[ 0.197427] media: Linux media interface: v0.10
[ 0.197464] Linux video capture interface: v2.00
[ 0.197560] pps_core: LinuxPPS API ver. 1 registered
[ 0.197568] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giome
tti <giometti@linux.it>
[ 0.197588] PTP clock support registered
[ 0.197618] EDAC MC: Ver: 3.0.0
[ 0.198068] dmi: Firmware registration failed.
[ 0.198437] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
[ 0.198716] Advanced Linux Sound Architecture Driver Initialized.
[ 0.199924] clocksource: Switched to clocksource timer1
[ 0.206999] NET: Registered protocol family 2
[ 0.207658] TCP established hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.207704] TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.207742] TCP: Hash tables configured (established 4096 bind 4096)
[ 0.207829] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.207846] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.207970] NET: Registered protocol family 1
[ 0.208363] RPC: Registered named UNIX socket transport module.
[ 0.208374] RPC: Registered udp transport module.
[ 0.208380] RPC: Registered tcp transport module.
[ 0.208386] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.208399] PCI: CLS 0 bytes, default 64
[ 0.209444] hw perfevents: no interrupt-affinity property for /pmu, guessing.
[ 0.209565] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counter
s available
[ 0.210950] workingset: timestamp_bits=14 max_order=17 bucket_order=3
[ 0.214577] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.215260] NFS: Registering the id_resolver key type
[ 0.215302] Key type id_resolver registered
[ 0.215308] Key type id_legacy registered
[ 0.215352] ntfs: driver 2.1.32 [Flags: R/O].
[ 0.217045] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 2
45)
[ 0.217063] io scheduler noop registered
[ 0.217071] io scheduler deadline registered
[ 0.217251] io scheduler cfq registered (default)
[ 0.217261] io scheduler mq-deadline registered
[ 0.217268] io scheduler kyber registered
[ 0.218423] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568
[ 0.220674] of_get_named_gpiod_flags: parsed 'enable-gpios' property of node
'/clk_mcasp0[0]' - status (0)
[ 0.262173] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled
[ 0.264877] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 30, base_baud =
3000000) is a 8250
[ 0.896098] console [ttyS0] enabled
[ 0.901295] omap_rng 48310000.rng: Random Number Generator ver. 20
[ 0.917002] brd: module loaded
[ 0.925905] loop: module loaded
[ 0.931011] mdio_bus fixed-0: GPIO lookup for consumer reset
[ 0.931023] mdio_bus fixed-0: using lookup tables for GPIO lookup
[ 0.931030] mdio_bus fixed-0: lookup for GPIO reset failed
[ 0.931051] libphy: Fixed MDIO Bus: probed
[ 0.950254] mdio_bus 4a101000.mdio: GPIO lookup for consumer reset
[ 0.950265] mdio_bus 4a101000.mdio: using lookup tables for GPIO lookup
[ 0.950272] mdio_bus 4a101000.mdio: lookup for GPIO reset failed
[ 1.009989] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6, bus freq 1
000000
[ 1.017690] davinci_mdio 4a101000.mdio: detected phy mask fffffffe
[ 1.025043] libphy: 4a101000.mdio: probed
[ 1.029083] davinci_mdio 4a101000.mdio: phy[0]: device 4a101000.mdio:00, driv
er SMSC LAN8710/LAN8720
[ 1.039121] cpsw 4a100000.ethernet: Detected MACID = e8:eb:11:27:b9:2b
[ 1.045881] cpsw 4a100000.ethernet: initialized cpsw ale version 1.4
[ 1.052352] cpsw 4a100000.ethernet: ALE Table size 1024
[ 1.057638] cpsw 4a100000.ethernet: cpts: overflow check period 500 (jiffies)
[ 1.066070] i2c /dev entries driver
[ 1.070099] IR NEC protocol handler initialized
[ 1.074655] IR RC5(x/sz) protocol handler initialized
[ 1.079723] IR RC6 protocol handler initialized
[ 1.084292] IR JVC protocol handler initialized
[ 1.088838] IR Sony protocol handler initialized
[ 1.093483] IR SANYO protocol handler initialized
[ 1.098204] IR Sharp protocol handler initialized
[ 1.102934] IR MCE Keyboard/mouse protocol handler initialized
[ 1.108788] IR XMP protocol handler initialized
[ 1.114700] cpuidle: enable-method property 'ti,am3352' found operations
[ 1.121819] sdhci: Secure Digital Host Controller Interface driver
[ 1.128027] sdhci: Copyright(c) Pierre Ossman
[ 1.132977] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 1.132984] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 1.133016] of_get_named_gpiod_flags: parsed 'cd-gpios' property of node '/oc
p/mmc@48060000[0]' - status (0)
[ 1.133081] omap_hsmmc 48060000.mmc: Got CD GPIO
[ 1.137728] omap_hsmmc 48060000.mmc: GPIO lookup for consumer wp
[ 1.137732] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 1.137741] of_get_named_gpiod_flags: can't parse 'wp-gpios' property of node
'/ocp/mmc@48060000[0]'
[ 1.137748] of_get_named_gpiod_flags: can't parse 'wp-gpio' property of node
'/ocp/mmc@48060000[0]'
[ 1.137753] omap_hsmmc 48060000.mmc: using lookup tables for GPIO lookup
[ 1.137761] omap_hsmmc 48060000.mmc: lookup for GPIO wp failed
[ 1.190717] omap_hsmmc 481d8000.mmc: GPIO lookup for consumer cd
[ 1.190729] omap_hsmmc 481d8000.mmc: using device tree for GPIO lookup
[ 1.190744] of_get_named_gpiod_flags: can't parse 'cd-gpios' property of node
'/ocp/mmc@481d8000[0]'
[ 1.190751] of_get_named_gpiod_flags: can't parse 'cd-gpio' property of node
'/ocp/mmc@481d8000[0]'
[ 1.190757] omap_hsmmc 481d8000.mmc: using lookup tables for GPIO lookup
[ 1.190763] omap_hsmmc 481d8000.mmc: lookup for GPIO cd failed
[ 1.190772] omap_hsmmc 481d8000.mmc: GPIO lookup for consumer wp
[ 1.190777] omap_hsmmc 481d8000.mmc: using device tree for GPIO lookup
[ 1.190783] of_get_named_gpiod_flags: can't parse 'wp-gpios' property of node
'/ocp/mmc@481d8000[0]'
[ 1.190790] of_get_named_gpiod_flags: can't parse 'wp-gpio' property of node
'/ocp/mmc@481d8000[0]'
[ 1.190795] omap_hsmmc 481d8000.mmc: using lookup tables for GPIO lookup
[ 1.190800] omap_hsmmc 481d8000.mmc: lookup for GPIO wp failed
[ 1.237078] mmc0: host does not support reading read-only switch, assuming wr
ite-enable
[ 1.247064] mmc0: new high speed SDHC card at address 0007
[ 1.252816] sdhci-pltfm: SDHCI platform and OF driver helper
[ 1.253468] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds/
led2[0]' - status (0)
[ 1.253480] no flags found for gpios
[ 1.253615] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds/
led3[0]' - status (0)
[ 1.253622] no flags found for gpios
[ 1.253722] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds/
led4[0]' - status (0)
[ 1.253727] no flags found for gpios
[ 1.253810] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds/
led5[0]' - status (0)
[ 1.253815] no flags found for gpios
[ 1.254166] ledtrig-cpu: registered to indicate activity on CPUs
[ 1.263480] NET: Registered protocol family 10
[ 1.264555] Segment Routing with IPv6
[ 1.264622] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[ 1.265220] NET: Registered protocol family 17
[ 1.265471] Key type dns_resolver registered
[ 1.265669] omap_voltage_late_init: Voltage driver support not added
[ 1.306361] mmcblk0: mmc0:0007 Y16AG 14.5 GiB
[ 1.314004] mmcblk0: p1 p2
[ 1.344335] random: fast init done
[ 1.352985] tps65217 0-0024: TPS65217 ID 0xe version 1.2
[ 1.358948] at24 0-0050: 32768 byte 24c256 EEPROM, writable, 1 bytes/write
[ 1.370253] mmc1: new high speed MMC card at address 0001
[ 1.376189] mmcblk1: mmc1:0001 M62704 3.56 GiB
[ 1.380981] mmcblk1boot0: mmc1:0001 M62704 partition 1 2.00 MiB
[ 1.387064] mmcblk1boot1: mmc1:0001 M62704 partition 2 2.00 MiB
[ 1.393156] mmcblk1rpmb: mmc1:0001 M62704 partition 3 512 KiB
[ 1.502180] tda998x 0-0070: found TDA19988
[ 1.507433] tilcdc 4830e000.lcdc: bound 0-0070 (ops tda998x_ops)
[ 1.513537] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 1.520194] [drm] No driver support for vblank timestamp query.
[ 1.630598] Console: switching to colour frame buffer device 128x48
[ 1.650161] tilcdc 4830e000.lcdc: fb0: frame buffer device
[ 1.656306] [drm] Initialized tilcdc 1.0.0 20121205 for 4830e000.lcdc on mino
r 0
[ 1.663950] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz
[ 1.790996] omap_i2c 4819c000.i2c: bus 2 rev0.11 at 100 kHz
[ 1.798637] hctosys: unable to open rtc device (rtc0)
[ 1.804366] ALSA device list:
[ 1.807356] No soundcards found.
[ 1.846719] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. O
pts: (null)
[ 1.855121] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 1.864508] devtmpfs: mounted
[ 1.869890] Freeing unused kernel memory: 1024K
[ 2.306496] systemd[1]: System time before build time, advancing clock.
[ 2.376374] systemd[1]: systemd 234 running in system mode. (+PAM -AUDIT -SEL
INUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +
XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN default-hierarchy=hybrid)
[ 2.398125] systemd[1]: Detected architecture arm.
[ 2.443396] systemd[1]: Set hostname to <am335x-evm>.
[ 2.845220] systemd[1]: /lib/systemd/system/gadget-init.service:15: Unknown l
value 'ExecStopPre' in section 'Service'
[ 3.141504] random: systemd: uninitialized urandom read (16 bytes read)
[ 3.148660] systemd[1]: Listening on Syslog Socket.
[ 3.180247] random: systemd: uninitialized urandom read (16 bytes read)
[ 3.189749] systemd[1]: Created slice User and Session Slice.
[ 3.282484] random: systemd: uninitialized urandom read (16 bytes read)
[ 3.304246] systemd[1]: Listening on Process Core Dump Socket.
[ 3.340723] systemd[1]: Listening on udev Kernel Socket.
[ 3.372907] systemd[1]: Listening on /dev/initctl Compatibility Named Pipe.
[ 3.412934] systemd[1]: Listening on Journal Socket.
[ 3.687909] cryptodev: loading out-of-tree module taints kernel.
[ 3.697333] cryptodev: driver 1.9 loaded.
[ 3.747108] usbcore: registered new interface driver usbfs
[ 3.757662] usbcore: registered new interface driver hub
[ 3.765980] usbcore: registered new device driver usb
[ 3.783218] usbcore: registered new interface driver usbserial
[ 3.865728] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
[ 4.641160] systemd-journald[76]: Received request to flush runtime journal f
rom PID 1
[ 6.651995] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 6.740803] omap_rtc 44e3e000.rtc: already running
[ 6.783233] omap_rtc 44e3e000.rtc: char device (253:0)
[ 6.783405] omap_rtc 44e3e000.rtc: registered as rtc0
[ 8.264903] omap-sham 53100000.sham: hw accel on OMAP rev 4.3
[ 8.274630] remoteproc remoteproc0: wkup_m3 is available
[ 8.287827] remoteproc remoteproc0: powering up wkup_m3
[ 8.353109] PM: Cannot get wkup_m3_ipc handle
[ 8.365168] remoteproc remoteproc0: Booting fw image am335x-pm-firmware.elf,
size 224628
[ 8.365418] remoteproc remoteproc0: remote processor wkup_m3 is now up
[ 8.365448] wkup_m3_ipc 44e11324.wkup_m3_ipc: CM3 Firmware Version = 0x192
[ 8.644039] PM: bootloader does not support rtc-only!
[ 8.652959] [drm] Initialized pvr 1.14.3699939 20110701 for 56000000.sgx on m
inor 1
[ 8.654567] omap-aes 53500000.aes: OMAP AES hw accel rev: 3.2
[ 8.673410] omap-aes 53500000.aes: will run requests pump with realtime prior
ity
[ 8.882039] hdmi-audio-codec hdmi-audio-codec.0.auto: ASoC: no source widget
found for Playback
[ 8.882050] hdmi-audio-codec hdmi-audio-codec.0.auto: ASoC: Failed to add rou
te Playback -> direct -> TX
[ 8.882149] of_get_named_gpiod_flags: can't parse 'simple-audio-card,hp-det-g
pio' property of node '/sound[0]'
[ 8.882157] of_get_named_gpiod_flags: can't parse 'simple-audio-card,mic-det-
gpio' property of node '/sound[0]'
[ 9.068520] asoc-simple-card sound: i2s-hifi <-> 48038000.mcasp mapping ok
[ 9.118601] asoc-simple-card sound: ASoC: no DMI vendor name!
[ 9.687652] random: crng init done
[ 9.807267] random: 7 urandom warning(s) missed due to ratelimiting
[ 11.813144] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data
may be corrupt. Please run fsck.
[ 11.951965] net eth0: initializing cpsw version 1.12 (0)
[ 12.061268] SMSC LAN8710/LAN8720 4a101000.mdio:00: attached PHY driver [SMSC
LAN8710/LAN8720] (mii_bus:phy_addr=4a101000.mdio:00, irq=POLL)
[ 12.285811] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[ 14.321366] cpsw 4a100000.ethernet eth0: Link is Up - 100Mbps/Full - flow con
trol rx/tx
[ 14.419251] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
[ 14.643332] udc-core: couldn't find an available UDC - added [g_multi] to lis
t of pending drivers
[ 15.423726] am335x-phy-driver 47401300.usb-phy: GPIO lookup for consumer rese
t
[ 15.423742] am335x-phy-driver 47401300.usb-phy: using device tree for GPIO lo
okup
[ 15.423764] of_get_named_gpiod_flags: can't parse 'reset-gpios' property of n
ode '/ocp/usb@47400000/usb-phy@47401300[0]'
[ 15.423773] of_get_named_gpiod_flags: can't parse 'reset-gpio' property of no
de '/ocp/usb@47400000/usb-phy@47401300[0]'
[ 15.423779] am335x-phy-driver 47401300.usb-phy: using lookup tables for GPIO
lookup
[ 15.423787] am335x-phy-driver 47401300.usb-phy: lookup for GPIO reset failed
[ 15.423795] am335x-phy-driver 47401300.usb-phy: GPIO lookup for consumer vbus
-detect
[ 15.423800] am335x-phy-driver 47401300.usb-phy: using device tree for GPIO lo
okup
[ 15.423807] of_get_named_gpiod_flags: can't parse 'vbus-detect-gpios' propert
y of node '/ocp/usb@47400000/usb-phy@47401300[0]'
[ 15.423814] of_get_named_gpiod_flags: can't parse 'vbus-detect-gpio' property
of node '/ocp/usb@47400000/usb-phy@47401300[0]'
[ 15.423819] am335x-phy-driver 47401300.usb-phy: using lookup tables for GPIO
lookup
[ 15.423825] am335x-phy-driver 47401300.usb-phy: lookup for GPIO vbus-detect f
ailed
[ 15.423902] am335x-phy-driver 47401300.usb-phy: 47401300.usb-phy supply vcc n
ot found, using dummy regulator
[ 15.723632] using random self ethernet address
[ 15.728150] using random host ethernet address
[ 15.808742] using host ethernet address: E8:EB:11:27:B9:2D
[ 15.808807] using random self ethernet address
[ 15.932163] using random host ethernet address
[ 16.059470] using host ethernet address: E8:EB:11:27:B9:2D
[ 16.083136] usb0: HOST MAC e8:eb:11:27:b9:2d
[ 16.196758] usb0: MAC 6e:1e:47:a1:5d:20
[ 16.363847] Mass Storage Function, version: 2009/09/11
[ 16.369061] LUN: removable file: (no medium)
[ 16.460720] LUN: removable read only file: /dev/mmcblk0p1
[ 16.525480] Number of LUNs=1
[ 16.567609] g_multi gadget: Multifunction Composite Gadget
[ 16.626610] g_multi gadget: g_multi ready
[ 16.678566] am335x-phy-driver 47401b00.usb-phy: GPIO lookup for consumer rese
t
[ 16.678579] am335x-phy-driver 47401b00.usb-phy: using device tree for GPIO lo
okup
[ 16.678597] of_get_named_gpiod_flags: can't parse 'reset-gpios' property of n
ode '/ocp/usb@47400000/usb-phy@47401b00[0]'
[ 16.678606] of_get_named_gpiod_flags: can't parse 'reset-gpio' property of no
de '/ocp/usb@47400000/usb-phy@47401b00[0]'
[ 16.678613] am335x-phy-driver 47401b00.usb-phy: using lookup tables for GPIO
lookup
[ 16.678621] am335x-phy-driver 47401b00.usb-phy: lookup for GPIO reset failed
[ 16.678629] am335x-phy-driver 47401b00.usb-phy: GPIO lookup for consumer vbus
-detect
[ 16.678634] am335x-phy-driver 47401b00.usb-phy: using device tree for GPIO lo
okup
[ 16.678641] of_get_named_gpiod_flags: can't parse 'vbus-detect-gpios' propert
y of node '/ocp/usb@47400000/usb-phy@47401b00[0]'
[ 16.678648] of_get_named_gpiod_flags: can't parse 'vbus-detect-gpio' property
of node '/ocp/usb@47400000/usb-phy@47401b00[0]'
[ 16.678654] am335x-phy-driver 47401b00.usb-phy: using lookup tables for GPIO
lookup
[ 16.678659] am335x-phy-driver 47401b00.usb-phy: lookup for GPIO vbus-detect f
ailed
[ 16.678740] am335x-phy-driver 47401b00.usb-phy: 47401b00.usb-phy supply vcc n
ot found, using dummy regulator
[ 16.816022] musb-hdrc musb-hdrc.1: MUSB HDRC host driver
[ 16.913207] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus numbe
r 1
[ 16.997354] hub 1-0:1.0: USB hub found
[ 17.031053] hub 1-0:1.0: 1 port detected
[ 17.148922] g_multi gadget: high-speed config #2: Multifunction with CDC ECM
[ 17.570106] usb 1-1: new full-speed USB device number 2 using musb-hdrc
[ 18.055891] pruss 4a300000.pruss: creating PRU cores and other child platform
devices
[ 18.768786] remoteproc remoteproc1: 4a334000.pru is available
[ 18.833385] pru-rproc 4a334000.pru: PRU rproc node /ocp/pruss_soc_bus@4a32600
4/pruss@0/pru@34000 probed successfully
[ 18.925025] remoteproc remoteproc2: 4a338000.pru is available
[ 18.966331] pru-rproc 4a338000.pru: PRU rproc node /ocp/pruss_soc_bus@4a32600
4/pruss@0/pru@38000 probed successfully
[ 19.656047] input: Microsoft Microsoft\xffffffc2\xffffffae 2.4GHz Transceiver
v8.0 as /devices/platform/ocp/47400000.usb/47401c00.usb/musb-hdrc.1/usb1/1-1/1-
1:1.0/0003:045E:0745.0001/input/input0
[ 19.773623] hid-generic 0003:045E:0745.0001: input: USB HID v1.11 Keyboard [M
icrosoft Microsoft\xffffffc2\xffffffae 2.4GHz Transceiver v8.0] on usb-musb-hdrc
.1-1/input0
[ 19.846316] input: Microsoft Microsoft\xffffffc2\xffffffae 2.4GHz Transceiver
v8.0 as /devices/platform/ocp/47400000.usb/47401c00.usb/musb-hdrc.1/usb1/1-1/1-
1:1.1/0003:045E:0745.0002/input/input1
[ 19.961359] hid-generic 0003:045E:0745.0002: input: USB HID v1.11 Mouse [Micr
osoft Microsoft\xffffffc2\xffffffae 2.4GHz Transceiver v8.0] on usb-musb-hdrc.1-
1/input1
[ 20.078099] input: Microsoft Microsoft\xffffffc2\xffffffae 2.4GHz Transceiver
v8.0 as /devices/platform/ocp/47400000.usb/47401c00.usb/musb-hdrc.1/usb1/1-1/1-
1:1.2/0003:045E:0745.0003/input/input2
[ 20.223790] hid-generic 0003:045E:0745.0003: input: USB HID v1.11 Device [Mic
rosoft Microsoft\xffffffc2\xffffffae 2.4GHz Transceiver v8.0] on usb-musb-hdrc.1
-1/input2
[ 20.278168] usbcore: registered new interface driver usbhid
[ 20.307312] usbhid: USB HID core driver
[ 22.362613] PVR_K: UM DDK-(3699939) and KM DDK-(3699939) match. [ OK ]
[ 28.263176] hrtimer: interrupt took 188334 ns
[ 135.481183] NET: Registered protocol family 15
[ 136.668494] Initializing XFRM netlink socket