Part Number: AM5728
Other Parts Discussed in Thread: DRA752, BEAGLEBOARD-X15, , PMP
Tool/software: Linux
Hello support,
I am using : Ubuntu 14.04; clean install of SDK 5.0
my connections are : VMWare Ubuntu --> AP/router --> EVM.
I've tried static and dhcp ip addresses
Question: why is ipaddr needed if i'm setup for DHCP?
Question: where does u-boot get the names of zImage, DTB, etc?
Question: what am i missing?
I am using the following TFT and NFS setup files:
# /etc/default/tftpd-hpa
TFTP_USERNAME="tftp"
TFTP_DIRECTORY="/home/marc/ti-sdk05-am57xx-evm/filesystem/boot"
TFTP_ADDRESS=":69"
TFTP_OPTIONS="--secure --create --listen"
RUN_DEAMON="yes"
marc@ubuntu:~$ cat /etc/exports
# /etc/exports: the access control list for filesystems which may be exported
/home/marc/ti-sdk05-am57xx-evm/filesystem *(rw,nohide,insecure,no_subtree_check,async,no_root_squash)
/home/marc/ti-sdk05-am57xx-evm/targetNFS *(rw,nohide,insecure,no_subtree_check,async,no_root_squash)
I've restarted TFTP and NFS servers:
TFTP : sudo /etc/init.d/tftpd-hpa restart
NFS : sudo /etc/init.d/nfs-kernel-server restart
Using out-of-box u-boot settings with the following additions
setenv autoload no
setenv serverip 192.168.1.101
setenv rootpath /home/marc/ti-sdk05-am57xx-evm/filesystem
setenv nfsopts 'nolock,proto=udp'
setenv myargs 'setenv bootargs console=${console} ${optargs} root=/dev/nfs nfsroot=${serverip}:${rootpath},${nfsopts} rw ip=dhcp earlyprintk'
setenv uenvcmd dhcp; tftp ${loadaddr}; run myargs; tftp ${fdtaddr} ${fdtfile}; bootz ${loadaddr} - ${fdtaddr}
#setenv fdtfile devicetree-zImage-am57xx-evm-reva3.dtb
#setenv filename zImage
printenv output
=>
arch=arm
args_mmc=run finduuid;setenv bootargs console=${console} ${optargs} root=PARTUUID=${uuid} rw rootfstype=${mmcrootfstype}
autoload=no
baudrate=115200
board=am57xx
board_name=am57xx_evm
board_rev=A.20
board_serial=40154P550164
boot_fdt=try
boot_fit=0
bootargs=console=ttyO2,115200n8 root=/dev/nfs nfsroot=192.168.1.101:/home/marc/ti-sdk05-am57xx-evm/filesystem,nolock,proto=udp rw ip=dhcp earlyprintk
bootcmd=run findfdt; run getuenv; setenv autoload no;dhcp ;tftp ${loadaddr} zImage-am57xx-evm.bin; tftp ${fdtaddr} ${fdtfile}; run netargs; bootz ${loadaddr} - ${fdtaddr}
bootdelay=2
bootdir=/boot
bootenvfile=uEnv.txt
bootfile=zImage-am57xx-evm.bin
bootm_size=0x10000000
bootpart=0:2
bootscript=echo Running bootscript from mmc${mmcdev} ...; source ${loadaddr}
console=ttyO2,115200n8
cpu=armv7
dfu_alt_info_emmc=rawemmc raw 0 3751936;boot part 1 1;rootfs part 1 2;MLO fat 1 1;MLO.raw raw 0x100 0x100;u-boot.img.raw raw 0x300 0x1000;u-env.raw raw 0x1300 0x200;spl-os-args.raw raw 0x1500 0x200;spl-os-image.raw raw 0x1700 0x6900;spl-os-args fat 1 1;spl-os-image fat 1 1;u-boot.img fat 1 1;uEnv.txt fat 1 1
dfu_alt_info_mmc=boot part 0 1;rootfs part 0 2;MLO fat 0 1;MLO.raw raw 0x100 0x100;u-boot.img.raw raw 0x300 0x1000;u-env.raw raw 0x1300 0x200;spl-os-args.raw raw 0x1500 0x200;spl-os-image.raw raw 0x1700 0x6900;spl-os-args fat 0 1;spl-os-image fat 0 1;u-boot.img fat 0 1;uEnv.txt fat 0 1
dfu_alt_info_ram=kernel ram 0x80200000 0x4000000;fdt ram 0x80f80000 0x80000;ramdisk ram 0x81000000 0x4000000
dfu_bufsiz=0x10000
dofastboot=0
emmc_android_boot=echo Trying to boot Android from eMMC ...; run update_to_fit; setenv eval_bootargs setenv bootargs $bootargs; run eval_bootargs; setenv mmcdev 1; setenv fdt_part 3; setenv boot_part 9; setenv machid fe6; mmc dev $mmcdev; mmc rescan; part start mmc ${mmcdev} ${fdt_part} fdt_start; part size mmc ${mmcdev} ${fdt_part} fdt_size; part start mmc ${mmcdev} ${boot_part} boot_start; part size mmc ${mmcdev} ${boot_part} boot_size; mmc read ${fdtaddr} ${fdt_start} ${fdt_size}; mmc read ${loadaddr} ${boot_start} ${boot_size}; bootm ${loadaddr}#${fdtfile};
emmc_linux_boot=echo Trying to boot Linux from eMMC ...; setenv mmcdev 1; setenv bootpart 1:2; setenv mmcroot /dev/mmcblk0p2 rw; run mmcboot;
envboot=mmc dev ${mmcdev}; if mmc rescan; then echo SD/MMC found on device ${mmcdev};if run loadbootscript; then run bootscript;else if run loadbootenv; then echo Loaded env from ${bootenvfile};run importbootenv;fi;if test -n $uenvcmd; then echo Running uenvcmd ...;run uenvcmd;fi;fi;fi;
ethact=ethernet@48484000
ethaddr=74:da:ea:47:b8:ca
fastboot.board_rev=A.20
fastboot.cpu=DRA752
fastboot.secure=GP
fdt_addr_r=0x88000000
fdtaddr=0x88000000
fdtcontroladdr=fdf15d98
fdtfile=undefined
findfdt=if test $board_name = omap5_uevm; then setenv fdtfile omap5-uevm.dtb; fi; if test $board_name = dra7xx; then setenv fdtfile dra7-evm.dtb; fi;if test $board_name = dra72x-revc; then setenv fdtfile dra72-evm-revc.dtb; fi;if test $board_name = dra72x; then setenv fdtfile dra72-evm.dtb; fi;if test $board_name = dra71x && test $boot_nand = 1; then setenv fdtfile dra71-evm-nand.dtb; fi;if test $board_name = dra71x && test $boot_nand = 0; then setenv fdtfile dra71-evm.dtb; fi;if test $board_name = dra71-lcard; then setenv fdtfile dra71-lcard.dtb; fi;if test $board_name = dra76x_acd; then setenv fdtfile dra76-evm.dtb; fi;if test $board_name = beagle_x15; then setenv fdtfile am57xx-beagle-x15.dtb; fi;if test $board_name = beagle_x15_revb1; then setenv fdtfile am57xx-beagle-x15-revb1.dtb; fi;if test $board_name = beagle_x15_revc; then setenv fdtfile am57xx-beagle-x15-revc.dtb; fi;if test $board_name = am572x_idk && test $idk_lcd = no; then setenv fdtfile am572x-idk.dtb; fi;if test $board_name = am572x_idk && test $idk_lcd = osd101t2045; then setenv fdtfile am572x-idk-lcd-osd101t2045.dtb; fi;if test $board_name = am572x_idk && test $idk_lcd = osd101t2587; then setenv fdtfile am572x-idk-lcd-osd101t2587.dtb; fi;if test $board_name = am574x_idk && test $idk_lcd = no; then setenv fdtfile am574x-idk.dtb; fi;if test $board_name = am574x_idk && test $idk_lcd = osd101t2587; then setenv fdtfile am574x-idk-lcd-osd101t2587.dtb; fi;if test $board_name = am57xx_evm; then setenv fdtfile am57xx-evm.dtb; fi;if test $board_name = am57xx_evm_reva3; then setenv fdtfile am57xx-evm-reva3.dtb; fi;if test $board_name = am571x_idk && test $idk_lcd = no; then setenv fdtfile am571x-idk.dtb; fi;if test $board_name = am571x_idk && test $idk_lcd = osd101t2045; then setenv fdtfile am571x-idk-lcd-osd101t2045.dtb; fi;if test $board_name = am571x_idk && test $idk_lcd = osd101t2587; then setenv fdtfile am571x-idk-lcd-osd101t2587.dtb; fi;if test $fdtfile = undefined; then echo WARNING: Could not determine device tree to use; fi;
finduuid=part uuid mmc ${bootpart} uuid
fit_bootfile=fitImage
fit_loadaddr=0x87000000
getuenv=mmc dev ${mmcdev}; if mmc rescan; then if run loadbootenv; then run importbootenv; fi; fi;
importbootenv=echo Importing environment from mmc${mmcdev} ...; env import -t ${loadaddr} ${filesize}
ip_method=dhcp
ipaddr=192.168.1.102
kernel_addr_r=0x82000000
loadaddr=0x82000000
loadbootenv=fatload mmc ${mmcdev} ${loadaddr} ${bootenvfile}
loadbootscript=load mmc ${mmcdev} ${loadaddr} boot.scr
loadfdt=load ${devtype} ${bootpart} ${fdtaddr} ${bootdir}/${fdtfile}
loadfit=run args_mmc; bootm ${loadaddr}#${fdtfile};
loadimage=load ${devtype} ${bootpart} ${loadaddr} ${bootdir}/${bootfile}
mmcboot=mmc dev ${mmcdev}; setenv devnum ${mmcdev}; setenv devtype mmc; if mmc rescan; then echo SD/MMC found on device ${mmcdev};if run loadimage; then if test ${boot_fit} -eq 1; then run loadfit; else run mmcloados;fi;fi;fi;
mmcdev=0
mmcloados=run args_mmc; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if run loadfdt; then bootz ${loadaddr} - ${fdtaddr}; else if test ${boot_fdt} = try; then bootz; else echo WARN: Cannot load the DT; fi; fi; else bootz; fi;
mmcrootfstype=ext4 rootwait
myargs=setenv bootargs console=${console} ${optargs} root=/dev/nfs nfsroot=${serverip}:${rootpath},${nfsopts} rw ip=dhcp earlyprintk
netargs=setenv bootargs console=${console} ${optargs} root=/dev/nfs nfsroot=${serverip}:${rootpath},${nfsopts} rw ip=dhcp
netboot=echo Booting from network ...; setenv autoload no; dhcp; run netloadimage; run netloadfdt; run netargs; bootz ${loadaddr} - ${fdtaddr}
netloadfdt=tftp ${fdtaddr} ${fdtfile}
netloadimage=tftp ${loadaddr} ${bootfile}
nfsopts=nolock,proto=udp
partitions=uuid_disk=${uuid_gpt_disk};name=bootloader,start=384K,size=1792K,uuid=${uuid_gpt_bootloader};name=rootfs,start=2688K,size=-,uuid=${uuid_gpt_rootfs}
partitions_android=uuid_disk=${uuid_gpt_disk};name=xloader,start=128K,size=256K,uuid=${uuid_gpt_xloader};name=bootloader,size=1792K,uuid=${uuid_gpt_bootloader};name=environment,size=128K,uuid=${uuid_gpt_environment};name=misc,size=128K,uuid=${uuid_gpt_misc};name=reserved,size=256K,uuid=${uuid_gpt_reserved};name=efs,size=16M,uuid=${uuid_gpt_efs};name=crypto,size=16K,uuid=${uuid_gpt_crypto};name=recovery,size=40M,uuid=${uuid_gpt_recovery};name=boot,size=10M,uuid=${uuid_gpt_boot};name=system,size=768M,uuid=${uuid_gpt_system};name=vendor,size=256M,uuid=${uuid_gpt_vendor};name=cache,size=256M,uuid=${uuid_gpt_cache};name=ipu1,size=1M,uuid=${uuid_gpt_ipu1};name=ipu2,size=1M,uuid=${uuid_gpt_ipu2};name=userdata,size=-,uuid=${uuid_gpt_userdata}
pxefile_addr_r=0x80100000
ramdisk_addr_r=0x88080000
rdaddr=0x88080000
rootpath=/home/marc/ti-sdk05-am57xx-evm/filesystem
scriptaddr=0x80000000
scsidevs=0
serial#=1501300a628c0121
serverip=192.168.1.101
soc=omap5
static_ip=${ipaddr}:${serverip}:${gatewayip}:${netmask}:${hostname}::off
stderr=serial@48020000
stdin=serial@48020000
stdout=serial@48020000
uenvcmd=dhcp
update_to_fit=setenv loadaddr ${fit_loadaddr}; setenv bootfile ${fit_bootfile}
usbtty=cdc_acm
vendor=ti
ver=U-Boot 2018.01-g131dc82830 (Jul 25 2018 - 16:55:31 +0000)
vram=16M
Environment size: 8062/131067 bytes
=>
Boot dhcp log
U-Boot 2018.01-g131dc82830 (Jul 25 2018 - 16:55:31 +0000)
CPU : DRA752-GP ES1.1
Model: TI AM5728 BeagleBoard-X15
Board: AM572x EVM REV A.20
DRAM: 2 GiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
GUID Partition Table Header signature is wrong: 0x0 != 0x5452415020494645
part_get_info_efi: *** ERROR: Invalid GPT ***
GUID Partition Table Header signature is wrong: 0x0 != 0x5452415020494645
part_get_info_efi: *** ERROR: Invalid Backup GPT ***
SCSI: SATA link 0 timeout.
AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst
scanning bus for devices...
Found 0 device(s).
Net: eth0: ethernet@48484000
Hit any key to stop autoboot: 0
=>
=> setenv autoload no
=> setenv serverip 192.168.1.101
=> setenv rootpath /home/marc/ti-sdk05-am57xx-evm/filesystem
=> setenv nfsopts 'nolock,proto=udp'
=> setenv myargs 'setenv bootargs console=${console} ${optargs} root=/dev/nfs nfsroot=${serverip}:${rootpath},${nfsopts} rw ip=dhcp earlyprintk'
=> setenv ip_method dhcp
=> setenv uenvcmd dhcp; tftp ${loadaddr}; run myargs; tftp ${fdtaddr} ${fdtfile}; bootz ${loadaddr} - ${fdtaddr}
link up on port 0, speed 100, full duplex
*** ERROR: `ipaddr' not set
link up on port 0, speed 100, full duplex
*** ERROR: `ipaddr' not set
=>
try 'dhcp'
=> dhcp
link up on port 0, speed 100, full duplex
BOOTP broadcast 1
BOOTP broadcast 2
DHCP client bound to address 192.168.1.102 (1920 ms)
try TFTPBOOT
=> tftpboot
link up on port 0, speed 100, full duplex
Using ethernet@48484000 device
TFTP from server 192.168.1.101; our IP address is 192.168.1.102
Filename 'undefined'.
Load address: 0x82000000
Loading: *
Abort
Question: why is ipaddr needed if i'm setup for DHCP?
Question: where does u-boot get the names of zImage, DTB, etc?