Part Number: AM4372
Other Parts Discussed in Thread: TPS65218,
1) Looking at the EVM schematic I notice that there is a LDO connected to pin 24 of the TPS65218 that is supplying V1_8BAT. There is also an option to use the DCDC6 output for V1_8BAT, but the 0 ohm is DNI. Also, the data sheet for the TPS65218 states that "Connecting any external load to this pin is not recommended." Can you explain why this is being done on the EVM design? Is there some issue with the DCDC6 supply?
2) On the AC_DET pin (9) of the TPS615218 there is a 10k pull-up and a 0 ohm pull down. Both seem to be installed according to the schematic and BOM. Is this an error?
3) On the EVM schematics page 25 You have the signal LCD_AC_BIAS_EN pin also marked as SYSBOOT18. The TRM has references to SYSBOOT18 but the latest data sheet has no mention of SYSBOOT18.