This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Downloading older versions of the DVSDK

Is it possible to download older versions of the DVSDK?  I have not been able to find it on the TI site in the DaVinci Software section.

I have a customer who needs dvsdk_1_01_00_15.

Thanks!

  • This depends on the particular device you are obtaining the DVSDK for, in the case of the DM6446 they are all up on the updates site through www.ti.com/davinciregistration, however it looks like the older versions of the DM6437 are not listed (which I assume you are using based on the version number). I will have to take a look into why the older versions are no longer linked on there, though I would like to see customers move to the latest versions in general there are still legitimate reasons to download the old versions.

    On a positive note the actual old DVSDK file is still up there, though since the link is not you have to make a bit of a URL hack to get to it. On the downloads site there should be a link to dm6437_dvsdk_setupwin32_1_11_00_00.exe, if you modify the URL so that the file it goes for is dm6437_dvsdk_setupwin32_1_01_00_15.exe than you can get the older version.

  • Bernie, you just saved my customer and me days of labor and helped us all get to market faster! :)

    Thanks once again for the help.

  • Here is the direct download link for older DVSDKs for DM648 and DM6437 platforms:

    http://software-dl.ti.com/dsps/dsps_registered_sw/sdo_sb/targetcontent/dvsdk/bios_dvsdk/index.html

    Thanks.