Part Number: AM5728
Other Parts Discussed in Thread: DRA752, TPD12S015, TMP102, TLV320AIC3104, PMP
Tool/software: Linux
Hello,
We are trying to use the on board camera module ( Aptina Mt9t111 ), module in not being detected by the board.
Linux SDK v.5.0.
We have tried with using below reference but still it is not detecting.

but it is not working.
We have also checked the SCLK and Vin clk in CRO on camera module but both are not showing any thing means there is no clock input from the processor to Camera module. Also checked the power input to camera.
What is the reason behind this clock not working?
What i understand is if this clock works properly the camera will work to?
Is there anything else so the camera is not working.
Any help will be appreciated.
Thanks
Hiren Kumbhare