Part Number: AM3358
Dears:
Is there any driver about TF Card of MMC2? Since TF Card can not be recognized using MMC2.
And the driver refereed the driver of MMC1.
Pls. give some advice about the driver.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dears:
Pls. refer the below files, and pin mux's code is added in mmc.c.
#include "mmc.h"
#include "pin_mux.h"
#include <plat/mmc.h>
#include "../hsmmc.h"
/* Module pin mux for mmc0 */
static struct pinmux_config mmc0_common_pin_mux[] = {
{"mmc0_dat3.mmc0_dat3", OMAP_MUX_MODE0 | AM33XX_PIN_INPUT_PULLUP},
{"mmc0_dat2.mmc0_dat2", OMAP_MUX_MODE0 | AM33XX_PIN_INPUT_PULLUP},
{"mmc0_dat1.mmc0_dat1", OMAP_MUX_MODE0 | AM33XX_PIN_INPUT_PULLUP},
{"mmc0_dat0.mmc0_dat0", OMAP_MUX_MODE0 | AM33XX_PIN_INPUT_PULLUP},
{"mmc0_clk.mmc0_clk", OMAP_MUX_MODE0 | AM33XX_PIN_INPUT_PULLUP},
{"mmc0_cmd.mmc0_cmd", OMAP_MUX_MODE0 | AM33XX_PIN_INPUT_PULLUP},
{"mmc0_sdcd.gpio3_14", OMAP_MUX_MODE7 | AM33XX_PIN_INPUT_PULLUP},
{NULL, 0},
};
/* Module pin mux for mmc1 */
static struct pinmux_config mmc1_common_pin_mux[] = {
{"gpmc_ad3.mmc1_dat3", OMAP_MUX_MODE1 | AM33XX_PIN_INPUT_PULLUP},
{"gpmc_ad2.mmc1_dat2", OMAP_MUX_MODE1 | AM33XX_PIN_INPUT_PULLUP},
{"gpmc_ad1.mmc1_dat1", OMAP_MUX_MODE1 | AM33XX_PIN_INPUT_PULLUP},
{"gpmc_ad0.mmc1_dat0", OMAP_MUX_MODE1 | AM33XX_PIN_INPUT_PULLUP},
{"gpmc_csn1.mmc1_clk", OMAP_MUX_MODE2 | AM33XX_PIN_INPUT_PULLUP},
{"gpmc_csn2.mmc1_cmd", OMAP_MUX_MODE2 | AM33XX_PIN_INPUT_PULLUP},
{NULL, 0},
};
static struct pinmux_config mmc1_dat4_7_pin_mux[] = {
{"gpmc_ad7.mmc1_dat7", OMAP_MUX_MODE1 | AM33XX_PIN_INPUT_PULLUP},
{"gpmc_ad6.mmc1_dat6", OMAP_MUX_MODE1 | AM33XX_PIN_INPUT_PULLUP},
{"gpmc_ad5.mmc1_dat5", OMAP_MUX_MODE1 | AM33XX_PIN_INPUT_PULLUP},
{"gpmc_ad4.mmc1_dat4", OMAP_MUX_MODE1 | AM33XX_PIN_INPUT_PULLUP},
{NULL, 0},
};
//add 1 by liguang
static struct pinmux_config mmc2_com_pin_mux[] = {
{"gpmc_ad12.mmc2_dat0", OMAP_MUX_MODE3 | AM33XX_PIN_INPUT_PULLUP},
{"gpmc_ad13.mmc2_dat1", OMAP_MUX_MODE3 | AM33XX_PIN_INPUT_PULLUP},
{"gpmc_ad14.mmc2_dat2", OMAP_MUX_MODE3 | AM33XX_PIN_INPUT_PULLUP},
{"gpmc_ad15.mmc2_dat3", OMAP_MUX_MODE3 | AM33XX_PIN_INPUT_PULLUP},
{"gpmc_csn3.mmc2_cmd", OMAP_MUX_MODE3 | AM33XX_PIN_INPUT_PULLUP},
{"gpmc_clk.mmc2_clk", OMAP_MUX_MODE3 | AM33XX_PIN_INPUT_PULLUP},
{"gpmc_wpn.gpio0_31", OMAP_MUX_MODE7 | AM33XX_PIN_INPUT_PULLUP},
{NULL, 0},
};
//end 1
static struct omap2_hsmmc_info am335x_mmc[] __initdata = {
{
.mmc = 1,
.caps = MMC_CAP_4_BIT_DATA,
.gpio_cd = GPIO_TO_PIN(3, 14),
.gpio_wp = -EINVAL,
.ocr_mask = MMC_VDD_32_33 | MMC_VDD_33_34, /* 3V3 */
},
{
.mmc = 0, /* will be set at runtime */
},
{
.mmc = 0, /* will be set at runtime */
},
{} /* Terminator */
};
//add 2 by liguang
static struct omap2_hsmmc_info am335x_mmc2[] __initdata = {
{
.mmc = 3,
.caps = MMC_CAP_4_BIT_DATA,
.gpio_cd = GPIO_TO_PIN(0, 31),
.gpio_wp = -EINVAL,
.ocr_mask = MMC_VDD_32_33 | MMC_VDD_33_34, /* 3V3 */
},
{} /* Terminator */
};
//end 2
void mmc0_init(int evm_id, int profile)
{
setup_pin_mux(mmc0_common_pin_mux);
omap2_hsmmc_init(am335x_mmc);
return;
}
void mmc1_emmc_init(int evm_id, int profile)
{
setup_pin_mux(mmc1_common_pin_mux);
setup_pin_mux(mmc1_dat4_7_pin_mux);
am335x_mmc[1].mmc = 2;
am335x_mmc[1].caps = MMC_CAP_8_BIT_DATA;
am335x_mmc[1].gpio_cd = -EINVAL;
am335x_mmc[1].gpio_wp = -EINVAL;
am335x_mmc[1].ocr_mask = MMC_VDD_32_33 | MMC_VDD_33_34; /* 3V3 */
/* mmc will be initialized when mmc0_init is called */
return;
}
//add 3 by liguang
void mmc2_init(int evm_id, int profile)
{
setup_pin_mux(mmc2_com_pin_mux);
omap2_hsmmc_init(am335x_mmc2);
return;
}
// end 3
dmesg [ 0.000000] Linux version 3.2.0 (root@steve-virtual-machine) (gcc version 4.7.3 20130226 (prerelease) (crosstool-NG linaro-1.13.1-4.7-2013.03-20130313 - Linaro GCC 2013.03) ) #422 Fri Aug 24 09:58:50 CST 2018 [ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache [ 0.000000] Machine: am335xevm [ 0.000000] Memory policy: ECC disabled, Data cache writeback [ 0.000000] On node 0 totalpages: 131072 [ 0.000000] free_area_init_node: node 0, pgdat c0577670, node_mem_map c05af000 [ 0.000000] Normal zone: 1024 pages used for memmap [ 0.000000] Normal zone: 0 pages reserved [ 0.000000] Normal zone: 130048 pages, LIFO batch:31 [ 0.000000] AM335X ES2.1 (sgx neon ) [ 0.000000] pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768 [ 0.000000] pcpu-alloc: [0] 0 [ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 130048 [ 0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk1p2 ro rootfstype=ext3 rootwait ip=none [ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes) [ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes) [ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes) [ 0.000000] Memory: 512MB = 512MB total [ 0.000000] Memory: 513932k/513932k available, 10356k reserved, 0K highmem [ 0.000000] Virtual kernel memory layout: [ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB) [ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB) [ 0.000000] vmalloc : 0xe0800000 - 0xff000000 ( 488 MB) [ 0.000000] lowmem : 0xc0000000 - 0xe0000000 ( 512 MB) [ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB) [ 0.000000] .text : 0xc0008000 - 0xc04eb000 (5004 kB) [ 0.000000] .init : 0xc04eb000 - 0xc0523000 ( 224 kB) [ 0.000000] .data : 0xc0524000 - 0xc0580100 ( 369 kB) [ 0.000000] .bss : 0xc0580124 - 0xc05ae2d4 ( 185 kB) [ 0.000000] NR_IRQS:396 [ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts [ 0.000000] Total of 128 interrupts on 1 active controller [ 0.000000] OMAP clockevent source: GPTIMER2 at 24000000 Hz [ 0.000000] OMAP clocksource: GPTIMER1 at 32768 Hz [ 0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 131071999ms [ 0.000000] Console: colour dummy device 80x30 [ 0.000091] Calibrating delay loop... 795.44 BogoMIPS (lpj=3977216) [ 0.039093] pid_max: default: 32768 minimum: 301 [ 0.039184] Security Framework initialized [ 0.039276] Mount-cache hash table entries: 512 [ 0.039611] CPU: Testing write buffer coherency: ok [ 0.059387] omap_hwmod: pruss: failed to hardreset [ 0.060394] print_constraints: dummy: [ 0.060699] NET: Registered protocol family 16 [ 0.062591] OMAP GPIO hardware version 0.1 [ 0.064605] omap_mux_init: Add partition: #1: core, flags: 0 [ 0.066192] omap_i2c.1: alias fck already exists [ 0.066375] The board is a HDZX AM335x 1501. [ 0.066558] _omap_mux_get_by_name: Could not find signal mmc0_sdcd.gpio3_14 [ 0.066589] omap_hsmmc.0: alias fck already exists [ 0.066802] omap_hsmmc.1: alias fck already exists [ 0.067504] d_can.0: alias fck already exists [ 0.067993] omap_i2c.3: alias fck already exists [ 0.068420] omap3_has_sgx...... [ 0.069030] _regulator_get: l3_main.0 supply vdd_core not found, using dummy regulator [ 0.069152] am335x_opp_update: physical regulator not present for core(-22) [ 0.069213] platform mpu.0: opp_set_availability: Device OPP not found (-19) [ 0.069244] platform mpu.0: opp_set_availability: Device OPP not found (-19) [ 0.069427] registered am33xx_sr device [ 0.070739] edma.0: alias fck already exists [ 0.070770] edma.0: alias fck already exists [ 0.070770] edma.0: alias fck already exists [ 0.091430] bio: create slab <bio-0> at 0 [ 0.093414] SCSI subsystem initialized [ 0.094024] usbcore: registered new interface driver usbfs [ 0.094299] usbcore: registered new interface driver hub [ 0.094482] usbcore: registered new device driver usb [ 0.094757] registerd cppi-dma Intr @ IRQ 17 [ 0.094757] Cppi41 Init Done Qmgr-base(e087a000) dma-base(e0878000) [ 0.094787] Cppi41 Init Done [ 0.094787] musb-ti81xx musb-ti81xx: musb0, board_mode=0x13, plat_mode=0x3 [ 0.095092] musb-ti81xx musb-ti81xx: musb1, board_mode=0x13, plat_mode=0x1 [ 0.096099] omap_i2c omap_i2c.1: bus 1 rev2.4.0 at 100 kHz [ 0.097106] tps65910 1-002d: JTAGREVNUM 0x0 [ 0.099456] print_constraints: VRTC: [ 0.100860] print_constraints: VIO: at 1500 mV [ 0.103118] print_constraints: VDD1: 600 <--> 1500 mV at 1100 mV normal [ 0.105377] print_constraints: VDD2: 600 <--> 1500 mV at 1100 mV normal [ 0.106353] print_constraints: VDD3: 5000 mV [ 0.107727] print_constraints: VDIG1: at 1800 mV [ 0.109130] print_constraints: VDIG2: at 1800 mV [ 0.110534] print_constraints: VPLL: at 1800 mV [ 0.111907] print_constraints: VDAC: at 1800 mV [ 0.113311] print_constraints: VAUX1: at 1800 mV [ 0.114715] print_constraints: VAUX2: at 3300 mV [ 0.116088] print_constraints: VAUX33: at 3300 mV [ 0.117462] print_constraints: VMMC: at 3300 mV [ 0.117919] tps65910 1-002d: No interrupt support, no core IRQ [ 0.129119] omap_i2c omap_i2c.3: bus 3 rev2.4.0 at 100 kHz [ 0.130950] Switching to clocksource gp timer [ 0.144775] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host) [ 0.144958] musb-hdrc musb-hdrc.0: dma type: dma-cppi41 [ 0.145233] MUSB0 controller's USBSS revision = 4ea20800 [ 0.145263] TxFifo Empty intr disabled [ 0.145263] musb0: Enabled SW babble control [ 0.145538] musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn) [ 0.145538] musb-hdrc: MHDRC RTL version 2.0 [ 0.145568] musb-hdrc: setup fifo_mode 4 [ 0.145599] musb-hdrc: 28/31 max ep, 16384/16384 memory [ 0.145599] musb-hdrc.0: bulk split disabled [ 0.145599] musb-hdrc.0: bulk combine disabled [ 0.146057] musb-hdrc musb-hdrc.0: USB OTG mode controller at e083c000 using DMA, IRQ 18 [ 0.146209] musb-hdrc musb-hdrc.1: dma type: dma-cppi41 [ 0.146484] MUSB1 controller's USBSS revision = 4ea20800 [ 0.146484] TxFifo Empty intr disabled [ 0.146484] musb1: Enabled SW babble control [ 0.146728] musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn) [ 0.146759] musb-hdrc: MHDRC RTL version 2.0 [ 0.146759] musb-hdrc: setup fifo_mode 4 [ 0.146789] musb-hdrc: 28/31 max ep, 16384/16384 memory [ 0.146789] musb-hdrc.1: bulk split disabled [ 0.146820] musb-hdrc.1: bulk combine disabled [ 0.146881] musb-hdrc musb-hdrc.1: MUSB HDRC host driver [ 0.146942] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 1 [ 0.147064] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002 [ 0.147064] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 0.147094] usb usb1: Product: MUSB HDRC host driver [ 0.147094] usb usb1: Manufacturer: Linux 3.2.0 musb-hcd [ 0.147094] usb usb1: SerialNumber: musb-hdrc.1 [ 0.147827] hub 1-0:1.0: USB hub found [ 0.147857] hub 1-0:1.0: 1 port detected [ 0.148345] musb-hdrc musb-hdrc.1: USB Host mode controller at e083e800 using DMA, IRQ 19 [ 0.148712] NET: Registered protocol family 2 [ 0.148895] IP route cache hash table entries: 4096 (order: 2, 16384 bytes) [ 0.149169] TCP established hash table entries: 16384 (order: 5, 131072 bytes) [ 0.149414] TCP bind hash table entries: 16384 (order: 4, 65536 bytes) [ 0.149566] TCP: Hash tables configured (established 16384 bind 16384) [ 0.149597] TCP reno registered [ 0.149597] UDP hash table entries: 256 (order: 0, 4096 bytes) [ 0.149627] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes) [ 0.149810] NET: Registered protocol family 1 [ 0.150024] RPC: Registered named UNIX socket transport module. [ 0.150054] RPC: Registered udp transport module. [ 0.150054] RPC: Registered tcp transport module. [ 0.150054] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.150299] NetWinder Floating Point Emulator V0.97 (double precision) [ 0.168212] VFS: Disk quotas dquot_6.5.2 [ 0.168243] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes) [ 0.168731] msgmni has been set to 1003 [ 0.171539] alg: No test for stdrng (krng) [ 0.172119] io scheduler noop registered [ 0.172149] io scheduler deadline registered [ 0.172210] io scheduler cfq registered (default) [ 0.173461] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0 [ 0.880645] console [ttyO0] enabled [ 0.884857] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1 [ 0.892639] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2 [ 0.900390] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3 [ 0.908142] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4 [ 0.915893] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5 [ 0.924102] omap4_rng omap4_rng: OMAP4 Random Number Generator ver. 2.00 [ 0.939361] brd: module loaded [ 0.946960] loop: module loaded [ 0.950408] i2c-core: driver [tsl2550] using legacy suspend method [ 0.956909] i2c-core: driver [tsl2550] using legacy resume method [ 0.963317] at24_init begin [ 0.968475] mtdoops: mtd device (mtddev=name/number) must be supplied [ 0.976867] tun: Universal TUN/TAP device driver, 1.6 [ 0.982147] tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com> [ 0.988830] CAN device driver interface [ 0.992858] CAN bus driver for Bosch D_CAN controller 1.0 [ 0.999206] d_can d_can.0: device registered (irq=52, irq_obj=53) [ 1.051727] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6 [ 1.058197] davinci_mdio davinci_mdio.0: detected phy mask fffffff4 [ 1.066467] davinci_mdio.0: probed [ 1.070007] davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver unknown [ 1.077423] davinci_mdio davinci_mdio.0: phy[1]: device 0:01, driver unknown [ 1.084808] davinci_mdio davinci_mdio.0: phy[3]: device 0:03, driver unknown [ 1.092346] PPP generic driver version 2.4.2 [ 1.097137] PPP BSD Compression module registered [ 1.102081] SLIP: version 0.8.4-NET3.019-NEWTTY (dynamic channels, max=256). [ 1.109436] CSLIP: code copyright 1989 Regents of the University of California. [ 1.117309] usbcore: registered new interface driver cdc_ether [ 1.123565] usbcore: registered new interface driver cdc_eem [ 1.129608] usbcore: registered new interface driver dm9601 [ 1.135498] cdc_ncm: 04-Aug-2011 [ 1.139007] usbcore: registered new interface driver cdc_ncm [ 1.144958] Initializing USB Mass Storage driver... [ 1.150238] usbcore: registered new interface driver usb-storage [ 1.156555] USB Mass Storage support registered. [ 1.161712] usbcore: registered new interface driver usbserial [ 1.167938] USB Serial support registered for generic [ 1.173370] usbcore: registered new interface driver usbserial_generic [ 1.180206] usbserial: USB Serial Driver core [ 1.184906] USB Serial support registered for GSM modem (1-port) [ 1.191467] usbcore: registered new interface driver option [ 1.197296] option: v0.7.2:USB Driver for GSM modems [ 1.202911] mousedev: PS/2 mouse device common for all mice [ 1.212127] rtc-ds1307 1-0068: rtc core: registered ds1339 as rtc0 [ 1.219055] i2c /dev entries driver [ 1.223297] Linux video capture interface: v2.00 [ 1.228393] usbcore: registered new interface driver uvcvideo [ 1.234436] USB Video Class driver (1.1.1) [ 1.239501] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec [ 1.247955] cpuidle: using governor ladder [ 1.252685] cpuidle: using governor menu [ 1.260284] omap4_aes_mod_init: loading AM33X AES driver [ 1.265991] omap4-aes omap4-aes: AM33X AES hw accel rev: 3.02 [ 1.272705] omap4_aes_probe: probe() done [ 1.277099] omap4_sham_mod_init: loading AM33X SHA/MD5 driver [ 1.283233] omap4-sham omap4-sham: AM33X SHA/MD5 hw accel rev: 4.03 [ 1.297454] omap4_sham_probe: probe() done [ 1.302612] tiadc tiadc: attached adc driver [ 1.308227] oprofile: hardware counters not available [ 1.313537] oprofile: using timer interrupt. [ 1.318023] nf_conntrack version 0.5.0 (8030 buckets, 32120 max) [ 1.324798] ip_tables: (C) 2000-2006 Netfilter Core Team [ 1.330444] TCP cubic registered [ 1.333862] NET: Registered protocol family 17 [ 1.340789] can: controller area network core (rev 20090105 abi 8) [ 1.347381] NET: Registered protocol family 29 [ 1.352081] can: raw protocol (rev 20090105) [ 1.356536] can: broadcast manager protocol (rev 20090105 t) [ 1.362487] 8021q: 802.1Q VLAN Support v1.8 [ 1.366882] lib80211: common routines for IEEE802.11 drivers [ 1.372802] lib80211_crypt: registered algorithm 'NULL' [ 1.372833] Registering the dns_resolver key type [ 1.377807] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3 [ 1.385833] ThumbEE CPU extension supported. [ 1.390350] mux: Failed to setup hwmod io irq -22 [ 1.395874] Power Management for AM33XX family [ 1.400695] Trying to load am335x-pm-firmware.bin (60 secs timeout) [ 1.407409] Copied the M3 firmware to UMEM [ 1.411773] Cortex M3 Firmware Version = 0x181 [ 1.416442] DIEID: 0700b028 0168453b 00000000 316e0002 [ 1.416442] EFUSE SMA register val = 00013e2f [ 1.416473] Compensating OPP0: Orig nvalue:0x99b7a9 New nvalue:0x99b7a9 [ 1.416503] Compensating OPP1: Orig nvalue:0x9a86f4 New nvalue:0x9a86f4 [ 1.417968] Compensating OPP0: Orig nvalue:0x99aaa3 New nvalue:0x99aaa3 [ 1.417968] Compensating OPP1: Orig nvalue:0x998f85 New nvalue:0x998f85 [ 1.417999] Compensating OPP2: Orig nvalue:0xaae6d4 New nvalue:0xaae6d4 [ 1.417999] Compensating OPP3: Orig nvalue:0xaac5b6 New nvalue:0xaac5b6 [ 1.417999] Compensating OPP4: Orig nvalue:0xaac5b6 New nvalue:0xaa978d [ 1.418060] create_regulator: VDD1: Failed to create debugfs directory [ 1.426422] smartreflex smartreflex: am33xx_sr_probe: Driver initialized [ 1.439422] clock: disabling unused clocks to save power [ 1.453430] mmc0: host does not support reading read-only switch. assuming write-enable. [ 1.464294] mmc0: new high speed SDHC card at address 1234 [ 1.470672] mmcblk0: mmc0:1234 SA08G 7.21 GiB [ 1.476593] Random MACID=f2:56:7d:f0:d6:aa [ 1.481781] mmcblk0: p1 p2 [ 1.485473] cpsw: Random MACID = 7e:29:b4:58:da:b6 [ 1.491577] PHY 0:02 not found [ 1.496093] rtc-ds1307 1-0068: setting system clock to 2015-10-22 09:33:36 UTC (1445506416) [ 1.505340] Waiting for root device /dev/mmcblk1p2... [ 1.566497] mmc1: new high speed MMC card at address 0001 [ 1.572723] mmcblk1: mmc1:0001 004GE0 3.68 GiB [ 1.577575] mmcblk1boot0: mmc1:0001 004GE0 partition 1 2.00 MiB [ 1.583923] mmcblk1boot1: mmc1:0001 004GE0 partition 2 2.00 MiB [ 1.592376] mmcblk1: p1 p2 p3 p4 < p5 p6 > [ 1.599975] mmcblk1boot1: unknown partition table [ 1.606689] mmcblk1boot0: unknown partition table [ 1.723724] EXT3-fs (mmcblk1p2): recovery required on readonly filesystem [ 1.730834] EXT3-fs (mmcblk1p2): write access will be enabled during recovery [ 1.766265] kjournald starting. Commit interval 5 seconds [ 1.772125] EXT3-fs (mmcblk1p2): recovery complete [ 1.778961] EXT3-fs (mmcblk1p2): mounted filesystem with ordered data mode [ 1.786254] VFS: Mounted root (ext3 filesystem) readonly on device 179:10. [ 1.793823] Freeing init memory: 224K [ 5.369903] EXT3-fs (mmcblk1p2): using internal journal [ 5.958129] net eth1: CPSW phy found : id is : 0x1cc916 [ 6.030761] net lan1: CPSW phy found : id is : 0x1cc916 [ 6.506347] kjournald starting. Commit interval 5 seconds [ 6.513122] EXT3-fs (mmcblk1p3): using internal journal [ 6.518585] EXT3-fs (mmcblk1p3): recovery complete [ 6.523620] EXT3-fs (mmcblk1p3): mounted filesystem with ordered data mode [ 6.551666] kjournald starting. Commit interval 5 seconds [ 6.558105] EXT3-fs (mmcblk1p5): using internal journal [ 6.563598] EXT3-fs (mmcblk1p5): recovery complete [ 6.569824] EXT3-fs (mmcblk1p5): mounted filesystem with ordered data mode [ 6.589172] kjournald starting. Commit interval 5 seconds [ 6.596008] EXT3-fs (mmcblk1p6): using internal journal [ 6.601470] EXT3-fs (mmcblk1p6): recovery complete [ 6.606506] EXT3-fs (mmcblk1p6): mounted filesystem with ordered data mode [ 6.798431] gadget: Mass Storage Function, version: 2009/09/11 [ 6.804687] gadget: Number of LUNs=1 [ 6.808532] lun0: LUN: removable file: /dev/mmcblk0p1 [ 6.813964] gadget: Mass Storage Gadget, version: 2009/09/11 [ 6.819976] gadget: userspace failed to provide iSerialNumber [ 6.826110] gadget: g_mass_storage ready [ 6.830322] musb-hdrc musb-hdrc.0: MUSB HDRC host driver [ 6.835937] musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 2 [ 6.843811] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002 [ 6.850921] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 6.858489] usb usb2: Product: MUSB HDRC host driver [ 6.863708] usb usb2: Manufacturer: Linux 3.2.0 musb-hcd [ 6.869262] usb usb2: SerialNumber: musb-hdrc.0 [ 6.874542] hub 2-0:1.0: USB hub found [ 6.878479] hub 2-0:1.0: 1 port detected [ 6.983795] gpio_to_irq irq=249 [ 7.079284] USB Serial support registered for EXAR USB serial port [ 7.085937] usbcore: registered new interface driver xr_usb_serial [ 7.092376] Exar USB UART (serial port) driver: 1A [ 7.394165] kjournald starting. Commit interval 5 seconds [ 7.619659] EXT3-fs (mmcblk0p2): using internal journal [ 7.625152] EXT3-fs (mmcblk0p2): recovery complete [ 7.630187] EXT3-fs (mmcblk0p2): mounted filesystem with ordered data mode
Don't use device tree, and the Kernel version is Linux3.2.0