This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Devrocket 5.2 MontaVista Target Manage Creating New Remote Connection

Expert 1130 points

In DevRocket 5.2, Target Management/Create New Connection I select MontaVista Linux as the Remote System Type. I put the IP address of the Target as the Host name, the next window shows Sftp files using Ssh/Sftp File Service and SSH Connector Service. But using this setup I can't connect to the target. I get a connection refused error message. When I type in ssh <Target_IP_Address> I get a connection refused as well. How do set my connection so that I can connect to the Target using DevRocket 5.2?

Mike