This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

lupdate error in processor SDK yocto

Part Number: DRA72XEVM

Hi,

I have to use Qt Linguist feature in my qt app for which i need lupdate command to build .ts from .pro file. But it displayed error  could not exec from /usr/lib/x86_64-linux-gnu/qt4/bin/lupdate

but after installing qt4-dev-tools in the building pc i get error as

 /home/*****/Downloads/SDK/sysroots/armv7ahf-neon-linux-gnueabi/usr/lib/qt5/mkspecs/features/qt_config.prf(3): Missing ] terminator [found /]/home/*****/Downloads/SDK/sysroots/armv7ahf-neon-linux-gnueabi/usr/lib/qt5/mkspecs/features/default_pre.prf(19): Missing ] terminator [found /]/home/*****/Downloads/SDK/sysroots/armv7ahf-neon-linux-gnueabi/usr/lib/qt5/mkspecs/features/resolve_config.prf(25): 'addExclusiveBuilds' is not a recognized test function/home/*****/Downloads/SDK/sysroots/armv7ahf-neon-linux-gnueabi/usr/lib/qt5/mkspecs/features/resolve_config.prf(37): 'addExclusiveBuilds' is not a recognized test function/home/*****/Downloads/SDK/sysroots/armv7ahf-neon-linux-gnueabi/usr/lib/qt5/mkspecs/features/link_pkgconfig.prf(1): 'pkgConfigExecutable' is not a recognized replace functionUpdating '***_***_********/t1_hi.ts'...
    Found 0 source text(s) (0 new and 0 already existing)
Updating 'ITS_HMI_Latest/t1_ma.ts'...
    Found 0 source text(s) (0 new and 0 already existing)