Part Number: AM5728
Tool/software: Linux
Hello,
As per the SDK developer guide to build the minimal filesystem using arago-base-tisdk-image.
I am following the link:

facing the below bitbake error:
hirenk@optimus:/media/1TB_1/Facial/tisdk/build$ MACHINE=am57xx-evm bitbake arago-base-tisdk-image
NOTE: Your conf/bblayers.conf has been automatically updated.
NOTE: Your conf/bblayers.conf has been automatically updated.
Parsing recipes: 100% |#############################################################################################| Time: 0:08:04
Parsing of 3137 .bb files complete (0 cached, 3137 parsed). 4046 targets, 439 skipped, 0 masked, 0 errors.
WARNING: No recipes available for:
/media/1TB_1/Facial/tisdk/sources/meta-arago/meta-arago-distro/recipes-multimedia/gstreamer/gstreamer1.0-plugins-base_1.8.3.bbappend
/media/1TB_1/Facial/tisdk/sources/meta-processor-sdk/recipes-devtools/python/python3-native_3.5.2.bbappend
/media/1TB_1/Facial/tisdk/sources/meta-processor-sdk/recipes-graphics/wayland/weston_1.11.0.bbappend
NOTE: Resolving any missing task queue dependencies
Build Configuration:
BB_VERSION = "1.36.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "ubuntu-16.04"
TARGET_SYS = "arm-linux-gnueabi"
MACHINE = "am57xx-evm"
DISTRO = "arago"
DISTRO_VERSION = "2018.04"
TUNE_FEATURES = "arm armv7a vfp thumb neon callconvention-hard"
TARGET_FPU = "hard"
meta-processor-sdk = "HEAD:264dc66c689e0e4212c43358382986ee470619d4"
meta-ros = "HEAD:e2566402ab108a19634354a934788109422cf409"
meta-arago-distro
meta-arago-extras = "HEAD:d54e9d6c1d461dbf3189e691088d328bf4c4fb19"
meta-browser = "HEAD:26d50665e2f7223c5f4ad7481a8d2431e7cb55fb"
meta-qt5 = "HEAD:682ad61c071a9710e9f9d8a32ab1b5f3c14953d1"
meta-networking
meta-python
meta-oe
meta-gnome
meta-multimedia = "HEAD:352531015014d1957d6444d114f4451e241c4d23"
meta-ti = "HEAD:8555084679dc5c668e5fb60a16425ca32b10ff21"
meta-linaro-toolchain
meta-optee = "HEAD:75dfb67bbb14a70cd47afda9726e2e1c76731885"
meta = "HEAD:931a52e8698f684ccbb26ddec18764ad9d9a3e8f"
Initialising tasks: 100% |##########################################################################################| Time: 0:00:19
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
WARNING: zlib-native-1.2.11-r0 do_fetch: Failed to fetch URL downloads.sourceforge.net/.../zlib-1.2.11.tar.xz, attempting MIRRORS if available
WARNING: bzip2-native-1.0.6-r5 do_fetch: Checksum mismatch for local file /media/1TB_1/Facial/tisdk/downloads/bzip2-1.0.6.tar.gz
Cleaning and trying again.
WARNING: bzip2-native-1.0.6-r5 do_fetch: Renaming /media/1TB_1/Facial/tisdk/downloads/bzip2-1.0.6.tar.gz to /media/1TB_1/Facial/tisdk/downloads/bzip2-1.0.6.tar.gz_bad-checksum_bff5360d1d726346262f06da7973448d
WARNING: bzip2-native-1.0.6-r5 do_fetch: Checksum failure encountered with download of www.bzip.org/.../bzip2-1.0.6.tar.gz - will attempt other sources if available
WARNING: external-linaro-toolchain-2017.11-r0.arago36 do_package: QA Issue: external-linaro-toolchain: Files/directories were installed but not shipped in any package:
/lib/libcilkrts.so
/lib/libcilkrts.spec
/lib/libcilkrts.so.5
/lib/libcilkrts.so.5.0.0
Please set FILES such that these items are packaged. Alternatively if they are unneeded, avoid installing them or delete them within do_install.
external-linaro-toolchain: 4 installed and not shipped files. [installed-vs-shipped]
WARNING: libpng-native-1.6.31-r0 do_fetch: Failed to fetch URL downloads.sourceforge.net/.../libpng-1.6.31.tar.xz, attempting MIRRORS if available
ERROR: linux-ti-staging-4.14.40+gitAUTOINC+4796173fc5-r7a.arago5.tisdk0.1 do_create_srcipk: Function failed: do_create_srcipk (log file is located at /media/1TB_1/Facial/tisdk/build/arago-tmp-external-linaro-toolchain/work/am57xx_evm-linux-gnueabi/linux-ti-staging/4.14.40+gitAUTOINC+4796173fc5-r7a.arago5.tisdk0.1/temp/log.do_create_srcipk.30636)
ERROR: Logfile of failure stored in: /media/1TB_1/Facial/tisdk/build/arago-tmp-external-linaro-toolchain/work/am57xx_evm-linux-gnueabi/linux-ti-staging/4.14.40+gitAUTOINC+4796173fc5-r7a.arago5.tisdk0.1/temp/log.do_create_srcipk.30636
Log data follows:
| DEBUG: Executing python function sstate_task_prefunc
| DEBUG: Python function sstate_task_prefunc finished
| DEBUG: Executing shell function do_create_srcipk
| Cloning into '/media/1TB_1/Facial/tisdk/build/arago-tmp-external-linaro-toolchain/work/am57xx_evm-linux-gnueabi/linux-ti-staging/4.14.40+gitAUTOINC+4796173fc5-r7a.arago5.tisdk0.1/temp-git-shallow-clone'...
| error: inflate: data stream error (invalid code -- missing end-of-block)
| error: failed to read object 4ada120eaa2d57378b9c270273e8c0b7e542f019 at offset 46159309 from /media/1TB_1/Facial/tisdk/build/arago-tmp-external-linaro-toolchain/work/am57xx_evm-linux-gnueabi/linux-ti-staging/4.14.40+gitAUTOINC+4796173fc5-r7a.arago5.tisdk0.1/temp-git-shallow-clone/.git/objects/pack/pack-9165e2ebca14442a972576f94fc762ecaad1ff2f.pack
| fatal: packed object 4ada120eaa2d57378b9c270273e8c0b7e542f019 (stored in /media/1TB_1/Facial/tisdk/build/arago-tmp-external-linaro-toolchain/work/am57xx_evm-linux-gnueabi/linux-ti-staging/4.14.40+gitAUTOINC+4796173fc5-r7a.arago5.tisdk0.1/temp-git-shallow-clone/.git/objects/pack/pack-9165e2ebca14442a972576f94fc762ecaad1ff2f.pack) is corrupt
| fatal: remote did not send all necessary objects
| WARNING: /media/1TB_1/Facial/tisdk/build/arago-tmp-external-linaro-toolchain/work/am57xx_evm-linux-gnueabi/linux-ti-staging/4.14.40+gitAUTOINC+4796173fc5-r7a.arago5.tisdk0.1/temp/run.do_create_srcipk.30636:1 exit 128 from 'git clone --depth 400 --branch processor-sdk-linux-4.14.y file://$PWD/.git $gitshallowclone'
| ERROR: Function failed: do_create_srcipk (log file is located at /media/1TB_1/Facial/tisdk/build/arago-tmp-external-linaro-toolchain/work/am57xx_evm-linux-gnueabi/linux-ti-staging/4.14.40+gitAUTOINC+4796173fc5-r7a.arago5.tisdk0.1/temp/log.do_create_srcipk.30636)
ERROR: Task (/media/1TB_1/Facial/tisdk/sources/meta-ti/recipes-kernel/linux/linux-ti-staging_4.14.bb:do_create_srcipk) failed with exit code '1'
NOTE: Tasks Summary: Attempted 887 tasks of which 0 didn't need to be rerun and 1 failed.
Summary: 1 task failed:
/media/1TB_1/Facial/tisdk/sources/meta-ti/recipes-kernel/linux/linux-ti-staging_4.14.bb:do_create_srcipk
Summary: There were 7 WARNING messages shown.
Summary: There was 1 ERROR message shown, returning a non-zero exit code.
Need help.
Thanks and regards,
Hiren Kumbhare