Other Parts Discussed in Thread: TMS320DM6437
Hi to everyone,
I would like to ask a question about powering my TMS320DM6437.
I have seen the reference design from the EVM (they use 3 DC/DC converters) and also the application note "5Vin DM643x Power using a PMIC (Multi-output DC/DC Converter) (slta066.pdf)". Actually I would like to use just one DC/DC converter so I decided to go for the multioutput. But when analyzing the sch, I realize that they use the 3.3V output as the core output, instead of using the 1.2V / 0.8 A output that this converter has.
¿Is this because 0.8 A is not enought for supplying the core?
Thanks in advance,
Nuba.