Part Number: AM3358
Tool/software: Linux
Hi,
I am unable to login as 'root' on latest Sitara SDK : PROCESSOR-SDK-LINUX-AM335X 05_00_00_15
I get 'login incorrect' error. I am running default binaries on beaglebone black. Log attached .
Thanks
Saurabh
U-Boot SPL 2018.01-g131dc82830 (Jul 25 2018 - 15:30:24)
Trying to boot from MMC1
*** Warning - bad CRC, using default environment
reading u-boot.img
reading u-boot.img
reading u-boot.img
reading u-boot.img
U-Boot 2018.01-g131dc82830 (Jul 25 2018 - 15:30:24 +0000)
CPU : AM335X-GP rev 2.1
Model: TI AM335x BeagleBone Black
DRAM: 512 MiB
NAND: 0 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
*** Warning - bad CRC, using default environment
<ethaddr> not set. Validating first E-fuse MAC
Net: cpsw, usb_ether
Hit any key to stop autoboot: 2 1 0
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
** Unable to read file boot.scr **
** Unable to read file uEnv.txt **
switch to partitions #0, OK
mmc0 is current device
Scanning mmc 0:1...
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
3842560 bytes read in 301 ms (12.2 MiB/s)
33640 bytes read in 43 ms (763.7 KiB/s)
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8fff4000, end 8ffff367 ... OK
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 4.14.40-g4796173fc5 (oe-user@oe-host) (gcc version 7.2.1 20171011 (Linaro GCC 7.2-2017.11)) #1 PREEMPT Wed Jul 25 15:43:15 UTC 2018
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] OF: fdt: Machine model: TI AM335x BeagleBone Black
[ 0.000000] Memory policy: Data cache writeback
[ 0.000000] efi: Getting EFI parameters from FDT:
[ 0.000000] efi: UEFI not found.
[ 0.000000] cma: Reserved 48 MiB at 0x9d000000
[ 0.000000] CPU: All CPU(s) started in SVC mode.
[ 0.000000] AM335X ES2.1 (sgx neon)
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 129920
[ 0.000000] Kernel command line: console=ttyO0,115200n8 root=PARTUUID=0005a474-02 rw rootfstype=ext4 rootwait
[ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Memory: 456932K/524288K available (8192K kernel code, 318K rwdata, 2488K rodata, 1024K init, 275K bss, 18204K reserved, 49152K cma-reserved, 0K highmem)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
[ 0.000000] vmalloc : 0xe0800000 - 0xff800000 ( 496 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xe0000000 ( 512 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc0900000 (9184 kB)
[ 0.000000] .init : 0xc0c00000 - 0xc0d00000 (1024 kB)
[ 0.000000] .data : 0xc0d00000 - 0xc0d4fb08 ( 319 kB)
[ 0.000000] .bss : 0xc0d4fb08 - 0xc0d948bc ( 276 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] Tasks RCU enabled.
[ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[ 0.000000] OMAP clockevent source: timer2 at 24000000 Hz
[ 0.000013] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns
[ 0.000030] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns
[ 0.000040] OMAP clocksource: timer1 at 24000000 Hz
[ 0.000177] timer_probe: no matching timers found
[ 0.000360] Console: colour dummy device 80x30
[ 0.000387] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
[ 0.000393] This ensures that you still see kernel messages. Please
[ 0.000398] update your kernel commandline.
[ 0.000425] Calibrating delay loop... 996.14 BogoMIPS (lpj=4980736)
[ 0.089227] pid_max: default: 32768 minimum: 301
[ 0.089393] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.089406] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.090095] CPU: Testing write buffer coherency: ok
[ 0.090721] Setting up static identity map for 0x80100000 - 0x80100060
[ 0.090848] Hierarchical SRCU implementation.
[ 0.091128] EFI services will not be available.
[ 0.092284] devtmpfs: initialized
[ 0.098813] random: get_random_u32 called from bucket_table_alloc+0x8c/0x1ac with crng_init=0
[ 0.099343] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 0.099629] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.099649] futex hash table entries: 256 (order: -1, 3072 bytes)
[ 0.102963] pinctrl core: initialized pinctrl subsystem
[ 0.103636] DMI not present or invalid.
[ 0.104005] NET: Registered protocol family 16
[ 0.105950] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.113945] omap_hwmod: tptc0 using broken dt data from edma
[ 0.114062] omap_hwmod: tptc1 using broken dt data from edma
[ 0.114162] omap_hwmod: tptc2 using broken dt data from edma
[ 0.118380] omap_hwmod: debugss: _wait_target_disable failed
[ 0.170558] cpuidle: using governor ladder
[ 0.170589] cpuidle: using governor menu
[ 0.173512] OMAP GPIO hardware version 0.1
[ 0.182268] No ATAGs?
[ 0.182285] hw-breakpoint: debug architecture 0x4 unsupported.
[ 0.189853] edma 49000000.edma: Legacy memcpy is enabled, things might not work
[ 0.193190] edma 49000000.edma: TI EDMA DMA engine driver
[ 0.195977] omap_i2c 44e0b000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_i2c0_pins, deferring probe
[ 0.196036] omap_i2c 4802a000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_i2c1_pins, deferring probe
[ 0.196072] omap_i2c 4819c000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_i2c2_pins, deferring probe
[ 0.196172] media: Linux media interface: v0.10
[ 0.196210] Linux video capture interface: v2.00
[ 0.196306] pps_core: LinuxPPS API ver. 1 registered
[ 0.196314] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.196334] PTP clock support registered
[ 0.196364] EDAC MC: Ver: 3.0.0
[ 0.196816] dmi: Firmware registration failed.
[ 0.197175] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
[ 0.197475] Advanced Linux Sound Architecture Driver Initialized.
[ 0.198493] clocksource: Switched to clocksource timer1
[ 0.205715] NET: Registered protocol family 2
[ 0.206369] TCP established hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.206415] TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.206454] TCP: Hash tables configured (established 4096 bind 4096)
[ 0.206543] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.206560] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.206690] NET: Registered protocol family 1
[ 0.207075] RPC: Registered named UNIX socket transport module.
[ 0.207087] RPC: Registered udp transport module.
[ 0.207093] RPC: Registered tcp transport module.
[ 0.207099] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.207879] hw perfevents: no interrupt-affinity property for /pmu, guessing.
[ 0.207989] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available
[ 0.209474] workingset: timestamp_bits=14 max_order=17 bucket_order=3
[ 0.213082] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.213784] NFS: Registering the id_resolver key type
[ 0.213827] Key type id_resolver registered
[ 0.213833] Key type id_legacy registered
[ 0.213872] ntfs: driver 2.1.32 [Flags: R/O].
[ 0.215590] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245)
[ 0.215608] io scheduler noop registered
[ 0.215616] io scheduler deadline registered
[ 0.215803] io scheduler cfq registered (default)
[ 0.215813] io scheduler mq-deadline registered
[ 0.215820] io scheduler kyber registered
[ 0.216650] pinctrl-single 44e10800.pinmux: please update dts to use #pinctrl-cells = <1>
[ 0.216968] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568
[ 0.259929] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled
[ 0.262622] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 27, base_baud = 3000000) is a 8250
[ 0.937351] console [ttyS0] enabled
[ 0.941870] 48022000.serial: ttyS1 at MMIO 0x48022000 (irq = 28, base_baud = 3000000) is a 8250
[ 0.951578] 481a8000.serial: ttyS4 at MMIO 0x481a8000 (irq = 29, base_baud = 3000000) is a 8250
[ 0.961919] omap_rng 48310000.rng: Random Number Generator ver. 20
[ 0.977522] brd: module loaded
[ 0.986462] loop: module loaded
[ 0.991488] libphy: Fixed MDIO Bus: probed
[ 1.068567] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6, bus freq 1000000
[ 1.076269] davinci_mdio 4a101000.mdio: detected phy mask fffffffe
[ 1.083638] libphy: 4a101000.mdio: probed
[ 1.087682] davinci_mdio 4a101000.mdio: phy[0]: device 4a101000.mdio:00, driver SMSC LAN8710/LAN8720
[ 1.097673] cpsw 4a100000.ethernet: Detected MACID = 98:5d:ad:7f:bb:91
[ 1.104430] cpsw 4a100000.ethernet: initialized cpsw ale version 1.4
[ 1.110897] cpsw 4a100000.ethernet: ALE Table size 1024
[ 1.116182] cpsw 4a100000.ethernet: cpts: overflow check period 500 (jiffies)
[ 1.124607] i2c /dev entries driver
[ 1.128473] IR NEC protocol handler initialized
[ 1.133130] IR RC5(x/sz) protocol handler initialized
[ 1.138200] IR RC6 protocol handler initialized
[ 1.142764] IR JVC protocol handler initialized
[ 1.147311] IR Sony protocol handler initialized
[ 1.151955] IR SANYO protocol handler initialized
[ 1.156675] IR Sharp protocol handler initialized
[ 1.161406] IR MCE Keyboard/mouse protocol handler initialized
[ 1.167261] IR XMP protocol handler initialized
[ 1.172780] cpu cpu0: OPP-v2 not supported, cpufreq-dt will attempt to use legacy tables.
[ 1.181540] sdhci: Secure Digital Host Controller Interface driver
[ 1.187750] sdhci: Copyright(c) Pierre Ossman
[ 1.192603] omap_hsmmc 48060000.mmc: Got CD GPIO
[ 1.295677] mmc0: host does not support reading read-only switch, assuming write-enable
[ 1.305671] mmc0: new high speed SDHC card at address 0007
[ 1.311644] mmcblk0: mmc0:0007 Y004C 3.71 GiB
[ 1.317732] mmcblk0: p1 p2
[ 1.398733] sdhci-pltfm: SDHCI platform and OF driver helper
[ 1.405863] ledtrig-cpu: registered to indicate activity on CPUs
[ 1.417395] omap_hsmmc 481d8000.mmc: card claims to support voltages below defined range
[ 1.426693] NET: Registered protocol family 10
[ 1.427811] Segment Routing with IPv6
[ 1.427879] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[ 1.428464] NET: Registered protocol family 17
[ 1.428874] Key type dns_resolver registered
[ 1.429062] omap_voltage_late_init: Voltage driver support not added
[ 1.474687] random: fast init done
[ 1.478960] mmc1: new high speed SDIO card at address 0001
[ 1.495945] tps65217 0-0024: TPS65217 ID 0xe version 1.2
[ 1.501916] at24 0-0050: 32768 byte 24c256 EEPROM, writable, 1 bytes/write
[ 1.509161] pinctrl-single 44e10800.pinmux: pin PIN52 already requested by 481a8000.serial; cannot claim for 0-0070
[ 1.519677] pinctrl-single 44e10800.pinmux: pin-52 (0-0070) status -22
[ 1.526235] pinctrl-single 44e10800.pinmux: could not request pin 52 (PIN52) from group nxp_hdmi_bonelt_pins on device pinctrl-single
[ 1.538386] tda998x 0-0070: Error applying setting, reverse things back
[ 1.545059] tda998x: probe of 0-0070 failed with error -22
[ 1.550696] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz
[ 1.557294] i2c i2c-1: of_i2c: modalias failure on /ocp/i2c@4802a000/tps@24
[ 1.564355] i2c i2c-1: Failed to create I2C device for /ocp/i2c@4802a000/tps@24
[ 1.571724] omap_i2c 4802a000.i2c: bus 1 rev0.11 at 400 kHz
[ 1.577541] pinctrl-single 44e10800.pinmux: pin PIN94 already requested by 48022000.serial; cannot claim for 4819c000.i2c
[ 1.588590] pinctrl-single 44e10800.pinmux: pin-94 (4819c000.i2c) status -22
[ 1.595672] pinctrl-single 44e10800.pinmux: could not request pin 94 (PIN94) from group pinmux_i2c2_pins on device pinctrl-single
[ 1.607474] omap_i2c 4819c000.i2c: Error applying setting, reverse things back
[ 1.614757] omap_i2c: probe of 4819c000.i2c failed with error -22
[ 1.622339] cpufreq: cpufreq_online: CPU0: Running at unlisted freq: 1000000 KHz
[ 1.629906] cpu cpu0: dev_pm_opp_set_rate: failed to find current OPP for freq 1000000000 (-34)
[ 1.640292] cpufreq: cpufreq_online: CPU0: Unlisted initial frequency changed to: 720000 KHz
[ 1.649565] hctosys: unable to open rtc device (rtc0)
[ 1.655123] wlan-en-regulator: disabling
[ 1.659215] ALSA device list:
[ 1.662201] No soundcards found.
[ 8.438898] EXT4-fs (mmcblk0p2): recovery complete
[ 8.447120] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[ 8.455482] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 8.463380] devtmpfs: mounted
[ 8.472130] Freeing unused kernel memory: 1024K
[ 8.833130] systemd[1]: System time before build time, advancing clock.
[ 8.885617] systemd[1]: Configuration file /etc/systemd/system.conf is marked executable. Please remove executable permission bits. Proceeding anyway.
[ 8.899785] systemd[1]: Configuration file /etc/systemd/system.conf is marked world-writable. Please remove world writability permission bits. Proceeding anyway.
[ 8.932736] systemd[1]: systemd 234 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN default-hierarchy=hybrid)
[ 8.954443] systemd[1]: Detected architecture arm.
Welcome to Arago 2018.04!
[ 8.992923] systemd[1]: Set hostname to <am335x-evm>.
[ 9.398035] systemd[1]: Configuration file /etc/systemd/system/systemd-udevd.service is marked executable. Please remove executable permission bits. Proceeding anyway.
[ 9.413370] systemd[1]: Configuration file /etc/systemd/system/systemd-udevd.service is marked world-writable. Please remove world writability permission bits. Proceeding anyway.
[ 9.476051] systemd[1]: /lib/systemd/system/gadget-init.service:15: Unknown lvalue 'ExecStopPre' in section 'Service'
[ 9.635835] systemd[1]: Configuration file /etc/systemd/system/systemd-hostnamed.service is marked executable. Please remove executable permission bits. Proceeding anyway.
[ 9.651445] systemd[1]: Configuration file /etc/systemd/system/systemd-hostnamed.service is marked world-writable. Please remove world writability permission bits. Proceeding anyway.
[ 9.776933] systemd[1]: Configuration file /etc/systemd/system/sync-clocks.service is marked executable. Please remove executable permission bits. Proceeding anyway.
[ 9.792115] systemd[1]: Configuration file /etc/systemd/system/sync-clocks.service is marked world-writable. Please remove world writability permission bits. Proceeding anyway.
[ 9.885860] random: systemd: uninitialized urandom read (16 bytes read)
[ OK ] Reached target Swap.
[ 9.918929] random: systemd: uninitialized urandom read (16 bytes read)
[ OK ] Created slice System Slice.
[ 9.960233] random: systemd: uninitialized urandom read (16 bytes read)
Mounting Kernel Debug File System...
[ OK ] Created slice system-serial\x2dgetty.slice.
Mounting Temporary Directory (/tmp)...
[ OK ] Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket.
[ OK ] Listening on Syslog Socket.
Starting Journal Service...
[ OK ] Reached target Remote File Systems.
[ 10.258374] systemd-journald[60]: Configuration file /etc/systemd/journald.conf is marked executable. Please remove executable permission bits. Proceeding anyway.
[ 10.273555] systemd-journald[60]: Configuration file /etc/systemd/journald.conf is marked world-writable. Please remove world writability permission bits. Proceeding anyway.
[ OK ] Started Forward Password Requests to Wall Directory Watch.
Starting Remount Root and Kernel File Systems...
[ OK ] Listening on udev Control Socket.
[ OK ] Listening on Network Service Netlink Socket.
[ 10.398142] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
[ OK ] Listening on Process Core Dump Socket.
Starting Load Kernel Modules...
[ OK ] Created slice system-getty.slice.
[ 10.561005] cryptodev: loading out-of-tree module taints kernel.
Mounting POSIX Message Queue File System...
[ 10.579596] cryptodev: driver 1.9 loaded.
[ OK ] Created slice User and Session Slice.
[ OK ] Reached target Slices.
[ 10.649313] usbcore: registered new interface driver usbfs
[ 10.654933] usbcore: registered new interface driver hub
[ OK ] Listening on /dev/initctl Compatibility Named[ 10.663491] usbcore: registered new device driver usb
Pipe.
[ 10.683930] usbcore: registered new interface driver usbserial
[ OK ] Listening on udev Kernel Socket.
[ OK ] Started Dispatch Password Requests to Console Directory Watch.
[ OK ] Reached target Paths.
[ OK ] Mounted Kernel Debug File System.
[ OK ] Mounted POSIX Message Queue File System.
[ OK ] Mounted Temporary Directory (/tmp).
[ OK ] Started Journal Service.
[ OK ] Started Remount Root and Kernel File Systems.
[FAILED] Failed to start Load Kernel Modules.
See 'systemctl status systemd-modules-load.service' for details.
Mounting Kernel Configuration File System...
Starting Apply Kernel Variables...
Starting Rebuild Hardware Database...
Starting Create System Users...
Starting Flush Journal to Persistent Storage...
[ OK ] Mounted Kernel Configuration File System.
[ OK ] Started Apply Kernel Variables.
[ OK ] Started Create System Users.
[ 11.421562] systemd-journald[60]: Received request to flush runtime journal from PID 1
Starting Create Static Device Nodes in /dev...
[ OK ] Started Flush Journal to Persistent Storage.
[ OK ] Started Create Static Device Nodes in /dev.
[ OK ] Reached target Local File Systems (Pre).
Mounting /media/ram...
Mounting /var/volatile...
Starting udev Kernel Device Manager...
[ OK ] Mounted /var/volatile.
[ OK ] Mounted /media/ram.
Starting Load/Save Random Seed...
[ OK ] Reached target Local File Systems.
Starting Rebuild Dynamic Linker Cache...
Starting Create Volatile Files and Directories...
Starting Rebuild Journal Catalog...
[ OK ] Started Load/Save Random Seed.
[ OK ] Started udev Kernel Device Manager.
[ OK ] Started Create Volatile Files and Directories.
Starting Update UTMP about System Boot/Shutdown...
Starting Network Time Synchronization...
[ OK ] Started Rebuild Journal Catalog.
[ OK ] Started Update UTMP about System Boot/Shutdown.
[ OK ] Started Rebuild Dynamic Linker Cache.
[ OK ] Started Network Time Synchronization.
[ OK ] Reached target System Time Synchronized.
[ OK ] Started Rebuild Hardware Database.
Starting Update is Completed...
Starting udev Coldplug all Devices...
[ OK ] Started Update is Completed.
[ OK ] Started udev Coldplug all Devices.
[ OK ] Reached target System Initialization.
[ 19.709228] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
Starting Network Service...
[ OK ] Listening on D-Bus System Message Bus Socket.
[ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[ OK ] Started Daily Cleanup of Temporary Directories.
[ 19.882502] omap_rtc 44e3e000.rtc: registered as rtc0
[ OK ] Listening on dropbear.socket.
[ OK ] Started Daily rotation of log files.
[ OK ] Reached target Timers.
[ OK ] Listening on RPCbind Server Activation Socket.
[ OK ] Reached target Sockets.
[ OK ] Reached target Basic System.
[ OK ] Started Periodic Command Scheduler.
[ OK ] Reached target Containers.
[ OK ] Started Kernel Logging Service.
Starting uim-sysfs.service...
[ 20.523276] omap-sham 53100000.sham: hw accel on OMAP rev 4.3
[ OK ] Started Job spooling tools.
[ OK ] Started D-Bus System Message Bus.
[ 20.778974] omap-aes 53500000.aes: OMAP AES hw accel rev: 3.2
[ 20.803116] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 20.836005] omap-aes 53500000.aes: will run requests pump with realtime priority
[ 21.014356] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 21.037842] PM: Cannot get wkup_m3_ipc handle
[ 21.175724] PM: Cannot get wkup_m3_ipc handle
[ 21.239651] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 21.440200] remoteproc remoteproc0: wkup_m3 is available
[ 21.445933] PM: Cannot get wkup_m3_ipc handle
[ 21.486223] PM: Cannot get wkup_m3_ipc handle
[ 21.490941] remoteproc remoteproc0: powering up wkup_m3
[ 21.519105] remoteproc remoteproc0: Booting fw image am335x-pm-firmware.elf, size 224628
[ 21.519373] remoteproc remoteproc0: remote processor wkup_m3 is now up
[ 21.519399] wkup_m3_ipc 44e11324.wkup_m3_ipc: CM3 Firmware Version = 0x192
Starting Login Service...
Starting Print notice about GPLv3 packages...
[ 22.493093] net eth0: initializing cpsw version 1.12 (0)
Starting RPC Bind Service...
[ 22.680129] SMSC LAN8710/LAN8720 4a101000.mdio:00: attached PHY driver [SMSC LAN8710/LAN8720] (mii_bus:phy_addr=4a101000.mdio:00, irq=POLL)
Starting Avahi mDNS/DNS-SD Stack...
[ 22.833591] libphy: PHY 4a101000.mdio:01 not found
[ 22.983012] net eth0: phy "4a101000.mdio:01" not found on slave 1, err -19
[ 23.023630] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[ OK ] Started System Logging Service.
[ OK ] Started Hardware RNG Entropy Gatherer Daemon.
[ OK ] Started Network Service.
[ OK ] Started RPC Bind Service.
[ 23.665283] random: crng init done
[ 23.823850] random: 7 urandom warning(s) missed due to ratelimiting
[ OK ] Found device /dev/ttyS0.
[ OK ] Found device /dev/ttyS3.
[ 25.304828] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[ OK ] Found device /dev/mmcblk0p1.
[ OK ] Started Avahi mDNS/DNS-SD Stack.
[ OK ] Started Login Service.
Starting Start USB gadget...
[ OK ] Listening on Load/Save RF Kill Switch Status /dev/rfkill Watch.
Starting Wait for Network to be Configured...
[ OK ] Reached target Network.
[ OK ] Started Redis In-Memory Data Store.
Starting Enable and configure wl18xx bluetooth stack...
Starting Permit User Sessions...
Starting Simple Network Management Protocol (SNMP) Daemon....
Starting Lightning Fast Webserver With Light System Requirements...
Starting Network Name Resolution...
[ 28.047972] udc-core: couldn't find an available UDC - added [g_multi] to list of pending drivers
[ OK ] Started Permit User Sessions.
[ OK ] Started Enable and configure wl18xx bluetooth stack.
[ OK ] Started Lightning Fast Webserver With Light System Requirements.
[ OK ] Started Network Name Resolution.
[ OK ] Started uim-sysfs.service.
[FAILED] Failed to start Start USB gadget.
See 'systemctl status gadget-init.service' for details.
[ OK ] Started Simple Network Management Protocol (SNMP) Daemon..
[ 30.793015] pm33xx pm33xx: PM: am33xx_pm_alloc_sram: Unable to get sram pool for ocmcram
[ 30.832453] am335x-phy-driver 47401300.usb-phy: 47401300.usb-phy supply vcc not found, using dummy regulator
[ 30.941037] am335x-phy-driver 47401b00.usb-phy: 47401b00.usb-phy supply vcc not found, using dummy regulator
[ 31.185277] using random self ethernet address
[ 31.197085] using random host ethernet address
[ 31.247986] using host ethernet address: 98:5D:AD:7F:BB:93
[ 31.248057] using random self ethernet address
[ 31.358902] using random host ethernet address
[ 31.363410] using host ethernet address: 98:5D:AD:7F:BB:93
[ 31.430203] usb0: HOST MAC 98:5d:ad:7f:bb:93
[ 31.525112] usb0: MAC 2e:34:16:ed:3f:0e
[ 31.660204] Mass Storage Function, version: 2009/09/11
[ 31.692496] LUN: removable file: (no medium)
[ 31.697118] LUN: removable read only file: /dev/mmcblk0p1
[ 31.780053] Number of LUNs=1
[ 31.805937] g_multi gadget: Multifunction Composite Gadget
[ 31.861552] g_multi gadget: g_multi ready
[ 31.945108] musb-hdrc musb-hdrc.1: MUSB HDRC host driver
[ 31.974883] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 1
[ 32.022420] hub 1-0:1.0: USB hub found
[ 32.038366] hub 1-0:1.0: 1 port detected
[ 32.377225] wl18xx_driver wl18xx.0.auto: Direct firmware load for ti-connectivity/wl1271-nvs.bin failed with error -2
[ 33.210179] wlcore: wl18xx HW: 183x or 180x, PG 2.2 (ROM 0x11)
[ 33.492276] wlcore: loaded
[ OK ] Found device /dev/ttyGS0.
Starting Load/Save RF Kill Switch Status...
Starting rc.pvr.service...
[ OK ] Reached target Host and Network Name Lookups.
[ OK ] Started NFS status monitor for NFSv2/3 locking..
[ OK ] Started Serial Getty on ttyS3.
[ OK ] Started Getty on tty1.
[ OK ] Started Serial Getty on ttyS0.
[ OK ] Started Serial Getty on ttyGS0.
[ OK ] Reached target Login Prompts.
Starting Synchronize System and HW clocks...
[ OK ] Started Load/Save RF Kill Switch Status.
[ OK ] Started Synchronize System and HW clocks.
[ 36.409857] cpsw 4a100000.ethernet eth0: Link is Up - 100Mbps/Full - flow control off
[ 36.417903] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
[ OK ] Started rc.pvr.service.
Starting weston.service...
[ OK ] Started weston.service.
Starting telnetd.service...
[ OK ] Started telnetd.service.
Starting busybox-udhcpd.service...
Starting thttpd.service...
[ OK ] Started busybox-udhcpd.service.
[ 38.192919] wlcore: PHY firmware version: Rev 8.2.0.0.240
[ 38.298223] wlcore: firmware booted (Rev 8.9.0.0.76)
[ 38.336978] IPv6: ADDRCONF(NETDEV_UP): wlan0: link is not ready
[ OK ] Started thttpd.service.
Starting rng-tools.service...
[ 38.571541] IPv6: ADDRCONF(NETDEV_UP): usb0: link is not ready
[ OK ] Started rng-tools.service.
Starting SYSV: The kdump script provides the support:...
[ 38.928667] wlcore: ERROR ELP wakeup timeout!
[ 38.942595] ------------[ cut here ]------------
[ 38.989660] WARNING: CPU: 0 PID: 76 at /oe/bld/build-CORTEX_1/arago-tmp-external-linaro-toolchain/work-shared/am335x-evm/kernel-source/drivers/net/wireless/ti/wlcore/main.c:796 wl12xx_queue_recovery_work.part.10+0x6c/0x70 [wlcore]
[ 38.989668] Modules linked in: pvrsrvkm(O) arc4 wl18xx wlcore mac80211 usb_f_acm u_serial cfg80211 usb_f_ecm musb_dsps phy_am335x phy_generic phy_am335x_control musb_hdrc g_multi usb_f_mass_storage usb_f_rndis u_ether libcomposite udc_core wkup_m3_rproc pm33xx wlcore_sdio wkup_m3_ipc remoteproc ti_emif_sram omap_aes_driver crypto_engine omap_crypto omap_sham rtc_omap musb_am335x omap_wdt sch_fq_codel uio_module_drv(O) uio usbserial usbcore usb_common cryptodev(O)
[ 38.989787] CPU: 0 PID: 76 Comm: kworker/u2:2 Tainted: G O 4.14.40-g4796173fc5 #1
[ 38.989791] Hardware name: Generic AM33XX (Flattened Device Tree)
[ 38.990157] Workqueue: phy0 ieee80211_reconfig_filter [mac80211]
[ 38.994323] Backtrace:
[ 38.994379] [<c010ba48>] (dump_backtrace) from [<c010bd2c>] (show_stack+0x18/0x1c)
[ 38.994391] r7:00000009 r6:00000000 r5:bf2af060 r4:00000000
[ 38.994409] [<c010bd14>] (show_stack) from [<c0829588>] (dump_stack+0x24/0x28)
[ 38.994426] [<c0829564>] (dump_stack) from [<c0128ab4>] (__warn+0xe8/0x100)
[ 38.994439] [<c01289cc>] (__warn) from [<c0128b84>] (warn_slowpath_null+0x28/0x30)
[ 38.994449] r9:bf2b7cc0 r8:00000000 r7:ffff99d1 r6:ffffff92 r5:c0d152c0 r4:d6910d00
[ 38.994658] [<c0128b5c>] (warn_slowpath_null) from [<bf297a70>] (wl12xx_queue_recovery_work.part.10+0x6c/0x70 [wlcore])
[ 38.994810] [<bf297a04>] (wl12xx_queue_recovery_work.part.10 [wlcore]) from [<bf29b228>] (wl12xx_queue_recovery_work+0x1c/0x20 [wlcore])
[ 38.994816] r5:c0d152c0 r4:d6910d00
[ 38.994953] [<bf29b20c>] (wl12xx_queue_recovery_work [wlcore]) from [<bf2a5040>] (wl1271_ps_elp_wakeup+0x158/0x260 [wlcore])
[ 38.995086] [<bf2a4ee8>] (wl1271_ps_elp_wakeup [wlcore]) from [<bf295ccc>] (wl1271_op_configure_filter+0x5c/0x17c [wlcore])
[ 38.995097] r9:d6910d38 r8:d695ec40 r7:d6910d00 r6:dc7e9ecc r5:bf295c70 r4:d6910420
[ 38.995495] [<bf295c70>] (wl1271_op_configure_filter [wlcore]) from [<bf21e59c>] (ieee80211_configure_filter+0x14c/0x1bc [mac80211])
[ 38.995508] r10:c0d152c0 r9:00000000 r8:dc005000 r7:00000000 r6:d695ec40 r5:bf295c70
[ 38.995511] r4:d6910420
[ 38.995781] [<bf21e450>] (ieee80211_configure_filter [mac80211]) from [<bf21e620>] (ieee80211_reconfig_filter+0x14/0x18 [mac80211])
[ 38.995789] r7:00000000 r6:da6a8e00 r5:da005380 r4:d69107ec
[ 38.995922] [<bf21e60c>] (ieee80211_reconfig_filter [mac80211]) from [<c013fb74>] (process_one_work+0x1f8/0x444)
[ 38.995933] [<c013f97c>] (process_one_work) from [<c013fe44>] (worker_thread+0x84/0x680)
[ 38.995944] r10:c0d152c0 r9:00000088 r8:dc005014 r7:ffffe000 r6:da005398 r5:dc005000
[ 38.995947] r4:da005380
[ 38.995962] [<c013fdc0>] (worker_thread) from [<c0145bb8>] (kthread+0x15c/0x164)
[ 38.995973] r10:dc565e9c r9:c013fdc0 r8:da005380 r7:dc7e8000 r6:00000000 r5:dc6907c0
[ 38.995976] r4:dc690a00
[ 38.995991] [<c0145a5c>] (kthread) from [<c0107e08>] (ret_from_fork+0x14/0x2c)
[ 38.996000] r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c0145a5c
[ 38.996004] r4:dc6907c0
[ 38.996010] ---[ end trace ae67467c477b896d ]---
[ 39.040735] wlcore: Hardware recovery in progress. FW ver: Rev 8.9.0.0.76
[ 39.040745] ------------[ cut here ]------------
[ 39.040975] WARNING: CPU: 0 PID: 76 at /oe/bld/build-CORTEX_1/arago-tmp-external-linaro-toolchain/work-shared/am335x-evm/kernel-source/drivers/net/wireless/ti/wlcore/io.h:66 wlcore_set_partition+0xa8/0x508 [wlcore]
[ 39.040979] Modules linked in: pvrsrvkm(O) arc4 wl18xx wlcore mac80211 usb_f_acm u_serial cfg80211 usb_f_ecm musb_dsps phy_am335x phy_generic phy_am335x_control musb_hdrc g_multi usb_f_mass_storage usb_f_rndis u_ether libcomposite udc_core wkup_m3_rproc pm33xx wlcore_sdio wkup_m3_ipc remoteproc ti_emif_sram omap_aes_driver crypto_engine omap_crypto omap_sham rtc_omap musb_am335x omap_wdt sch_fq_codel uio_module_drv(O) uio usbserial usbcore usb_common cryptodev(O)
[ 39.041098] CPU: 0 PID: 76 Comm: kworker/u2:2 Tainted: G W O 4.14.40-g4796173fc5 #1
[ 39.041101] Hardware name: Generic AM33XX (Flattened Device Tree)
[ 39.041201] Workqueue: phy0 wl1271_recovery_work [wlcore]
[ 39.041206] Backtrace:
[ 39.041243] [<c010ba48>] (dump_backtrace) from [<c010bd2c>] (show_stack+0x18/0x1c)
[ 39.041253] r7:00000009 r6:00000000 r5:bf2b21d8 r4:00000000
[ 39.041270] [<c010bd14>] (show_stack) from [<c0829588>] (dump_stack+0x24/0x28)
[ 39.041287] [<c0829564>] (dump_stack) from [<c0128ab4>] (__warn+0xe8/0x100)
[ 39.041299] [<c01289cc>] (__warn) from [<c0128b84>] (warn_slowpath_null+0x28/0x30)
[ 39.041309] r9:00000000 r8:dc005000 r7:d6910d38 r6:bf2b7cc0 r5:bf2d9064 r4:d6910d00
[ 39.041397] [<c0128b5c>] (warn_slowpath_null) from [<bf2a0fb4>] (wlcore_set_partition+0xa8/0x508 [wlcore])
[ 39.041537] [<bf2a0f0c>] (wlcore_set_partition [wlcore]) from [<bf29a3a8>] (wl1271_recovery_work+0x148/0x350 [wlcore])
[ 39.041544] r6:da6a8e00 r5:d6910d00 r4:d6910f94
[ 39.041620] [<bf29a260>] (wl1271_recovery_work [wlcore]) from [<c013fb74>] (process_one_work+0x1f8/0x444)
[ 39.041629] r8:dc005000 r7:00000000 r6:da6a8e00 r5:da005380 r4:d6910f94
[ 39.041639] [<c013f97c>] (process_one_work) from [<c013fe44>] (worker_thread+0x84/0x680)
[ 39.041650] r10:c0d152c0 r9:00000088 r8:dc005014 r7:ffffe000 r6:da005398 r5:dc005000
[ 39.041653] r4:da005380
[ 39.041669] [<c013fdc0>] (worker_thread) from [<c0145bb8>] (kthread+0x15c/0x164)
[ 39.041680] r10:dc565e9c r9:c013fdc0 r8:da005380 r7:dc7e8000 r6:00000000 r5:dc6907c0
[ 39.041683] r4:dc690a00
[ 39.041695] [<c0145a5c>] (kthread) from [<c0107e08>] (ret_from_fork+0x14/0x2c)
[ 39.041705] r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c0145a5c
[ 39.041709] r4:dc6907c0
[ 39.041713] ---[ end trace ae67467c477b896e ]---
[ 39.041733] wlcore: down
[ 39.044616] ieee80211 phy0: Hardware restart was requested
[ 39.544887] wlcore: PHY firmware version: Rev 8.2.0.0.240
[ 39.683913] wlcore: firmware booted (Rev 8.9.0.0.76)
***************************************************************
***************************************************************
NOTICE: This file system contains the following GPLv3 packages:
autoconf
bash-dev
bash
binutils
cifs-utils
cpio
cpp-symlinks
cpp
dosfstools
elfutils
findutils
g++-symlinks
g++
gawk
gcc-symlinks
gcc
gdb
gdbserver
gettext
gstreamer1.0-libav
gzip
hidapi
libdw1
libelf1
libgdbm-compat4
libgdbm-dev
libgdbm4
libgettextlib
libgettextsrc
libgmp10
libidn11
libmavconn
libmpc3
libmpfr4
libreadline-dev
libreadline7
libunistring2
m4-dev
m4
make
mavlink
mavros-extras
mavros-msgs
mavros
nettle
python3-pycairo
socketcan-interface
which
If you do not wish to distribute GPLv3 components please remove
the above packages prior to distribution. This can be done using
the opkg remove command. i.e.:
opkg remove <package>
Where <package> is the name printed in the list above
NOTE: If the package is a dependency of another package you
will be notified of the dependent packages. You should
use the --force-removal-of-dependent-packages option to
also remove the dependent packages as well
***************************************************************
***************************************************************
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org am335x-evm ttyS0
Arago 2018.04 am335x-evm ttyS0
am335x-evm login: root
Login incorrect
am335x-evm login: root
Login incorrect
am335x-evm login: