Hello,
I write you because I have a problem working with SoC Analyzer 1.2 and dm6446.
In particular a window error appears, saying that an error occurs in rtadecode.exe; after that the application is going to close. Clicking on the link for more information I obtain the following result:
AppName: rtadecode.exe AppVer: 0.0.0.0 ModName: msvcrt.dll
ModVer: 7.0.2600.2180 Offset: 00031165
I would like to analyze a decode session, so, in the control panel I set these parameters:
Action: Online capture
Session: my_decode_session (this action creates my_decode_session empty folder)
Symbol file: C:\Programmi\Texas Instruments\SoCAnalyzer1_2\dvt_resources\platform\DM644x\solutions\SoCAnalyzer\sessions\decode\decodeCombo.x64P
Notice that the error window appears after the right starting and stopping of Target Capture and the correct transferring of the files from target disk to the host (in my_decode_session folder).
Contemporaneously to the rtadecode.exe error window, in the error log panel of the SoC Analyzer appears several times this error message:
IOException while writing to rtadecode input.
How can I solve it?
Thanks.