This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: MMCHS_SYSCTL register

Guru 10235 points

Part Number: AM5728

Hello, TI Experts,

Our customer sent us a questions about MMC1 interface of AM5728.

They used MMC1-IF for SD card(High Speed mode) by changing clock (48MHz->32MHz) to

configure MMC1.MMCHS_SYSCTL[15:6]=0x03 (0x2:MMCi_FCLK/2 -> 0x3:MMCi_FCLK/3)

based on TRM(SPRUHZ6J) "25.5.1.2.1.7.2 MMCHS Clock Frequency Change".

 

Question:

If they use SD-card(Default Speed mode only) to the MMC1-IF, they think

the clock is also changing to (24MHz->16MHz) automatically because of MMC1.MMCHS_SYSCTL[15:6]=0x03.

 

Is this understanding correct?

 

Best regards,