This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/TDA2: Cannot EDMA transfer between OSA_memAllocSR() and aligned_alloc() allocated buffers

Part Number: TDA2

Tool/software: Linux

Hello, I'm using Processor SDK 3.03, building for custom board with TDA2 chip.

So far I have successfully transferred data between two buffers allocated using OSA_memAllocSR() in a PSDK usecase. I did this by calling OSA_memVirt2Phys() to get physical addresses of those buffers and forwarded that information to an EDMA utility driver that I've written. Now, I need to transfer data between a buffer allocated with OSA_memAllocSR() and a buffer allocated with aligned_alloc() from POSIX. However, I don't know how to get physical address of the one allocated with aligned_alloc(). I would like to know how it could be done so that the EDMA transfer can work.

Thank you in advance.

Regards,

Nick

  • Hi,

    What you're trying to achieve isn't possible through a simple aligned_alloc() call. The aligned_alloc call provides a scattered list, which isn't continous. You need a special allocator such as a CMA which provides a continuous memory region. Please refer this link for more information.

    lwn.net/.../

    The reason OSA_memVirt2Phys() works is because the allocation happens from M4 where the physical to virtual address mapping is 1-1, but this isn't the case on Linux.
    If you intend to use EDMA from Linux, then you will need to use CMA for allocation. You also need a way to inteface your application with the EDMA driver (in vision-SDK EDMA is on M4).
    If you intend to use EDMA from M4, I would recommend allocating from SR and passing the buffer to M4.

    Regards
    Shravan
  • Hi Shravan,

    Can you confirm that the CMA is integrated into the DMA subsystem of ARM in kernel 4.4.84 which is used in PSDK 3.03? If yes, then I suppose it is only a matter of allocating memory with dma_alloc_coherent().

    Regards,
    Nick
  • Hi Nick,

    Sorry about the delayed response, I was on leave.
    Yes you can use dma_alloc_coherent, and if the device is NULL / the device doesn't have a dedicated dma pool, it will allocate from CMA. You can then use this to program the EDMA (the call as such returns a virtual address, but one of the arguments passed contains the physical address).

    Regards
    Shravan
  • Hi Shravan,

    I managed to use dma_alloc_coherent() and perform an EDMA transfer between that and the one allocated with OSA_memAllocSR() so that worked out great.

    The next problem that I'm having is that the buffer allocated with dma_alloc_coherent() cannot be written to a file on SSD opened with O_DIRECT flag. I have posted on a few Linux related forums since I don't think it is related to TI specifically any more but I have got no answers. Do you have any experience with this? I will post this as a new question if you have an answer.

    Looking forward to hearing from you.

    Regards,
    Nick
  • Hi Nick,

    I don't think this is permitted since it security flaw to allow I/O on kernel pages mapped to user-space. There will have to be a copy into kernel space which can then be written through O_DIRECT.

    Regards
    Shravan
  • Hi Shravan,

    We have tried to write to SSD directly from the dma_alloc_coherent() buffers from a kernel module but we have found that writing to disk from kernel space is not encouraged and is only available via certain hacks so we gave up on that. What I would like to know now is something else but I will make another thread and link it here if you would like to look at it, basically we would like to write to SSD directly from OSA_memAllocSR buffers (which is the original problem that drove us into this one) but more details on the thread. It can be found here: https://e2e.ti.com/support/arm/automotive_processors/f/1021/t/729926

    Regards,
    Nick