We have two DSPs in a one chain, in our board.
Currently we setup the code composer as one DSP and one bypass. When we connect to the DSP that we setup, it runs correctly. While this DSP continues to run, we change the bypass and the DSP from code composer setup, so that our active DSP is the other one. We can connect without a problem in this way. However, after we load the code and start to run, it gives an error and disconnects. Apperantly it seems this problem is born when we run the two DSPs together. Do you have any idea why or what should cause this problem?
Note: Our emulator is xds510usb emulator.
Thank you in advance,
Erman