This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: Reserved memory locations

Part Number: AM5728

This is a very basic question, but I cannot find a definitive answer within the documentation I have been reviewing.

When I am looking at the Memory Map (Table 2-1 in SPRUHZ6J.pdf, AM572x Technical Reference Manual), there are many regions indicated as "Reserved".  I am unclear if this means that those addresses are being used elsewhere within the addressing system, or if it means this memory is available as "uninitialized memory" which can be used to create and store variables. It seems to me that it the location is being used elsewhere, but I want to be certain, so your assistance is greatly appreciated. 

Thank you in advance.