This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LTE Turbo decoder with TCP2 on DSK 6455



Dear Sir

I need to develop the LTE Turbo decoder using the TCP2 on DSK6455. I saw few discussions on the E2E community that ends without firm conclusion.

Is there a sample LTE Turbo decoder code that includes both the encoder and decoder using the TCP2 ?

If yes, please let me know where I can find it.

If Turbo LTE is not available, any Turbo encoder and decoder eample is OK. It does not have to plot BER. All what is needed is an example that shows clearly the parameter settings and how to transmfer the systematic and parity bits to the TCP2 and how to transfer the interleaving pattern to the TCP2

Thanks

Essam Sourour