Part Number: TDA2
Tool/software: Linux
Hi,
We are using two TDA2xx evms for PCI interface integration between two boards.
This the link which we followed http://processors.wiki.ti.com/index.php/Linux_Core_PCIe_EP_User%27s_Guide
For the endpoint device we got error like below. How to resolve this error in endpoint controller device?
The kernel log is shown below:-
[ 0.599817] ---[ end trace 89b6ef26cae49ac5 ]---
[ 0.599829] dra7-pcie 51000000.pcie_ep: pm_runtime_get_sync failed
[ 0.599857] dra7-pcie: probe of 51000000.pcie_ep failed with error -22
We are using PROCESSOR_SDK_VISION_03_04_00_00