This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Micron MT9V022 and EVM-DM6437



I'm working with EVM-DM6437 evolution board and I'd like to connect Micron MT9V022 image sensor to it but I'm not sure how to do it. Problem is that on board I have coaxial and S-video input but sensor has some "50 pin champ" connector. I never saw that kind of connection and I’m not sure is there any adapter that can handle it. Does anyone have any idea what I should do? I know that RapidView board has interface but EVM-DM6437 board does not have it. Probably there is the way to connect it with EVM-DM6437 also but I don’t have any clue on how.

Any idea?