Part Number: AM5728
Tool/software: Linux
Hi
I have installed Linux SDK 5.00.00.15v for AM57xx EVM and using Ubuntu 16.04.
Linux SDK installed directory is : /opt/ti_linux_SDK
Qt Installed Directory is : home/ubuntu/Qt
My doubt is to display the example application(like @TargetNFS/usr/share/qt5/examples/opegl/cube) output on LCD, what are the steps need to be followed ?
In which files I have to make changes ?
And to display different application images in LCD1 and LCD2 what changes I have to do and where?
Please help me finding these answers.
Thanks and Regards
Arpita
Thanks