This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA3: TDA3M - eMMC support

Part Number: TDA3

Hi,

1) It is mentioned in datasheet that, TDA3x will support SD 3.1 Version and UHS-I. Shall I able to connect an eMMC Chip instead of SD Card?

2) In that case which eMMC version i have to be restricted?

3) What is the maximum Capacity I can connect over eMMC

4) What is the maximum capacity I can connect over SD using micro SD Card connector?

Need your input on the same ASAP.

Regards,

Chithambara Ganesh