Part Number: AM5726
Tool/software: TI-RTOS
SDK: processor_sdk_rtos_am57xx_5_00_00_15
Hello,
We want to use timer 15 on processor 5726. To initialize the timer, use the code below
app.cfg
var Timer = xdc.useModule('ti.sysbios.timers.dmtimer.Timer');
var IntXbar = xdc.useModule('ti.sysbios.family.shared.vayu.IntXbar');
var TimerSupport = xdc.useModule('ti.sysbios.family.shared.vayu.TimerSupport');
TimerSupport.availMask |= (0x1 << 14);
IntXbar.connectMeta(47, 341);
Timer.timerSettings[14].intNum = 70;
main.c
Void myIsr15(Void)
{
Log_info0("myIsr15");
}
static void TimerPRCMConfigure(void)
{
HW_WR_REG32(SOC_L4PER_CM_CORE_BASE + CM_L4PER3_TIMER15_CLKCTRL, 0x2);
while ((HW_RD_REG32(SOC_L4PER_CM_CORE_BASE + CM_L4PER3_TIMER15_CLKCTRL) & (0x00030000)) != 0x0) ;
}
Int main() {
Error_Block eb;
Error_init(&eb);
TimerPRCMConfigure();
Timer_Handle timerHandle;
Timer_Params timerParams;
Timer_Params_init(&timerParams);
timerParams.period = 1000; /* 1 ms */
timerParams.periodType = Timer_PeriodType_MICROSECS;
timerParams.arg = 1;
timerParams.runMode = Timer_RunMode_CONTINUOUS;
timerHandle = Timer_create(14, myIsr15, &timerParams, &eb);
if (timerHandle == NULL) {
Log_info0("Timer create failed");
}
BIOS_start(); /* does not return */
return(0);
}
At debugging In CCS it is visible that the timer 15 goes but function myIsr15 is not called.
When the timer 2 is initialized in function Timer_create instead of timer 15, the function myIsr15 is called up. If you do not turn off the power and running this code with the timer 2 and then run this code with timer 15 - function myIsr15 called. But after turning off the power and running code with timer 15 - function myIsr15 not called
Tell me what to do to make the timer 15 work correctly
Thanks