Tool/software: Code Composer Studio
Hi All,
I have some problems in SPI booting with C6678 board.
On one hand,If I just connect emulator in hardware,not launch .ccxml or not connect target, there always one device cannot running in SPI boot mode.And emulator cannot connect core 0 at this time when I want to know the status of the device,however,all the other cores are connected successfully.
On the other hand, if I completely take off the emulator ,no matter in hardware or software,all devices run successfully when I turn off and on the power.
As I know, JTAG mode can take effect only when I connect the target successful,right?And I also can be sure the power is enough to support all devices to run ,because I have successfully ran all in JTAG mode.
So, what may be the reasons?
Waiting for your reply!
Thanks,
HaiShan