hello everyone !
my algorithm need both RGB information and yuv information at the same time
,but what i have known is ,i can use YUV422 ,and convert it to yuv 420 by EDMA3.
but if i also need RGB information, i have two way
one is i convert yuv420 to RGB888 by DSP
the other is i also get the RGB888 by VPBE directly,just like yuv422
so
Can 6437 vpbe support both yuv and RGB888 at the same time ?