Tool/software: Linux
Hello,
is there a minimal C code example that runs on Linux (ARM) side and interacts with the PRU_RPMsg_Echo_Interrupt0/1 example from the PRU Software Support Package?
All it has to do is to 'kick' the PRU so that the pru_rpmsg_send() dst address can be 'learned' for the PRU to send messages to the ARM.
- Load FW into PRU
- Start PRU program
- Send msg to PRU
- Receive answer from PRU
Thank you,
Dusty.