This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI C6713 DSP STARTER KIT

Hello,
My names is Alex and I am working on my senior design project.
I am using DSP Starter Kit (DSK) for the TMS320C6713. What I am trying to do is to have bidirectional transmission between two C6713 boards. I am trying to input two different sine waves, convert it to digital, perform DSP , convert it back to analog and out from two outputs in a real time. Is this possible to do it simultaneous?(real time). I am not sure that AIC23 Codec can code an decode two different things at once by directionally. Is there any daughter cards available for analog inputs and outputs?

  • Alex Gerasimov said:
    I am not sure that AIC23 Codec can code an decode two different things at once by directionally.

    The AIC23 is a stereo audio codec so it could take 2 simultaneous analog inputs (left and right).  Similarly it can also output stereo analog data after you have processed it.

    I'm also attaching an old project I created at one point which takes in stereo audio and outputs stereo audio.  There is a file called processing.c intended for doing your signal processing.

    Alex Gerasimov said:
    My names is Alex and I am working on my senior design project.

    Good luck, Alex!  :)

    Audio Framework (PRISTINE).zip
  • Thank you so much.

    I will be definatly trying this.

    thank you again

    Alex