Tool/software: Linux
Dear all
The attached document is my kernel, and when the kernel boot, the log would indicate " Bad Linux ARM zImage magic! ",what's wrong with it? and how to resolve ?
U-Boot 2016.05-00304-gad06f64-dirty (Aug 21 2018 - 10:23:24 +0530)
CPU : AM335X-GP rev 2.1
Model: TI AM335x EVM
Watchdog enabled
DRAM: 512 MiB
NAND: 512 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
Card did not respond to voltage select!
** Bad device mmc 0 **
Using default environment
<ethaddr> not set. Validating first E-fuse MAC
Net: cpsw, usb_ether
Press SPACE to abort autoboot in 2 seconds
Booting from nand ...
NAND read: device 0 offset 0x100000, size 0x80000
524288 bytes read: OK
NAND read: device 0 offset 0x300000, size 0x800000
8388608 bytes read: OK
Bad Linux ARM zImage magic!
resetting ...