This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA2: EDMA

Part Number: TDA2

How EDMA is related to the QSPI? In my TI driver's code, RPRC image is read from the external SDF, in which EDMA is used. And EDMA is using the QSPI. I am not able to get how these two are related? Please Clarify. 

THanks in Advance!

 Regards, 
Sagar

  • Hi Sagar,

    There are two options for reading app Image from QSPI :CPU copy and EDMA.
    EDMA performs high-performance data transfers between two memories without CPU's intervention.
    Hence SBL uses EDMA.
    Hope this clarifies.

    Regards,
    Rishabh
  • Hi Rishabh,
    Thanks for reply.
    I want to clarify that whether EDMA uses the same pin which QSPI uses or different.
    In my SBL source code
    void QSPI_ReadSectors_edma(void *dstAddr, uint32_t srcOffsetAddr, uint32_t length, uint32_t edma_ch_num)
    this is the function which is used for reading from external SDF. Inside this function following function is called

    uint32_t EDMA3EnableTransfer(uint32_t baseAddr, uint32_t chNum,uint32_t trigMode)
    {
    uint32_t retVal = FALSE;
    switch (trigMode)
    {
    case EDMA3_TRIG_MODE_MANUAL:
    if (chNum < SOC_EDMA3_NUM_DMACH)
    {
    EDMA3SetEvt(baseAddr, chNum);
    retVal = (uint32_t) TRUE;
    }
    break;

    case EDMA3_TRIG_MODE_QDMA:
    if (chNum < SOC_EDMA3_NUM_QDMACH)
    {
    EDMA3EnableQdmaEvt(baseAddr, chNum);
    retVal = (uint32_t) TRUE;
    }
    break;

    case EDMA3_TRIG_MODE_EVENT:
    if (chNum < SOC_EDMA3_NUM_DMACH)
    {
    /*clear SECR & EMCR to clean any previous NULL request */
    EDMA3ClrMissEvt(baseAddr, chNum);

    /* Set EESR to enable event */
    EDMA3EnableDmaEvt(baseAddr, chNum);
    retVal = (uint32_t) TRUE;
    }
    break;

    default:
    retVal = (uint32_t) FALSE;
    break;
    }
    return retVal;
    }

    If you have the edma.c then please explain me how this function works.

    Also what is the meaning of shadow region?

    Thanks!
    Regards,
    Sagar
  • Hi Sagar,

    I would suggest you to go through EDMA chapter from TDA2 TRM.

    Regards,
    Rishabh