This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/LINUXSDK-AM35X: Qt3d examples issue

Part Number: LINUXSDK-AM35X

Tool/software: Linux

Dear Sir/Madam,

Having some issues running the qt3d examples in sdk 5.00.00.15 qt5.9. Following examples crash or work with errors

/usr/share/qt5/examples/qt3d

qardboard               anaglyph-rendering                    
scene2d                 compute-particles      widgets-scene3d

widget-scene3d rendering is completely corrupted while the same non-widget qt example "scene3d" rendering of the same file works.

Is this an issue with the processor, sdk or qt? Its very blurred

As a last resort I bitbaked qt3d and installed the packages on the target. It made no difference.

best regards

Naseer

Platform is

beaglebone black

24 bit rgb 7" display