Part Number: DRA74
Hello Support,
We’ve been trying to use the J6 PCIe interface to connect to a WiFi module on our board but we’re having some problems.
Our board is still based on the circuit from the evaluation board, can you tell me if this is intended to work as a PCI endpoint or a PCI host?
The Users Guide suggests that the DRA74x-evm boards are intended to be operated in Root Complex mode. However when we tried we found that we needed to replace the 100R termination resistor (across LJCB_CLKN and LJCB_CLKP) with two 50R resistors, one from each signal to ground. This piece of guesswork was based on a brief trawl of the internet which suggested that we might also need series resistor depending on the internal configuration of the host (J6). Based on this we’d like to know:-
- Are our 50R to ground termination resistors OK for the J6?
- Our WiFi module is on the same board as the J6; should we place the termination resistors near the module or near the J6?
- Should we fit series resistors as well? (And if so what value would be best?)
- Are there any other hardware features we should consider for reliable PCIe operation?
Thanks.