Other Parts Discussed in Thread: TVP5146
Hi,
I have a progressive cmos sensor(MT9M131) that can output ITU-R BT.656 (YCbCr), 565RGB, 555RGB, or 444RGB formats (progressive scan), i would like to modify vpfe driver for it.
Is the VPFE driver can configure as progressive BT.656 format input mode
(SYN_MODE:0x32f04,CCDCFG:0x8000,REC656IF:0x3)?
If yes, is the result of capture only can capture one field (not full sensor resolution)?
If no , are the other methods that configure in Bayer formats or RGB mode can quickly be implemented?
Any help will be highly appreciated.